This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TIDA-00731:61000-4-5测试的源阻抗

Guru**** 2609895 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1315680/tida-00731-source-impedance-for-61000-4-5-tests

器件型号:TIDA-00731

您好!  

我猜使用的是42欧姆。 无论是2、12还是42、都需要确认。

如果为42、则在2kV 时、理论峰值电流为47A。

压敏电阻的额定值为25A。

是否使用某种平均值计算来选择该特定部件? 可能是迭代仿真?

此致

迪安