This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TIDA-010242:扩展电压范围9-36V LM7480*&LM5069

Guru**** 2812305 points

Other Parts Discussed in Thread: LM5069

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1274288/tida-010242-extended-voltage-range-9-36v-lm7480-lm5069

器件型号:TIDA-010242
主题中讨论的其他器件:LM5069

我计划在产品中使用此基准电路、但理想情况下输入/输出范围为7-36V、电流原理图显示23-33V

我计划稍微增大 D4以实现最高36V。

我知道 LM5069的最小电压是9V、所以我会稳定下来、但是否需要对电路进行任何改动以确保实现这一点?


有人可以澄清 BOM 上没有的 NT1*组件吗? 我猜它们是网络联系/星级?