This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LM3488:LM3488

Guru**** 2502205 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1362403/lm3488-lm3488

器件型号:LM3488

您好!

请帮助我解决此问题。

第1

第32行错误:v:x1:1n014«»:3«0»v=v(N015)+v(n011)
未知参数"v"
第18行错误:v§ramp N015 0 puls(010*1m*1m/l ts 0/fs 1n 1/fs 0)
未知参数"*1m*1m/l" ts
第19行错误:v§CLOCK N018 0脉冲(0 1 0 1n 1n (0.1* ts)(ts))
未知参数"* ts "
第35行中的错误: v:x3:1n017»:3«0»:0«v=if(v(n014)>v(n012),1,0)
未知参数"v"

第2个
致命错误:斜坡:需要至少5个参数。 仅指定了2个。

此致、谢谢

阿姆里塔