This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS54560:降压转换器

Guru**** 2928980 points

Other Parts Discussed in Thread: TPS54560

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1398468/tps54560-buck-converter

器件型号:TPS54560

工具与软件:

在 LT Spice 中使用 TPS54560 iC 开发降压转换器。

输入电压15V

输出电压5V

当我在 LT SPICE 中仿真和运行设计时、我看到输入为197安培、我的负载最大3安培、能否使用需要的模型进行检查。