This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PMP20306:建议

Guru**** 2928980 points

Other Parts Discussed in Thread: PMP20834

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1402629/pmp20306-suggestion

器件型号:PMP20306
Thread 中讨论的其他器件:PMP20834

工具与软件:

嗨、团队:

客户正在其新项目中寻找直流/直流反激式解决方案、以便将400V (BMS 电池包)转换为5V (用于 CC2662)、非隔离式可以。

您能提供一些解决方案建议吗?

非常感谢!

谢谢、此致、

Wendy