This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPSM843620:TPSM843620 webench 负载瞬态仿真模型

Guru**** 2885260 points

Other Parts Discussed in Thread: TPSM843620

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1408963/tpsm843620-tpsm843620-webench-simulation-model-for-load-transient

器件型号:TPSM843620

工具与软件:

大家好、团队成员:

我将 TPSM843620器件用于我的设计、采用以下配置:

输入电压:12V

输出电压:1V

负载电流:4A

由于 Webench 仿真不适用于此配置、您能给我提供仿真模型吗?

谢谢!