This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TIDA-010015:请求磁性元件 L1、L6、L7和 T1的规格

Guru**** 2589265 points
Other Parts Discussed in Thread: TIDA-010015

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1419341/tida-010015-request-specifications-for-magnetic-elements-l1-l6-l7-and-t1

器件型号:TIDA-010015

工具与软件:

你好

我收到有关 TIDA-010015的疑问。

制造产品时、"L1、L6、L7、T1"被标识为需要制造的部件。

- L1, L6:变压器, 160 uH, TH
- L7:电感、铁氧体、330 µH、6.1A、0.074欧姆、 TH
- T1 : PQ3230(Payton )/变压器, TH

请提供制造上述磁性元件所需的磁芯、线轴、导线厚度和匝数比数据(数据表或规格)。