This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PSPICE-FOR-TI:TPS51385仿真问题

Guru**** 2957980 points

Other Parts Discussed in Thread: TPS51385

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1447132/pspice-for-ti-tps51385-simulation-issues

器件型号:PSPICE-FOR-TI
主题中讨论的其他器件:TPS51385

工具与软件:

您好!

我正在尝试在12V 输入和3.3V 输出下对 TPS51385进行瞬态仿真。 我已附加存档文件。 仿真运行、但我看到输出电压约为1.3V、并且开关在仿真开始时启动、但在4ms 左右停止。  您能帮助调试导致此仿真结果的问题吗?