This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PMP3162:PMP3162、提供24V 输出评估

Guru**** 2938610 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1477062/pmp3162-pmp3162-with-24v-output-evaluation

器件型号:PMP3162

工具与软件:

大家好、团队成员:  

客户寻求48Vin /24V out @12.5A ~ 25A、我们建议客户参考此参考设计。  

我们能否帮助客户 评估将输出扩展到24V 的此参考设计?  

谢谢、此致

Eddie