This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1120:2.1V时的CC1120电流消耗

Guru**** 2390735 points
Other Parts Discussed in Thread: TPS62740, CC1120
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/604659/cc1120-cc1120-current-consumption-at-2-1v

部件号:CC1120
主题中讨论的其他部件:TPS6.273万TPS6.274万

 您好,TI:

 您是否有  TX的当前功耗编号(在2.1 V时为+10 dBm,在0 dBm)和  RX 功耗编号(在2.1V时)?  我们需要此信息来决定是否使用TPS6.273万/TPS62740将6.274万将电压降至2.1V。

 电源是  一对并行CR2032。 我们需要设计一个寿命超过7年的CC1120+MSP430Gxxxx节点。

克里斯