This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1350STK:Contiki TSCH Mac,用于CC1350

Guru**** 2815225 points

Other Parts Discussed in Thread: CC1350, CC1310

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/632028/cc1350stk-contiki-tsch-mac-for-cc1350

部件号:CC1350STK
主题中讨论的其他部件:CC1350CC1310

您好,
我尝试在CC1350传感器标签上使用rime+TSCH。

  1. make target=srf06-cc26xx Board=sensortag/cc1350 at
    /home/ga83jok/contiki/examples/rime-TSCH/
  2. 我收到以下错误,
Starting Contiki-3.x-3336-g1364e98
With DriverLib v0.47020
TI CC1350 SensorTag
IEEE 802.15.4: Yes, Sub-GHz: Yes, BLE: Yes, Prop: Yes
 Net: Rime
 MAC: TSCH
 RDC: nordc
TSCH:! radio does not support getting RADIO_PARAM_RX_MODE. Abort `init.`

有人能帮我解决这个问题吗。 TSCH是否仍然没有连接到CC1350?

此致,
Abhishek