请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他部件:CC1125, CC1120你(们)好
我必须制造427 MHz - 447 MHz支持的产品
产品包括简单的数据交换和1:n通信
请 推荐开发套件。
感谢您的回答。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.