请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:CC1350 主题中讨论的其他部件: CC1190, CC1310
您好,
我想为CC1350设计一个50欧姆印刷电路板跟踪和50欧姆鞭状天线的匹配网络。
从MCU的RF_N和RF_P端口观察到的源阻抗是多少?
我正在使用915MHz频段。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.