This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1200:CC1200是否可以在262MHz ~ 264MHz下工作?

Guru**** 2766215 points

Other Parts Discussed in Thread: CC1200

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/662966/cc1200-can-cc1200-be-operated-in-262mhz-264mhz

部件号:CC1200

尊敬的先生:

我们已经完成了一些射频无线调制解调器的开发工作  ,这些调制解调器在欧洲为800MHz,在韩国为900MHz。

我们想知道CC1200可以在262MHz ~ 264MHz下工作。

如果无法在262MHz ~ 264MHz下工作,请推荐其他解决方案。

--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

如果可以在262MHz ~ 264MHz下工作,请发送一些信息。

祝您一切顺利,

光波格火腿