This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1312R:OBW测试失败

Guru**** 2593530 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1097512/cc1312r-obw-test-fail

部件号:CC1312R

大家好,  

我的客户 正在使用CC1312,但无法 通过日本占用的带宽测试。

他们尝试降低TX功率,但OBW测试仍然失败。

请帮助提供意见。 谢谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,

    请提供有关所执行测量的更多信息:

    • 客户使用的PHY是什么?
    • 是客户主板还是LaunchPad (通过SmartRF Studio或其他)?
    • 他们在这里使用什么设置? 这样,我们就能更好地了解他们应该期待什么。
    • 他们的测试设置是什么?

    此致,
    扎克

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    此外:他们正在使用多少单位信道(假设这是T-108)

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,  

    请检查以下各项:

    • 客户使用的PHY是什么?-->2-GFSK
    • 是客户主板还是LaunchPad (通过SmartRF Studio或其他)? -->客户主板
    • 他们在这里使用什么设置?-->
      //*********************************************************************************
      // Generated by SmartRF Studio version 2.23.0 (build#300)
      // The applied template is compatible with cc13x2_26x2 SDK version 2.10.xx.xx or newer.
      // Device: CC1312R Rev. E (2.1). 
      //
      //*********************************************************************************
      
      
      //*********************************************************************************
      // Parameter summary
      // Frequency: 927.80000 MHz
      // Data Format: Serial mode disable 
      // Deviation: 190.000 kHz
      // IEEE 802.15.4g Packet Length: 20 
      // Select bit order to transmit PSDU octets: 1 
      // Packet Data: 255 
      // Preamble Count: 7 Bytes 
      // Preamble Mode: Send 0 as the first preamble bit 
      // RX Filter BW: 1092.5 kHz
      // Symbol Rate: 500.00000 kBaud
      // Sync Word: 0x0055904e 
      // Sync Word Length: 24 Bits 
      // TX Power: 7 dBm 
      // Whitening: Dynamically IEEE 802.15.4g compatible whitener and 16/32-bit CRC 
      
      #include "smartrf_settings.h"
      
      #include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_prop.h)
      
      // TI-RTOS RF Mode Object
      RF_Mode RF_prop =
      {
          .rfMode = RF_MODE_AUTO,
          .cpePatchFxn = &rf_patch_cpe_prop,
          .mcePatchFxn = 0,
          .rfePatchFxn = 0
      };
      
      
      // Overrides for CMD_PROP_RADIO_DIV_SETUP
      uint32_t pOverrides[] =
      {
          // override_prop_common.xml
          // DC/DC regulator: In Tx, use DCDCCTL5[3:0]=0x7 (DITHER_EN=0 and IPEAK=7).
          (uint32_t)0x00F788D3,
          // override_prop_common_sub1g.xml
          // Set RF_FSCA.ANADIV.DIV_SEL_BIAS = 1. Bits [0:16, 24, 30] are don't care..
          (uint32_t)0x4001405D,
          // Set RF_FSCA.ANADIV.DIV_SEL_BIAS = 1. Bits [0:16, 24, 30] are don't care..
          (uint32_t)0x08141131,
          // override_tc178.xml
          // Synth: Set loop bandwidth after lock to 40 kHz (K2)
          (uint32_t)0x29200583,
          // Synth: Set loop bandwidth after lock to 40 kHz (K2)
          (uint32_t)0x000005A3,
          // Synth: Set loop bandwidth after lock to 40 kHz (K3, LSB)
          (uint32_t)0xF5700603,
          // Synth: Set loop bandwidth after lock to 40 kHz (K3, MSB)
          (uint32_t)0x00000623,
          // Synth: Set FREF = 4 MHz
          (uint32_t)0x000C84A3,
          // Tx: Configure PA ramp time, PACTL2.RC=0x1 (in ADI0, set PACTL2[4:3]=0x1)
          ADI_2HALFREG_OVERRIDE(0,16,0x8,0x8,17,0x1,0x0),
          // Rx: Set AGC reference level to 0x30 (default: 0x2E)
          HW_REG_OVERRIDE(0x609C,0x0030),
          // Rx: Set RSSI offset to adjust reported RSSI by -4 dB (default: -2), trimmed for external bias and differential configuration
          (uint32_t)0x000488A3,
          // Rx: Set anti-aliasing filter bandwidth to 0xA (in ADI0, set IFAMPCTL3[7:4]=0xA)
          ADI_HALFREG_OVERRIDE(0,61,0xF,0xA),
          // Tx: Set wait time before turning off ramp to 0x1A (default: 0x1F)
          HW_REG_OVERRIDE(0x6028,0x001A),
          // Set LNA IB offset to 0xF
          (uint32_t)0x000F8883,
          (uint32_t)0xFFFFFFFF
      };
      
      
      // CMD_PROP_RADIO_DIV_SETUP
      // Proprietary Mode Radio Setup Command for All Frequency Bands
      rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup =
      {
          .commandNo = 0x3807,
          .status = 0x0000,
          .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
          .startTime = 0x00000000,
          .startTrigger.triggerType = 0x0,
          .startTrigger.bEnaCmd = 0x0,
          .startTrigger.triggerNo = 0x0,
          .startTrigger.pastTrig = 0x0,
          .condition.rule = 0x1,
          .condition.nSkip = 0x0,
          .modulation.modType = 0x1,
          .modulation.deviation = 0x2F8,
          .modulation.deviationStepSz = 0x0,
          .symbolRate.preScale = 0xF,
          .symbolRate.rateWord = 0x50000,
          .symbolRate.decimMode = 0x0,
          .rxBw = 0x60,
          .preamConf.nPreamBytes = 0x7,
          .preamConf.preamMode = 0x0,
          .formatConf.nSwBits = 0x18,
          .formatConf.bBitReversal = 0x0,
          .formatConf.bMsbFirst = 0x1,
          .formatConf.fecMode = 0x0,
          .formatConf.whitenMode = 0x7,
          .config.frontEndMode = 0x0,
          .config.biasMode = 0x1,
          .config.analogCfgMode = 0x0,
          .config.bNoFsPowerUp = 0x0,
          .config.bSynthNarrowBand = 0x0,
          .txPower = 0x26D4,
          .pRegOverride = pOverrides,
          .centerFreq = 0x039F,
          .intFreq = 0x0800,
          .loDivider = 0x05
      };
      
      
      // CMD_FS
      // Frequency Synthesizer Programming Command
      rfc_CMD_FS_t RF_cmdFs =
      {
          .commandNo = 0x0803,
          .status = 0x0000,
          .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
          .startTime = 0x00000000,
          .startTrigger.triggerType = 0x0,
          .startTrigger.bEnaCmd = 0x0,
          .startTrigger.triggerNo = 0x0,
          .startTrigger.pastTrig = 0x0,
          .condition.rule = 0x1,
          .condition.nSkip = 0x0,
          .frequency = 0x039F,
          .fractFreq = 0xCCCD,
          .synthConf.bTxMode = 0x0,
          .synthConf.refFreq = 0x0,
          .__dummy0 = 0x00,
          .__dummy1 = 0x00,
          .__dummy2 = 0x00,
          .__dummy3 = 0x0000
      };
      
      
      // CMD_TX_TEST
      // Transmitter Test Command
      rfc_CMD_TX_TEST_t RF_cmdTxTest =
      {
          .commandNo = 0x0808,
          .status = 0x0000,
          .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
          .startTime = 0x00000000,
          .startTrigger.triggerType = 0x0,
          .startTrigger.bEnaCmd = 0x0,
          .startTrigger.triggerNo = 0x0,
          .startTrigger.pastTrig = 0x0,
          .condition.rule = 0x1,
          .condition.nSkip = 0x0,
          .config.bUseCw = 0x1,
          .config.bFsOff = 0x1,
          .config.whitenMode = 0x2,
          .__dummy0 = 0x00,
          .txWord = 0xFFFF,
          .__dummy1 = 0x00,
          .endTrigger.triggerType = 0x1,
          .endTrigger.bEnaCmd = 0x0,
          .endTrigger.triggerNo = 0x0,
          .endTrigger.pastTrig = 0x0,
          .syncWord = 0x0055904E,
          .endTime = 0x00000000
      };
      
      
    • 他们的测试设置是什么?-->

       请参阅 SWRA457复印的段落。 在客户情况下,限值将为600kHz而不是200kHz。

    谢谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,

    关于"他们使用的单位信道数量(假设这是T-108)",它是 3个信道,600kHz