This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1312R:如何降低射频 TX 电流

Guru**** 2548640 points
Other Parts Discussed in Thread: CC1312R

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1065731/cc1312r-how-to-decrease-rf-tx-current

器件型号:CC1312R

大家好、

我有具有 cc1312R 的定制板。 目前、当每5秒发送792字节数据时、我的电路板消耗20mA 电流。 但20mA 对于我的应用而言过高。 我想将其降低至10mA 或更小。 您可以在下面看到射频设置和代码。

我将更改 TX 功率、例如12.5或12、电流将降低约17.5mA。 但这对我来说还不够。 在以11或10更改 txpower 后、9射频流耗以某种方式增加。 无论如何,我不想降低太多的 Txpower。 因为我需要在50-100米左右发送数据。 如果我对 TX 功率进行降级、距离范围将减小。  

 

如何在不对 TX 功率进行过多去折痕的情况下对该电流进行去折痕?

缓冲区大小约为782字节。 更改尺寸对于当前组合很有用。

或者每秒发送一次是否合乎逻辑。(但发送时间可能会导致过多电流?)

另一个问题是数据发送时间大约为130-140毫秒。 这是正常的吗? 如何缩短此时间?

#include <ti/devices/DeviceFamily.h>
#include DeviceFamily_constructPath(driverlib/rf_mailbox.h)
#include DeviceFamily_constructPath(driverlib/rf_common_cmd.h)
#include DeviceFamily_constructPath(driverlib/rf_prop_cmd.h)
#include <ti/drivers/rf/RF.h>
#include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_prop.h)
#include <ti_radio_config.h>


// TI-RTOS RF Mode Object
RF_Mode RF_prop =
{
    .rfMode = RF_MODE_AUTO,
    .cpePatchFxn = &rf_patch_cpe_prop,
    .mcePatchFxn = 0,
    .rfePatchFxn = 0
};

// Overrides for CMD_PROP_RADIO_DIV_SETUP
uint32_t pOverrides[] =
{
    // override_prop_common.json
    // DC/DC regulator: In Tx, use DCDCCTL5[3:0]=0x7 (DITHER_EN=0 and IPEAK=7).
    (uint32_t)0x00F788D3,
    // override_prop_common_sub1g.json
    // Set RF_FSCA.ANADIV.DIV_SEL_BIAS = 1. Bits [0:16, 24, 30] are don't care..
    (uint32_t)0x4001405D,
    // Set RF_FSCA.ANADIV.DIV_SEL_BIAS = 1. Bits [0:16, 24, 30] are don't care..
    (uint32_t)0x08141131,
    // override_tc106.json
    // Tx: Configure PA ramp time, PACTL2.RC=0x3 (in ADI0, set PACTL2[4:3]=0x3)
    ADI_2HALFREG_OVERRIDE(0,16,0x8,0x8,17,0x1,0x1),
    // Rx: Set AGC reference level to 0x1A (default: 0x2E)
    HW_REG_OVERRIDE(0x609C,0x001A),
    // Rx: Set RSSI offset to adjust reported RSSI by -1 dB (default: -2), trimmed for external bias and differential configuration
    (uint32_t)0x000188A3,
    // Rx: Set anti-aliasing filter bandwidth to 0xD (in ADI0, set IFAMPCTL3[7:4]=0xD)
    ADI_HALFREG_OVERRIDE(0,61,0xF,0xD),
    // Tx: Set wait time before turning off ramp to 0x1A (default: 0x1F)
    HW_REG_OVERRIDE(0x6028,0x001A),

    // TX power override
    // Tx: Set PA trim to max to maximize its output power (in ADI0, set PACTL0=0xF8)
    ADI_REG_OVERRIDE(0,12,0xF8),

//     evalden yaklasik 5 dbm daha iyi sonuc verdi.
//    (uint32_t)0x00F688A3,

    (uint32_t)0xFFFFFFFF
};



// CMD_PROP_RADIO_DIV_SETUP
// Proprietary Mode Radio Setup Command for All Frequency Bands
rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup =
{
    .commandNo = 0x3807,
    .status = 0x0000,
    .pNextOp = 0,
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .modulation.modType = 0x1,
    .modulation.deviation = 0x64,
    .modulation.deviationStepSz = 0x0,
    .symbolRate.preScale = 0xF,
    .symbolRate.rateWord = 0x8000,
    .symbolRate.decimMode = 0x0,
    .rxBw = 0x52,
    .preamConf.nPreamBytes = 0x4,
    .preamConf.preamMode = 0x0,
    .formatConf.nSwBits = 0x20,
    .formatConf.bBitReversal = 0x0,
    .formatConf.bMsbFirst = 0x1,
    .formatConf.fecMode = 0x0,
    .formatConf.whitenMode = 0x0,
    .config.frontEndMode = 0x0,
    .config.biasMode = 0x1, //n-burasi 0 oalbilir
    .config.analogCfgMode = 0x0,
    .config.bNoFsPowerUp = 0x0,
    .config.bSynthNarrowBand = 0x0,
    .txPower = 0x013F, //14 dBm max outputs
//    .txPower = 0xA410  , //14 dBm max output
    .pRegOverride = pOverrides,
    .centerFreq = 0x0364,
    .intFreq = 0x8000,
    .loDivider = 0x05
};

// CMD_FS
// Frequency Synthesizer Programming Command
rfc_CMD_FS_t RF_cmdFs =
{
    .commandNo = 0x0803,
    .status = 0x0000,
    .pNextOp = 0,
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .frequency = 0x0364,
    .fractFreq = 0x0000,
    .synthConf.bTxMode = 0x0,
    .synthConf.refFreq = 0x0,
    .__dummy0 = 0x00,
    .__dummy1 = 0x00,
    .__dummy2 = 0x00,
    .__dummy3 = 0x0000
};

// CMD_PROP_RX_ADV
// Proprietary Mode Advanced Receive Command
rfc_CMD_PROP_RX_ADV_t RF_cmdPropRxAdv =
{
    .commandNo = 0x3804,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .pktConf.bFsOff = 0x0,
    .pktConf.bRepeatOk = 0x0,
    .pktConf.bRepeatNok = 0x0,
    .pktConf.bUseCrc = 0x0,
    .pktConf.bCrcIncSw = 0x0,
    .pktConf.bCrcIncHdr = 0x0,
    .pktConf.endType = 0x0,
    .pktConf.filterOp = 0x0,
    .rxConf.bAutoFlushIgnored = 0x0,
    .rxConf.bAutoFlushCrcErr = 0x0,
    .rxConf.bIncludeHdr = 0x0,
    .rxConf.bIncludeCrc = 0x0,
    .rxConf.bAppendRssi = 0x0,
    .rxConf.bAppendTimestamp = 0x0,
    .rxConf.bAppendStatus = 0x0,
    .syncWord0 = 0x930B51DE,
    .syncWord1 = 0x00000000,
    .maxPktLen = 0x00FF,
    .hdrConf.numHdrBits = 0x0,
    .hdrConf.lenPos = 0x0,
    .hdrConf.numLenBits = 0x0,
    .addrConf.addrType = 0x0,
    .addrConf.addrSize = 0x0,
    .addrConf.addrPos = 0x0,
    .addrConf.numAddr = 0x0,
    .lenOffset = 0x00,
    .endTrigger.triggerType = 0x0,
    .endTrigger.bEnaCmd = 0x0,
    .endTrigger.triggerNo = 0x0,
    .endTrigger.pastTrig = 0x0,
    .endTime = 0x00000000,
    .pAddr = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .pQueue = 0, // INSERT APPLICABLE POINTER: (dataQueue_t*)&xxx
    .pOutput = 0 // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
};


// CMD_PROP_TX_ADV
// Proprietary Mode Advanced Transmit Command
rfc_CMD_PROP_TX_ADV_t RF_cmdPropTxAdv =
{
    .commandNo = 0x3803,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,

    .pktConf.bFsOff = 0x0,
    .pktConf.bUseCrc = 0x1,
    .pktConf.bCrcIncSw = 0x0,
    .pktConf.bCrcIncHdr = 0x0,

    .numHdrBits = 16,

    .pktLen = 0x0000,

    .startConf.bExtTxTrig = 0x0,
    .startConf.inputMode = 0x0,
    .startConf.source = 0x0,

    .preTrigger.triggerType = 0x0,
    .preTrigger.bEnaCmd = 0x0,
    .preTrigger.triggerNo = 0x0,
    .preTrigger.pastTrig = 0x0,

    .preTime = 0x00000000,
    .syncWord = 0x930B51DE,
    .pPkt = 0 // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
};
void RFTx_Function(UArg arg0, UArg arg1)
{
    int i;
    RF_Params rfParams;
    RF_Params_init(&rfParams);

    RF_cmdPropTxAdv.pktLen =  PAYLOAD_LENGTH+2-1;
    RF_cmdPropTxAdv.pPkt = RF_Buffer2;
    RF_cmdPropTxAdv.startTrigger.triggerType = TRIG_ABSTIME;
    RF_cmdPropTxAdv.startTrigger.pastTrig = 1;

    if (!rfHandle)
    {
        rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);
        RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);
    }

    while(1)
    {
        Semaphore_pend(semTxHandle, BIOS_WAIT_FOREVER);
#ifdef WATCHDOG_ENABLE //# komutu ön işlemci komutu demek bu da program calısmaya baslamadan once bu komutun oldugu yerleri kontrol eder.
    	Watchdog_clear(watchdogHandle);
#endif

        RF_Buffer[0]=(uint8_t)(PAYLOAD_LENGTH);
        RF_Buffer[1]=(uint8_t)(PAYLOAD_LENGTH >> 8);

        RF_Buffer[2]=RF_Header[0];
        RF_Buffer[3]=RF_Header[1];

        RF_Buffer[5]=(uint8_t)(PAYLOAD_LENGTH);
        RF_Buffer[4]=(uint8_t)(PAYLOAD_LENGTH >> 8);

        RF_Buffer[7]=(uint8_t)(Destination_Address);
        RF_Buffer[6]=(uint8_t)(Destination_Address >> 8);

        RF_Buffer[9]=(uint8_t)(Source_Address);
        RF_Buffer[8]=(uint8_t)(Source_Address >> 8);

        RF_Buffer[10]=(uint8_t)(Command_Number);

        RF_Buffer[11]=(uint8_t)(Data_Number);
        Data_Number++;

        RF_Buffer[782]='\r';
        RF_Buffer[783]='\n';

        for(i = 0; i < PAYLOAD_LENGTH; i++)
        {	CRC_Buffer[i] = RF_Buffer[i + 2];}

        CRC_Code = CRC16_Calculate(CRC_Buffer, sizeof(CRC_Buffer));

        RF_Buffer[781]=(uint8_t)(CRC_Code);
        RF_Buffer[780]=(uint8_t)(CRC_Code >> 8);

        RFtime = RF_getCurrentTime();
        RFtime += PACKET_INTERVAL;
        RF_cmdPropTxAdv.startTime = RFtime;

        for(i = 0; i < 100; i++)
        {   RF_Buffer2[i] = RF_Buffer[i];}


        RF_EventMask result = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropTxAdv, RF_PriorityNormal, NULL, 0);
        RF_yield(rfHandle);

//                PIN_setOutputValue(hPin, STA_LED,!PIN_getOutputValue(STA_LED));

        memset(RF_Buffer, 0, sizeof(RF_Buffer));
        memset(CRC_Buffer, 0, sizeof(CRC_Buffer));
    }
}

如果您有任何想法或建议、请告诉我

谢谢你

此致

Bekir

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Bekir、

    有人会查看您的主题并尽快为您提供帮助。 感谢您的耐心等待。

    BR、
    安德烈斯

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    数据包传输时间为:

    1/datarate*8*(4+4+782+2)

    给定4字节前导码、4字节同步、2字节 CRC。 根据实际发送的字节数进行调整。

    电流消耗:这取决于您是查看平均电流还是峰值电流。 如果第一个、数据包长度和发送频率会产生影响。 对于峰值电流、数据包长度无关紧要。  

    降低峰值电流的唯一方法是降低输出功率。 此外、请确保使用3.6V 电压为器件供电、因为电流随着 VDDS 的降低而增加:。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的回答