This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1310:从关断状态单次唤醒

Guru**** 777950 points
Other Parts Discussed in Thread: CC1310, HDC2010, BOOSTXL-BASSENSORS
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1003499/cc1310-single-wakeup-from-shutdown

器件型号:CC1310
主题中讨论的其他器件: HDC2010

您好!

我的问题是、我 使用 Power_SHUTDOWN (0、0)将 CC1310置于关断状态  

我使用 GPIO 上的 IOC 唤醒、该功能 工作正常...一次...然后器件无限期保持关断状态。

在测试期间断开调试器。

任何指针都被赞赏。

下面是有关重现此问题的一些详细信息:

在我们的应用中、我们将 HDC2010传感器连接到 CC1310

HDC2010将中断引脚从高电平切换到低电平、以便在通过 I2C 准备好新的温度和湿度数据时触发

我们使用该引脚作为 CC1310的唤醒引脚、将数据传输到收集器、然后在数据采样之间进入关断状态。

采样率为每10秒一次

在硬件方面、我们使用 BOOSTXL-BASSENSORS 分线板与 CC1310 Launchpad

H_INT 是如图所示的唤醒引脚、它被配置为 IOID_25、因此我们知道硬件工作并且分配了正确的引脚。

在验证发生的情况方面、

Smart RF 屏幕截图下方仅显示 收集器接收到的2个数据包

第一个数据包在发送器的第一个 POR 时、第二个数据包是第一个数据包、并且我们只能看到从关断状态唤醒。

请注意、它们之间的间隔正确为10秒

下面的 H_INT 引脚屏幕截图也显示它正确变为高电平、并在 HDC2010通电时保持高电平。

在 t=0sec 时、引脚在 HDC2010上电时变为高电平

在 t=10sec 时、变为低电平、太快、无法在宽范围时基上看到、但 CC1310正确唤醒、读取 int 状态、引脚恢复为高电平。

但是、CC1310不会在下一个采样间隔(t=20秒)唤醒

因此、总高电平持续时间为20秒。

以下是代码、

唤醒引脚在 CC1310_LAUNCHXL.h 中定义为#define BOARD_HDC_DRDY  IOID_25

/*
 * Copyright (c) 2019, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

/***** Includes *****/
/* Standard C Libraries */
#include <stdlib.h>
#include <unistd.h>

/* TI Drivers */
#include <ti/drivers/Power.h>
#include <ti/drivers/rf/RF.h>
#include <ti/drivers/PIN.h>
#include <ti/drivers/I2C.h>
#include <ti/drivers/UART.h>
#include <ti/drivers/pin/PINCC26XX.h>

/* Driverlib Header files */
#include DeviceFamily_constructPath(driverlib/rf_prop_mailbox.h)
#include DeviceFamily_constructPath(driverlib/sys_ctrl.h)           // Needed for SysCtrlResetSourceGet()

// Hardware & Board Header files
#include "HDC2010.h"
#include "Board.h"

/* Application Header files */
#include "RFQueue.h"
#include "smartrf_settings/smartrf_settings.h"


#define HW_VER      0x01
#define FW_VER      0x02

/* Packet RX/TX Configuration */
// -----------------------------------------------------------------------------------------------------
// Defines
#define PAYLOAD_LENGTH      12                      // Max length byte the radio will accept
#define TX_DELAY          (uint32_t)(4000000*0.1f)  // Set Transmit (echo) delay to 100ms
#define PACKET_INTERVAL     500000                  // Set packet interval to 500000us or 500ms
#define NUM_DATA_ENTRIES    2                       // NOTE: Only two data entries supported at the moment
#define NUM_APPENDED_BYTES  2

// Variable declarations
static uint8_t HDC_data[4];
static uint8_t SGP_data[2];

static uint8_t txPacket[PAYLOAD_LENGTH];

// Buffer which contains all Data Entries for receiving data.
// Pragmas are needed to make sure this buffer is aligned to a 4 byte boundary (requirement from the RF core)
#pragma DATA_ALIGN(rxDataEntryBuffer, 4)
//static uint8_t rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,PAYLOAD_LENGTH,NUM_APPENDED_BYTES)];

static RF_Object rfObject;
static RF_Handle rfHandle;
//static rfc_propRxOutput_t rxStatistics;             // Receive Statistics
//static dataQueue_t dataQueue;                       // Receive dataQueue for RF Core to fill in data
//static rfc_dataEntryGeneral_t* currentDataEntry;
//static uint8_t packetLength;
//static uint8_t* packetDataPointer;

// Prototypes
//static void echoCallback(RF_Handle h, RF_CmdHandle ch, RF_EventMask e);

// Pre-compiler Defines
//#define LOG_RADIO_EVENTS                          // Log radio events in the callback

#ifdef LOG_RADIO_EVENTS
static volatile RF_EventMask eventLog[32];
static volatile uint8_t evIndex = 0;
#endif

const unsigned short txPowerTable[] = {
     0x0041,      //    0dBm
     0x10C3,      //    1dBm
     0x1042,      //    2dBm
     0x14C4,      //    3dBm
     0x18C5,      //    4dBm
     0x18C6,      //    5dBm
     0x1CC7,      //    6dBm
     0x20C9,      //    7dBm
     0x24CB,      //    8dBm
     0x2CCD,      //    9dBm
     0x38D3,      //   10dBm
     0x50DA,      //   11dBm
     0xB818,      //   12dBm
     0xA63F,      //   13dBm
     0xA73F,      //   14dBm
};


/* I2C Configuration */
// -----------------------------------------------------------------------------------------------------
// I2C variables
I2C_Handle          I2cHandle;
I2C_Params          I2cParams;
I2C_Transaction     i2cTransaction;


/* UART Configuration */
// -----------------------------------------------------------------------------------------------------
// Defines
#define UART_READ_DELAY   4                     // 4 seconds

// UART variables
UART_Handle uart;
UART_Params uartParams;
const char  echoPrompt[] = "Detail:";
char        input[10];
uint8_t     uartLineEndCount = 0;



/* GPIO Configuration */
// -----------------------------------------------------------------------------------------------------
// Pin driver handle
static PIN_Handle ledPinHandle;
static PIN_State ledPinState;

// LED Pin Table
PIN_Config pinTable[] =
{
    Board_PIN_LED1 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH | PIN_PUSHPULL | PIN_DRVSTR_MAX,    // Grn Led initially On
    Board_PIN_LED2 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,     // Red Led initially off
    PIN_TERMINATE
};
// WAKE-UP Pin Table
PIN_Config pinTableWakeUp[] = {
    BOARD_HDC_DRDY | PIN_INPUT_EN | PIN_PULLUP | PIN_HYSTERESIS | PINCC26XX_WAKEUP_NEGEDGE,
    PIN_TERMINATE
};
// -----------------------------------------------------------------------------------------------------

/* Flag to store whether we woke up from shutdown or not */
bool isWakingFromShutdown;


#define SENSOR  1






// Function definitions
// *********************************************************************************************************

void *mainThread(void *arg0)
{
    // Get reason for reset - wake from shutdown, POR, etc
    uint32_t rSrc = SysCtrlResetSourceGet();
    if(rSrc == RSTSRC_WAKEUP_FROM_SHUTDOWN){
        isWakingFromShutdown = true;
    }
    else{
        isWakingFromShutdown = false;
    }


    // Open LED pins
    ledPinHandle = PIN_open(&ledPinState, pinTable);
    if (ledPinHandle == NULL)
    {
        while(1);
    }


    if(SENSOR)       // SENSOR
    {

        // I2C COMMS Configuration
        // -----------------------------------------------------------------------------------------------------
        {
            #define I2C_READ_DELAY    5000                  // Delay in us or 5ms
            uint8_t hds_status = 0;

            I2C_init();
            I2C_Params_init(&I2cParams);
            I2cParams.transferMode = I2C_MODE_BLOCKING;
            I2cParams.transferCallbackFxn = NULL;
            I2cParams.bitRate = I2C_400kHz;
            I2cHandle = I2C_open(Board_I2C0, &I2cParams);
            if(I2cHandle == NULL){
               // Error opening I2C
            }
            if(!isWakingFromShutdown)
            {
                sleep(5);
                // Waking from Reset - Initialization of HDC2010
                //HDC2010_peripheral_init();
                I2C_Read(SGP_data,HDC2010_MANUFACTURER_ID_L_REG,2);         // read Product ID (0x4954) to check I2C
                hds_status = HDC2010_config_init();                                      // setup Interrupts and measurement mode
                I2C_Write(0x01,HDC2010_MEAS_CONFIG_REG,2);                  // initiate measurement for first time
                usleep(I2C_READ_DELAY);                                     // N.B too small and DRRDy pin will remain low
                I2C_Read(SGP_data,HDC2010_DRDY_INT_STATUS_REG,1);           // clear existing interrupts
            }

            // HDC Read the 4bytes of Temperature & Relative Humidity data
            if( !I2C_Read(HDC_data,HDC2010_TEMP_REG,4) ){
                // HDC2010 Config failed, load dummy data
                HDC_data[0] = 0xFF;
                HDC_data[1] = 0xFF;
                HDC_data[2] = 0xFF;
                HDC_data[3] = 0xFF;
            }
            I2C_close(I2cHandle);
        }
        // -----------------------------------------------------------------------------------------------------



        /* Radio Packet TX Configuration */
        // -----------------------------------------------------------------------------------------------------
        {
            RF_Params rfParams;
            RF_Params_init(&rfParams);
            rfParams.nInactivityTimeout = 1000;

            RF_cmdPropTx.pktLen = PAYLOAD_LENGTH;
            RF_cmdPropTx.pPkt = txPacket;
            RF_cmdPropTx.startTrigger.triggerType = TRIG_NOW;

            /* Request access to the radio */
            RF_cmdPropRadioDivSetup.txPower =  txPowerTable[14] ;
            rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);

            uint32_t macAddrLsb = HWREG(FCFG1_BASE + FCFG1_O_MAC_15_4_0);       // Get unique lower 16bit of IEEE MAC address as RF ID

            /* Set the frequency */
            RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);
            txPacket[0] = (uint8_t)(0xA5);
            txPacket[1] = (uint8_t)(0xA5);
            txPacket[2] = (macAddrLsb);
            txPacket[3] = (macAddrLsb >> 8);
            txPacket[4] = HW_VER;
            txPacket[5] = FW_VER;
            txPacket[6] = HDC_data[0];
            txPacket[7] = HDC_data[1];
            txPacket[8] = HDC_data[2];
            txPacket[9] = HDC_data[3];
            //txPacket[8] = SGP_data[0];
            //txPacket[9] = SGP_data[1];

            /* Send packet */
            RF_EventMask rfresult = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropTx,RF_PriorityNormal, NULL, 0);
            if (rfresult != RF_EventLastCmdDone)
            {
                while(1); // Error
            }
            /* Power down the radio */
            RF_yield(rfHandle);
        }
        // -----------------------------------------------------------------------------------------------------


        // Grn LED Off - going into shutdown
        PIN_setOutputValue(ledPinHandle, Board_PIN_LED1, 0);

        // Configure GPIO for Wake-up from Shutdown
        PINCC26XX_setWakeup(pinTableWakeUp);

        // Go to Shutdown
        Power_shutdown(0,0);

        // Should never get here!
        //PIN_setOutputValue(ledPinHandle, Board_PIN_LED1, 1);    // Grn LED On - Degging Only
        //PIN_setOutputValue(ledPinHandle, Board_PIN_LED2, 1);    // Red LED On - Degging Only

        while(1);

    }

}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    如果您使用 pinShutdown 示例 、并且仅将 WAKEUP 引脚更改为 DIO_25以在 DIO25上进行测试、您是否仍然看到唤醒问题?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你(们)好

    引脚关断示例工作正常。

    但是、作为起点并不实际。

    *关断示例仅适用于 RTOS。 由于 程序空间限制、我们的项目基于 NORTOS、因此我们根据我的代码片段将 pinShutdown 代码移植到了我们的项目中。

    *此外、无线电处理程序应该比简单的 IOC 唤醒功能更复杂、因此我们认为将回声接收 NORTOS 项目用作关断功能的起始点和端口、而不是相反。

    谢谢

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我没有使用 NORTOS pinShutDown 的经验、因此我建议等待 TI 员工对此进行澄清。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您是否检查了 noRTOS 实现实际上比 RTOS 实现更小的占用空间? 对于后者、某些代码放置在 ROM 中、这实际上可以提供更小的代码大小。

    为什么只有当 oyu 没有从关断状态唤醒时才初始化传感器(第214行):if (!isWakingFromShutdown)

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    只有 RTOS 引脚关断示例、因此无法在代码空间方面进行比较。

    TI 似乎没有提供 NORTOS 示例项目?

    就所需的其他功能(无线电、I2C、UART)而言、是的、我们确信 RTOS 版本更大、不仅大约1.5k、而且在尝试使用32k MCU 时、这一点很重要。

    为了回答您的问题、HDC2010将其所有设置存储在非易失性存储器中。 我们在第一个 POR 上写入这些设置(根据 TI 建议)以自动模式配置传感器、之后以自主方式定期采样、仅在数据准备好以实现绝对最小功耗时将 CC1310从关断状态唤醒。

    传感器基本上提供应用时基。

    如果您将我直接提供的代码片段移植到 EchoRx 示例中、则应该能够相当快速地复制问题。

    我发现它从关断状态唤醒一次这一事实非常奇怪、因为它排除了大多数明显的问题、例如引脚配置错误、或者由于模块仍在运行而实际上未进入关断状态等  

    任何想法/理论都是值得欢迎的

    谢谢

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    H_INT:我不熟悉传感器。 只要已经启动、它是否总是生成一个独立于 CC1310的中断? 如果是、H_INT 信号应每10秒切换一次?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你(们)好

    是的、没错、一旦最初配置为在 POR 上执行此操作、H_INT 将在每个 SamplePeriod 期间从高电平切换到低电平。

    它完全独立于所连接的 MCU。

    示波器跟踪表明、它在 t=20秒时从高电平切换到低电平时正在正确执行此操作...但 CC1310由于某种原因无法唤醒..despite 在 t=10秒时正确唤醒。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    但 H_INT 应该每10秒相等? 如果我正确读取该图、那么事件@10s 与事件@20s 是不同的?

    您是否曾尝试使用按钮按压或类似按钮来更换传感器的 H_INT?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    H_INT 在 t=0、t=10且 t=20时相同、但正确的是、它在图像中不会以这种方式出现。

    原因是示波器时基需要保持较宽的范围以向您显示整个范围。

    在返回 Hi 之前,线路会下降几毫秒,所以在每个分段范围时基(特别是在我昂贵的“汉森”范围内:)的2秒时不可见。

    我确实想用一个按钮来替换传感器、以调试这一点、今天已经没有时间了、明天我将在同一个 Booster 板上使用霍尔传感器进行复制并报告。

    由于没有 RTOS 关断示例、我刚才假定我可以直接将代码移植到 NORTOS 项目。 这是一个公平的假设吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    应该可以: e2e.ti.com/.../cc1310-cc1310-powerdown-with-nortos-standby-mode

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    虽然我不得不承认,我不知道为什么,但通过加入 RF_CLOSE (),我今天还是成功地使它正常工作。

    我曾假设 RF_Yield ()将正确关闭射频内核,确保 CC1310正确进入关断模式。。。因此,IOC 上的唤醒正常,但似乎并非如此。

    对这里实际发生的情况有什么想法?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我假设这是由于以下功率限制:

    Power_setDependency (PowerCC26XX_XOSC_HF)

    执行   RF_CLOCSE ()而不 是 RF_Yield ()时清除该选项