This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHXL-CC1350:交互使用射频和 UART 的一些问题

Guru**** 2927370 points

Other Parts Discussed in Thread: CC1350

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1161270/launchxl-cc1350-some-issue-about-using-rf-and-uart-interactively

器件型号:LAUNCHXL-CC1350
主题中讨论的其他器件:CC1350

大家好、

以下是客户的请求:

客户正在集成 RX 和 UART、主要是为了允许两个器件通过 UART 进行无线通信(UART 输入数据存储在数据包[2]中、 并转换为 INT、然后转换为 TX、RX 位于 callback_packet[2]中)、目前使用 SmartRF stdio 测试 TX 应该没有问题、但 RX 遇到以下问题:

  1. 测试以发送"123456789"、如果在 RX 接收成功时执行 UART_WRITE 的第一个字、则大部分时间都无法接收(客户操作 RX callbaclk 中的 printf 进行测试)。
  2. 目前、RX 结束时间用于关闭 RX、因为先使用 RX、但如果需要 TX、则当前执行的 RX 无法关闭、TX 需要等待接收到 RX 信号。  他们不知道用这个超时关闭 RX 的方法是正确的还是标准的。

程序根据    RfpacketRX 进行修改、 如下图所示:

/***** Includes *****/
/* Standard C Libraries */
#include <stdlib.h>

/* TI Drivers */
#include <ti/drivers/rf/RF.h>
#include <ti/drivers/PIN.h>
#include <ti/drivers/UART.h>
#include <ti/sysbios/knl/Task.h>

/* Driverlib Header files */
#include DeviceFamily_constructPath(driverlib/rf_prop_mailbox.h)

/* Board Header files */
#include "Board.h"

/* Application Header files */
#include "RFQueue.h"
#include "smartrf_settings/smartrf_settings.h"

/***** Defines *****/

/* Packet RX Configuration */
#define DATA_ENTRY_HEADER_SIZE 8 /* Constant header size of a Generic Data Entry */
#define MAX_LENGTH 30 /* Max length byte the radio will accept */
#define NUM_DATA_ENTRIES 2 /* NOTE: Only two data entries supported at the moment */
#define NUM_APPENDED_BYTES 2 /* The Data Entries data field will contain:
* 1 Header byte (RF_cmdPropRx.rxConf.bIncludeHdr = 0x1)
* Max 30 payload bytes
* 1 status byte (RF_cmdPropRx.rxConf.bAppendStatus = 0x1) */

/***** Prototypes *****/
static void callback(RF_Handle h, RF_CmdHandle ch, RF_EventMask e);

/***** Variable declarations *****/
static RF_Object rfObject;
static RF_Handle rfHandle;

/* Pin driver handle */
static PIN_Handle ledPinHandle;
static PIN_State ledPinState;

/* Buffer which contains all Data Entries for receiving data.
* Pragmas are needed to make sure this buffer is 4 byte aligned (requirement from the RF Core) */
#if defined(__TI_COMPILER_VERSION__)
#pragma DATA_ALIGN (rxDataEntryBuffer, 4);
static uint8_t
rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
MAX_LENGTH,
NUM_APPENDED_BYTES)];
#elif defined(__IAR_SYSTEMS_ICC__)
#pragma data_alignment = 4
static uint8_t
rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
MAX_LENGTH,
NUM_APPENDED_BYTES)];
#elif defined(__GNUC__)
static uint8_t
rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
MAX_LENGTH,
NUM_APPENDED_BYTES)]
__attribute__((aligned(4)));
#else
#error This compiler is not supported.
#endif

/* Receive dataQueue for RF Core to fill in data */
/*RX*/
static dataQueue_t dataQueue;
static rfc_dataEntryGeneral_t* currentDataEntry;
static uint8_t packetLength;
static uint8_t* packetDataPointer;
static uint8_t callback_packet[MAX_LENGTH + NUM_APPENDED_BYTES - 1]; /* The length byte is stored in a separate variable */
#define timeout (uint32_t)(4000000*0.1f)
/*RX*/

/*RX Task*/
static Task_Struct rxTask;
#define RX_TASK_STACK_SIZE 1024
static uint8_t rxTaskStack[RX_TASK_STACK_SIZE];
/*RX Task*/

/*TX*/
#define PAYLOAD_LENGTH 30
static uint8_t packet[PAYLOAD_LENGTH];
static uint16_t seqNumber;
int tx_sending = 0;
static uint8_t send_packet[MAX_LENGTH + NUM_APPENDED_BYTES - 1];
/*TX*/

/*TX Task*/
static Task_Struct txTask;
#define TX_TASK_STACK_SIZE 1024
static uint8_t txTaskStack[TX_TASK_STACK_SIZE];
/*TX Task*/

/*Uart*/
UART_Handle uart;
UART_Params uartParams;
char input,output;
/*Uart*/


/*
* Application LED pin configuration table:
* - All LEDs board LEDs are off.
*/
PIN_Config pinTable[] =
{
         Board_PIN_LED1 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
         Board_PIN_LED2 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
         PIN_TERMINATE
};

/***** Function definitions *****/

void led_init()
{
         puts("led_init start");
         ledPinHandle = PIN_open(&ledPinState, pinTable);

         PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,!PIN_getOutputValue(Board_PIN_LED1));
         usleep(300000);
         PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,!PIN_getOutputValue(Board_PIN_LED1));

         PIN_setOutputValue(ledPinHandle, Board_PIN_LED2,!PIN_getOutputValue(Board_PIN_LED2));
         usleep(300000);
         PIN_setOutputValue(ledPinHandle, Board_PIN_LED2,!PIN_getOutputValue(Board_PIN_LED2));

         if (ledPinHandle == NULL)
         {
                  while(1);
         }
}

void rfhandle_init()
{
         puts("rfhandle_init");
         RF_Params rfParams;
         RF_Params_init(&rfParams);

         if( RFQueue_defineQueue(&dataQueue,rxDataEntryBuffer,sizeof(rxDataEntryBuffer),NUM_DATA_ENTRIES,MAX_LENGTH + NUM_APPENDED_BYTES))
         {
                  /* Failed to allocate space for all data entries */
                  while(1);
         }

         rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);

         int i = 0;

         while(i<10)
         {
                  PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,!PIN_getOutputValue(Board_PIN_LED1));
                  usleep(100000);
                  i++;
         }

         PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,0);
}

void callback(RF_Handle h, RF_CmdHandle ch, RF_EventMask e)
{
         if (e & RF_EventRxEntryDone)
         {
                  /* Toggle pin to indicate RX */
                  PIN_setOutputValue(ledPinHandle, Board_PIN_LED2, 1);

                  /* Get current unhandled data entry */
                  currentDataEntry = RFQueue_getDataEntry();

                  /* Handle the packet data, located at &currentDataEntry->data:
                  * - Length is the first byte with the current configuration
                  * - Data starts from the second byte */
                  packetLength = *(uint8_t*)(&currentDataEntry->data);
                  packetDataPointer = (uint8_t*)(&currentDataEntry->data + 1);

                  /* Copy the payload + the status byte to the packet variable */
                  memcpy(callback_packet, packetDataPointer, (packetLength + 1));
                  printf("%d",callback_packet[2]);
                  RFQueue_nextEntry();
         }
}

void rx_init()
{
         puts("rx_init");
         /* Modify CMD_PROP_RX command for application needs */
         /* Set the Data Entity queue for received data */
         RF_cmdPropRx.pQueue = &dataQueue;
         /* Discard ignored packets from Rx queue */
         RF_cmdPropRx.rxConf.bAutoFlushIgnored = 1;
         /* Discard packets with CRC error from Rx queue */
         RF_cmdPropRx.rxConf.bAutoFlushCrcErr = 1;
         /* Implement packet length filtering to avoid PROP_ERROR_RXBUF */
         RF_cmdPropRx.maxPktLen = MAX_LENGTH;
         RF_cmdPropRx.pktConf.bRepeatOk = 0;
         RF_cmdPropRx.endTrigger.triggerType = TRIG_REL_START;
         RF_cmdPropRx.endTime = timeout;

         /* Set the frequency */
         RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);

         while(1)
         {
                  if(tx_sending == 0)
                  {
                           /* Enter RX mode and stay forever in RX */
                           RF_EventMask terminationReason = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropRx,RF_PriorityNormal, &callback,RF_EventRxEntryDone);

                           switch(terminationReason)
                           {
                                    case RF_EventLastCmdDone:
                                             // A stand-alone radio operation command or the last radio
                                             // operation command in a chain finished.
                                             //puts("RF_EventLastCmdDone");
                                             break;
                                    default:
                                             // Uncaught error event
                                             puts("error1");
                                             while(1);
                           }

                           uint32_t cmdStatus = ((volatile RF_Op*)&RF_cmdPropRx)->status;
                           switch(cmdStatus)
                           {
                                    case PROP_DONE_OK:
                                             // Packet received with CRC OK
                                             //puts("PROP_DONE_OK");
                                             PIN_setOutputValue(ledPinHandle, Board_PIN_LED2, 0);

                                             output = callback_packet[2];

                                             UART_write(uart,&output,1);
                                             break;
                                    default:
                                             // Uncaught error event - these could come from the
                                             // pool of states defined in rf_mailbox.h
                                             break;
                           }
                  }
         }
}

void uart_init()
{
         UART_init();

         UART_Params_init(&uartParams);
         uartParams.writeDataMode = UART_DATA_BINARY;
         uartParams.readDataMode = UART_DATA_BINARY;
         uartParams.readReturnMode = UART_RETURN_FULL;
         uartParams.readEcho = UART_ECHO_OFF;
         uartParams.baudRate = 9600;

         uart = UART_open(Board_UART0, &uartParams);

         if (uart == NULL)
         {
                  /* UART_open() failed */
                  while (1);
         }
}

void rx_task_init()
{
         puts("rx_task_init");

         Task_Params rxTaskParams;

         // TI-RTOS 用來初始化 Task_Params 的API ,這邊會給部分變數預設值
         Task_Params_init(&rxTaskParams);
         // 有些變數沒有預設值,必須要自行設定
         rxTaskParams.stack = rxTaskStack; // 規劃給任務使用的Stack位址
         rxTaskParams.stackSize = RX_TASK_STACK_SIZE;
         rxTaskParams.priority = 2; // 任務的優先級,數字越大代表該任務越重要

         Task_construct(&rxTask, rx_init, &rxTaskParams, NULL);
}

void task_init()
{
         puts("tx_init");

         RF_cmdPropTx.pktLen = PAYLOAD_LENGTH;
         RF_cmdPropTx.pPkt = packet;
         RF_cmdPropTx.startTrigger.triggerType = TRIG_NOW;

         while(1)
         {
                  UART_read(uart,&input,1);

                  tx_sending = 1;

                  PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,1);

                  RF_yield(rfHandle);

                  packet[0] = (uint8_t)(seqNumber >> 8);
                  packet[1] = (uint8_t)(seqNumber++);
                  uint8_t i;
                  for (i = 2; i < MAX_LENGTH; i++)
                  {
                           packet[i] = rand();
                  }

                  packet[2] = input;

                  RF_EventMask TXterminationReason = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropTx, RF_PriorityNormal, NULL, 0);

                  switch(TXterminationReason)
                  {
                           case RF_EventLastCmdDone:
                                    //puts("TX RF_EventLastCmdDone");
                                    break;
                           default:
                                    // Uncaught error event
                                    //puts("TX error1");
                                    while(1);
                  }

                  uint32_t TXcmdStatus = ((volatile RF_Op*)&RF_cmdPropTx)->status;
                  switch(TXcmdStatus)
                  {
                           case PROP_DONE_OK:
                                    //puts("TX PROP_DONE_OK");
                                    PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,!PIN_getOutputValue(Board_PIN_LED1));
                                    break;
                           default:
                                    //puts("TX error2");
                                    while(1);
                  }

                  tx_sending = 0;

                  PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,0);
         }
}

void tx_task_init()
{
         puts("tx_task_init");

         Task_Params txTaskParams;

         // TI-RTOS 用來初始化 Task_Params 的API ,這邊會給部分變數預設值
         Task_Params_init(&txTaskParams);
         // 有些變數沒有預設值,必須要自行設定
         txTaskParams.stack = txTaskStack; // 規劃給任務使用的Stack位址
         txTaskParams.stackSize = TX_TASK_STACK_SIZE;
         txTaskParams.priority = 3; // 任務的優先級,數字越大代表該任務越重要

         Task_construct(&txTask, task_init, &txTaskParams, NULL);
}

void *mainThread(void *arg0)
{
         while(ledPinHandle == NULL)
         {
                  led_init();
         }

         while(rfHandle == NULL)
         {
                  rfhandle_init();
         }

         while(uart == NULL)
         {
                  uart_init();
         }

         rx_task_init();

         tx_task_init();
}

您可以帮助检查此案例吗? 谢谢。

此致、                                                             

Nick

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    回调实际上是中断处理。 printf 需要2-3 ms、并将在打印时阻止、不应在回调中使用。 此示例: https://dev.ti.com/tirex/explore/node?node=A__AN.mFk-9oG8Hxbt-NK5NHw__com.ti.SIMPLELINK_CC13XX_CC26XX_SDK__BSEc4rl__LATEST 应该可以移植到 CC1350、或者他们至少应该查看此示例以了解如何执行射频+ UART。 由于许多客户询问此集成、因此添加了此示例。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    在测试您提供的示例时、存在一个小问题。 由于字节 ToRead 设置为64、 因此 UART 回调函数将在 UART 读取64个字后输入。 客户能否根据他输入的字数直接读取它?

    例如、当他输入 ABC 时、三个字将被传输(TX)。 是否有任何简单的示例?

    此致、                                                             

    Nick

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我是否可以知道此问题是否有任何更新?

    此致、                                                             

    Nick

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Nick、

    客户是否尝试更改字节 ToRead 的值?

    此致、

    Arthur