This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHXL-CC1352P:在 Mac OSX 上、simplelink_cc13xx_cc26xx_sdk_6_30_01_03中构建收集器示例失败

Guru**** 1350360 points
Other Parts Discussed in Thread: SYSCONFIG
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1173532/launchxl-cc1352p-building-collector-example-in-simplelink_cc13xx_cc26xx_sdk_6_30_01_03-fails-on-mac-osx

器件型号:LAUNCHXL-CC1352P
Thread 中讨论的其他器件:SysConfigSYSBIOS

尊敬的 TI:

当尝试构建最新的 simplelink SDK simplelink_cc13xx_cc26xx_sdk_6_30_01_03时、我遇到构建故障:

再现:

下载 simplelink SDK https://www.ti.com/tool/download/SIMPLELINK-CC13XX-CC26XX-SDK/6.30.01.03

2.打开 CCS 12.0.0

3.选择 Import CCS Projects

4.选择收集器项目

5.尝试构建

在出现以下错误之前、我在 /Applications/ti/sysconfig_1.14.0/nodejs/node.上遇到了包含的节点二进制文件具有错误权限的问题 我可以通过 chmod +x'ing 二进制文件来解决此问题、但现在遇到了这个问题。

Building target: "collector_CC1352P1_LAUNCHXL_tirtos7_ticlang.out"
Invoking: Arm Linker
"/Applications/ti/ccs1200/ccs/tools/compiler/ti-cgt-armllvm_2.1.0.LTS/bin/tiarmclang" @"/Users/user/workspace_v12/collector_CC1352P1_LAUNCHXL_tirtos7_ticlang/application/defines/collector.opts" @"/Users/user/workspace_v12/collector_CC1352P1_LAUNCHXL_tirtos7_ticlang/Release/syscfg/ti_154stack_config.opts" -mcpu=cortex-m4 -mfloat-abi=hard -mfpu=fpv4-sp-d16 -mlittle-endian -mthumb -Oz -DTIMAC_ROM_IMAGE_BUILD -DBoard_EXCLUDE_NVS_EXTERNAL_FLASH -DDeviceFamily_CC13X2 -gdwarf-3 -fdiagnostics-show-option -fshort-enums -munaligned-access -funsigned-char -fcommon -ffunction-sections -fno-strict-aliasing -march=armv7e-m -Wl,-m"collector_CC1352P1_LAUNCHXL_tirtos7_ticlang.map" -Wl,-i"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source" -Wl,-i"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/kernel/tirtos7/packages" -Wl,-i"/Users/user/workspace_v12/collector_CC1352P1_LAUNCHXL_tirtos7_ticlang/Release/syscfg" -Wl,-i"/Applications/ti/ccs1200/ccs/tools/compiler/ti-cgt-armllvm_2.1.0.LTS/lib" -Wl,--reread_libs -Wl,--define=NVOCMP_NVPAGES=4 -Wl,--define=TIRTOS7 -Wl,--diag_wrap=off -Wl,--display_error_number -Wl,--warn_sections -Wl,--xml_link_info="collector_CC1352P1_LAUNCHXL_tirtos7_ticlang_linkInfo.xml" -Wl,--rom_model -Wl,--unused_section_elimination=on -o "collector_CC1352P1_LAUNCHXL_tirtos7_ticlang.out" "./application/collector/collector.o" "./application/collector/csf.o" "./application/collector/link_controller/cllc.o" "./application/cui/cui.o" "./application/main.o" "./software_stack/ti15_4stack/mac/api_mac.o" "./software_stack/ti15_4stack/mac/macTask.o" "./software_stack/ti15_4stack/mac/low_level/mac_activity.o" "./software_stack/ti15_4stack/mac/mac_settings/mac_cfg.o" "./software_stack/ti15_4stack/mac/mac_settings/mac_settings.o" "./software_stack/ti15_4stack/mac/mac_settings/mac_user_config.o" "./software_stack/ti15_4stack/nv/crc.o" "./software_stack/ti15_4stack/nv/nvocmp.o" "../cc13x2_cc26x2_tirtos7.cmd" -Wl,-l"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/ti154stack/lib/rom/ticlang/timac_rom_PG2_0_rom_api_linker.cmd" -Wl,-lti_utils_build_linker.cmd.genlibs -Wl,-l"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/devices/cc13x2_cc26x2/driverlib/bin/ticlang/driverlib.lib" -Wl,-llibc.a
makefile:170: recipe for target 'collector_CC1352P1_LAUNCHXL_tirtos7_ticlang.out' failed
warning #10210-D: creating ".sysmem" section with default size of 0x800; use the -heap option to change the default size

undefined first referenced
symbol in file
--------- ----------------
AESCCM_config /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<AESCCM.c.obj>
BIOS_start ./application/main.o
Board_init ./application/main.o
Button_config /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<Button.c.obj>
Button_count /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<Button.c.obj>
ClockP_Params_init /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<LED.c.obj>
ClockP_construct /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
ClockP_create /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<LED.c.obj>
ClockP_delete /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<LED.c.obj>
ClockP_destruct /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
ClockP_getCpuFreq /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<UART2CC26X2.c.obj>
ClockP_getSystemTickPeriod /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
ClockP_getSystemTicks /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<Button.c.obj>
ClockP_getTimeout /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
ClockP_isActive /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
ClockP_setTimeout /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
ClockP_start /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
ClockP_stop /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
GPIO_config /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<GPIO.c.obj>
GPIO_pinLowerBound /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<GPIOCC26X2.c.obj>
GPIO_pinUpperBound /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<GPIOCC26X2.c.obj>
HwiP_Params_init /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
HwiP_construct /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
HwiP_destruct /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
HwiP_disable ./application/main.o
HwiP_enableInterrupt /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
HwiP_interruptsEnabled /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<UART2.c.obj>
HwiP_post /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
HwiP_restore ./software_stack/ti15_4stack/mac/macTask.o
HwiP_setFunc /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
HwiP_setPriority /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
LED_config ./application/cui/cui.o
LED_count ./application/cui/cui.o
NVS_config /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<NVS.c.obj>
NVS_count /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<NVS.c.obj>
PowerCC26X2_config /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<PowerCC26X2.c.obj>
RFCC26XX_hwAttrs /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
RF_cmdFs_2gfsk50kbps154g ./software_stack/ti15_4stack/mac/mac_settings/mac_user_config.o
RF_cmdPropCs_2gfsk50kbps154g ./software_stack/ti15_4stack/mac/mac_settings/mac_user_config.o
RF_cmdPropRadioDivSetup_2gfsk50kbps154g ./software_stack/ti15_4stack/mac/mac_settings/mac_user_config.o
RF_cmdPropRxAdv_2gfsk50kbps154g ./software_stack/ti15_4stack/mac/mac_settings/mac_user_config.o
RF_cmdPropTxAdv_2gfsk50kbps154g ./software_stack/ti15_4stack/mac/mac_settings/mac_user_config.o
RF_prop_2gfsk50kbps154g ./software_stack/ti15_4stack/mac/mac_settings/mac_user_config.o
SemaphoreP_Params_init ./application/cui/cui.o
SemaphoreP_construct ./application/cui/cui.o
SemaphoreP_constructBinary /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
SemaphoreP_destruct /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
SemaphoreP_pend ./application/cui/cui.o
SemaphoreP_post ./application/cui/cui.o
SwiP_Params_init /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
SwiP_construct /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
SwiP_destruct /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
SwiP_disable /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
SwiP_getTrigger /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
SwiP_or /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
SwiP_restore /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
SwiP_setPriority /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/rf/lib/ticlang/m4f/rf_multiMode_cc13x2.a<RFCC26X2_multiMode.c.cc13x2.ticlang.o>
SystemP_snprintf ./application/cui/cui.o
SystemP_vsnprintf ./application/cui/cui.o
UART2_config /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<UART2CC26X2.c.obj>
UART2_count /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<UART2CC26X2.c.obj>
UDMACC26XX_config /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/source/ti/drivers/lib/ticlang/m4f/drivers_cc13x2.a<UDMACC26XX.c.obj>
pthread_attr_init ./application/main.o
pthread_attr_setdetachstate ./application/main.o
pthread_attr_setschedparam ./application/main.o
pthread_attr_setstacksize ./application/main.o
pthread_create ./application/main.o
pthread_mutex_init ./software_stack/ti15_4stack/nv/nvocmp.o
pthread_mutex_lock ./software_stack/ti15_4stack/nv/nvocmp.o
pthread_mutex_unlock ./software_stack/ti15_4stack/nv/nvocmp.o
pthread_mutexattr_init ./software_stack/ti15_4stack/nv/nvocmp.o
pthread_self ./software_stack/ti15_4stack/mac/api_mac.o
sem_init ./software_stack/ti15_4stack/mac/api_mac.o
sem_post ./application/collector/csf.o
sem_wait ./software_stack/ti15_4stack/mac/api_mac.o
ti_sysbios_runtime_System_exit /Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_30_01_03/kernel/tirtos7/packages/ti/sysbios/lib/ticlang/m4f/sysbios.a<boot_cortex_m.obj>
txPowerTable_868_pa13 ./software_stack/ti15_4stack/mac/mac_settings/mac_user_config.o

error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "collector_CC1352P1_LAUNCHXL_tirtos7_ticlang.out" not built
tiarmclang: error: tiarmlnk command failed with exit code 1 (use -v to see invocation)
gmake[1]: *** [collector_CC1352P1_LAUNCHXL_tirtos7_ticlang.out] Error 1
gmake: *** [all] Error 2
makefile:166: recipe for target 'all' failed

**** Build Finished

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 CDev:  

    SysConfig 可能未按预期运行、您能否共享整个构建日志?  

    此致、

    SID