This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1101的 RX 灵敏度

Guru**** 2581345 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/569523/rx-sensitivity-of-cc1101

关于   CC1101DK433的射频性能测试, RX 动态范围为0dBm 至-95dbm  (BER  cretiria 为5%)@ 403MHzGFSK76kbaud

但缺点是  、当 RSSI =-76dBmBER 的行为 更糟高达12%时。