This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1310:如何更改频率和其他设置

Guru**** 2555630 points
Other Parts Discussed in Thread: CC1310

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1177612/cc1310-how-to-change-frequency-and-other-settings

器件型号:CC1310

//*********************************************************************************
// Generated by SmartRF Studio version 2.11.0 (build #122)
// Tested for SimpleLink SDK version: CC13x0 SDK 2.30.xx.xx
// Device: CC1310 Rev. 2.1
//
//*********************************************************************************


//*********************************************************************************
// Parameter summary
// Address: 0 
// Address0: 0xAA 
// Address1: 0xBB 
// Frequency: 868.00000 MHz
// Data Format: Serial mode disable 
// Deviation: 25.000 kHz
// pktLen: 30 
// 802.15.4g Mode: 0 
// Select bit order to transmit PSDU octets:: 1 
// Packet Length Config: Variable 
// Max Packet Length: 255 
// Packet Length: 30 
// Packet Data: 255 
// RX Filter BW: 98 kHz
// Symbol Rate: 50.00000 kBaud
// Sync Word Length: 32 Bits 
// TX Power: 14 dBm (requires define CCFG_FORCE_VDDR_HH = 1 in ccfg.c, see CC13xx/CC26xx Technical Reference Manual)
// Whitening: No whitening 


#include <ti/devices/DeviceFamily.h>
#include DeviceFamily_constructPath(driverlib/rf_mailbox.h)
#include DeviceFamily_constructPath(driverlib/rf_common_cmd.h)
#include DeviceFamily_constructPath(driverlib/rf_prop_cmd.h)
#include <ti/drivers/rf/RF.h>
#include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_genfsk.h)
#include DeviceFamily_constructPath(rf_patches/rf_patch_rfe_genfsk.h)
#include "smartrf_settings.h"


// TI-RTOS RF Mode Object
RF_Mode RF_prop =
{
    .rfMode = RF_MODE_PROPRIETARY_SUB_1,
    .cpePatchFxn = &rf_patch_cpe_genfsk,
    .mcePatchFxn = 0,
    .rfePatchFxn = &rf_patch_rfe_genfsk,
};

// Overrides for CMD_PROP_RADIO_DIV_SETUP
uint32_t pOverrides[] =
{
    // override_use_patch_prop_genfsk.xml
    // PHY: Use MCE ROM bank 4, RFE RAM patch
    MCE_RFE_OVERRIDE(0,4,0,1,0,0),
    // override_synth_prop_863_930_div5.xml
    // Synth: Set recommended RTRIM to 7
    HW_REG_OVERRIDE(0x4038,0x0037),
    // Synth: Set Fref to 4 MHz
    (uint32_t)0x000684A3,
    // Synth: Configure fine calibration setting
    HW_REG_OVERRIDE(0x4020,0x7F00),
    // Synth: Configure fine calibration setting
    HW_REG_OVERRIDE(0x4064,0x0040),
    // Synth: Configure fine calibration setting
    (uint32_t)0xB1070503,
    // Synth: Configure fine calibration setting
    (uint32_t)0x05330523,
    // Synth: Set loop bandwidth after lock to 20 kHz
    (uint32_t)0x0A480583,
    // Synth: Set loop bandwidth after lock to 20 kHz
    (uint32_t)0x7AB80603,
    // Synth: Configure VCO LDO (in ADI1, set VCOLDOCFG=0x9F to use voltage input reference)
    ADI_REG_OVERRIDE(1,4,0x9F),
    // Synth: Configure synth LDO (in ADI1, set SLDOCTL0.COMP_CAP=1)
    ADI_HALFREG_OVERRIDE(1,7,0x4,0x4),
    // Synth: Use 24 MHz XOSC as synth clock, enable extra PLL filtering
    (uint32_t)0x02010403,
    // Synth: Configure extra PLL filtering
    (uint32_t)0x00108463,
    // Synth: Increase synth programming timeout (0x04B0 RAT ticks = 300 us)
    (uint32_t)0x04B00243,
    // override_phy_rx_aaf_bw_0xd.xml
    // Rx: Set anti-aliasing filter bandwidth to 0xD (in ADI0, set IFAMPCTL3[7:4]=0xD)
    ADI_HALFREG_OVERRIDE(0,61,0xF,0xD),
    // override_phy_gfsk_rx.xml
    // Rx: Set LNA bias current trim offset to 3
    (uint32_t)0x00038883,
    // Rx: Freeze RSSI on sync found event
    HW_REG_OVERRIDE(0x6084,0x35F1),
    // override_phy_gfsk_pa_ramp_agc_reflevel_0x1a.xml
    // Tx: Configure PA ramping setting (0x41). Rx: Set AGC reference level to 0x1A.
    HW_REG_OVERRIDE(0x6088,0x411A),
    // Tx: Configure PA ramping setting
    HW_REG_OVERRIDE(0x608C,0x8213),
    // override_phy_rx_rssi_offset_5db.xml
    // Rx: Set RSSI offset to adjust reported RSSI by +5 dB (default: 0), trimmed for external bias and differential configuration
    (uint32_t)0x00FB88A3,
#if (CCFG_FORCE_VDDR_HH)
    // TX power override
    // Tx: Set PA trim to max (in ADI0, set PACTL0=0xF8)
    ADI_REG_OVERRIDE(0,12,0xF8),
#endif
    (uint32_t)0xFFFFFFFF,
};


// CMD_PROP_RADIO_DIV_SETUP
rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup =
{
    .commandNo = 0x3807,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .modulation.modType = 0x1,
    .modulation.deviation = 0x64,
    .symbolRate.preScale = 0xF,
    .symbolRate.rateWord = 0x8000,
    .symbolRate.decimMode = 0x0,
    .rxBw = 0x24,
    .preamConf.nPreamBytes = 0x4,
    .preamConf.preamMode = 0x0,
    .formatConf.nSwBits = 0x20,
    .formatConf.bBitReversal = 0x0,
    .formatConf.bMsbFirst = 0x1,
    .formatConf.fecMode = 0x0,
    .formatConf.whitenMode = 0x0,
    .config.frontEndMode = 0x0,
    .config.biasMode = 0x1,
    .config.analogCfgMode = 0x0,
    .config.bNoFsPowerUp = 0x0,
    .txPower = 0xA73F,
    .pRegOverride = pOverrides,
    .centerFreq = 0x0364,
    .intFreq = 0x8000,
    .loDivider = 0x05,
};

// CMD_FS
rfc_CMD_FS_t RF_cmdFs =
{
    .commandNo = 0x0803,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .frequency = 0x0364,
    .fractFreq = 0x0000,
    .synthConf.bTxMode = 0x0,
    .synthConf.refFreq = 0x0,
    .__dummy0 = 0x00,
    .__dummy1 = 0x00,
    .__dummy2 = 0x00,
    .__dummy3 = 0x0000,
};

// CMD_PROP_TX
rfc_CMD_PROP_TX_t RF_cmdPropTx =
{
    .commandNo = 0x3801,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .pktConf.bFsOff = 0x0,
    .pktConf.bUseCrc = 0x1,
    .pktConf.bVarLen = 0x1,
    .pktLen = 0x1E, // SET APPLICATION PAYLOAD LENGTH
    .syncWord = 0x930B51DE,
    .pPkt = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
};

// CMD_PROP_RX
rfc_CMD_PROP_RX_t RF_cmdPropRx =
{
    .commandNo = 0x3802,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .pktConf.bFsOff = 0x0,
    .pktConf.bRepeatOk = 0x0,
    .pktConf.bRepeatNok = 0x0,
    .pktConf.bUseCrc = 0x1,
    .pktConf.bVarLen = 0x1,
    .pktConf.bChkAddress = 0x0,
    .pktConf.endType = 0x0,
    .pktConf.filterOp = 0x0,
    .rxConf.bAutoFlushIgnored = 0x0,
    .rxConf.bAutoFlushCrcErr = 0x0,
    .rxConf.bIncludeHdr = 0x1,
    .rxConf.bIncludeCrc = 0x0,
    .rxConf.bAppendRssi = 0x0,
    .rxConf.bAppendTimestamp = 0x0,
    .rxConf.bAppendStatus = 0x1,
    .syncWord = 0x930B51DE,
    .maxPktLen = 0xFF, // MAKE SURE DATA ENTRY IS LARGE ENOUGH
    .address0 = 0xAA,
    .address1 = 0xBB,
    .endTrigger.triggerType = 0x1,
    .endTrigger.bEnaCmd = 0x0,
    .endTrigger.triggerNo = 0x0,
    .endTrigger.pastTrig = 0x0,
    .endTime = 0x00000000,
    .pQueue = 0, // INSERT APPLICABLE POINTER: (dataQueue_t*)&xxx
    .pOutput = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
};

// CMD_TX_TEST
rfc_CMD_TX_TEST_t RF_cmdTxTest =
{
    .commandNo = 0x0808,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .config.bUseCw = 0x0,
    .config.bFsOff = 0x1,
    .config.whitenMode = 0x2,
    .__dummy0 = 0x00,
    .txWord = 0xABCD,
    .__dummy1 = 0x00,
    .endTrigger.triggerType = 0x1,
    .endTrigger.bEnaCmd = 0x0,
    .endTrigger.triggerNo = 0x0,
    .endTrigger.pastTrig = 0x0,
    .syncWord = 0x930B51DE,
    .endTime = 0x00000000,
};
 

这是我在 CC1310Launchxl 的 rfWsnNode 示例中找到的 smart_settings.c 文件。
现在、我想更改一些数据、我该怎么做?
例如、如果我想达到12dBm、我可以更改什么?
如何更改频率或符号速率?
我是否必须使用 smartRFStudio?
我可以从代码中更改吗?

谢谢你。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您可以直接在代码中更改不同的参数、但需要使用 SmartRF Studio 为不同的参数生成正确的值。

    最简单的方法是使用 SmartRF Studio 生成新设置、然后使用 Studio 中的协同导出功能生成新的设置文件。 请注意、您不能采用 SmartRF Studio 设置、然后仅更改数据速率、并希望其正常工作。 如果更改数据速率、还需要修改偏差和 RX BW。

    此外、从设置文件中可以看到、您正在运行的示例使用的是正常的 TX 和 RX 命令、而不是高级命令。

    这意味着在执行代码导出时、您应该选择也使用正常命令的默认设置之一、并将其用作起点。

    Siri

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Siri、
    感谢您提供的信息。
    我的项目包括许多 TX、用于读取光脉冲并将其发送到集中器。
    我是否正在使用正确的项目?
    我还应该实现高级 TX 和 Rx 命令吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    当示例不使用高级命令时、没有理由实施高级命令。 如果您需要任何仅受高级命令支持的功能、并且需要使用它们、您还需要重新编写应用程序。

    您查看的示例应该非常适合您的应用。

    您还可以考虑使用 TI15.4堆栈下的传感器/收集器示例。

    Siri

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Siri、

    以及如何在最大传输模式下达到433MHz? 目前的最大数据传输速率是多少? 如何借助 SmartRFStudio 实现433MHz 特性? 有示例吗? 非常感谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我会将其重新分配给我们的射频团队:-)

    他们会给你回复

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Vignesh:

    此器件433MHz 频带支持的最高数据速率为50kbps。  我能问您该器件的用例是什么以及您需要多高的数据速率吗?

    下面是如何使用 SmartRF Studio 生成无线电配置代码:

    1. 在"典型设置"目录 中的" 431-527 MHz 频带的设置"下、选择50 kbps。
    2. 在"Frequency"下、选择所需的频率。
    3. 按"Code Export"。

    此致、

    Haiatullah

    此致、

    Haiatullah G.

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    [引用 userid="545176" URL"~/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1177612/cc1310-how-to-change-frequency-and-other-settings/4438598 #4438598"]此器件的433MHz 频带支持的最高数据速率为50kbps。

    这是错误的。 CC1310支持高达约1.5Mbps 的速率(请 参阅 https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/544821/still-remaining-question-maximum-data-rate-of-cc1310-in-the-band-of-433mhz)  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    支持的意思是、虽然器件能够以1.5Mbps 的速率发送和接收数据、但我们尚未对其进行描述。 我们没有此数据速率的官方设置。

    此致、

    Haiatullah

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    与868MHz (.lodiv 除外)相比、433MHz 上是否有设置不同的 phy?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、TheGhostOf、

    是的、433MHz 和868MHz 设置之间的唯一区别(中心频率除外)是.lodiv。 对于433MHz 频带、使用.lodiv 10。 而对于868MHz 频带、则使用.lodiv 5。

    此致、

    Haiatullah

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Haiatullah、

    感谢您的回复。

    用例是发送器应位于阻尼膜内、只有433MHz 的传输才能可靠地通过膜。 由于我们希望传输相对较大的数据(大约200KB - 500KB /秒)、因此高速模式保证1.5Mbps 的数据传输速率、这对我们来说是很有趣的。 它的适用性如何、那么在433MHz 时只能传输50kbps? 我们可以做些什么来实现更高的数据传输速率? 根据 SDK 提供的示例(rfpacketErrorRate)、868MHz 时似乎可以实现这一点。 谢谢你。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Vignesh:

    对于433MHz、我们不支持50kbps 以外的任何其它数据速率。 不过、您可以在 SmartRF Studio 中使用"频率"、"符号速率"、"偏差"和"RX 滤波器 BW"来查找433MHz 设置。 从50kbps 433MHz PHY 开始、并从  500kbps 868MHz PHY 复制各种参数、如"符号速率"、"偏差"和" RX 滤波器 BW"。 我对此进行了快速运行、能够在433MHz 时接收符号速率为500kbps 的数据包。  

    希望这对您有所帮助。

    请注意、

    Haiatullah

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    如果您不知道自己在做什么、请不要"四处走动"。 请参阅 https://www.ti.com/lit/an/swra682/swra682.pdf 获取指示。 要更改为高数据速率、需要更新覆盖项以获得最佳操作、只有更改数据速率才能获得良好的结果。  

    我将采用您想要的868MHz 设置、并仅更改频率和.lodiv。 您需要测试一些器件以验证功能、但这很可能是最安全的方法。