This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LPSTK-CC1352R:双模 Tx 和 Rx

Guru**** 2537450 points
Other Parts Discussed in Thread: CC1352R

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1226051/lpstk-cc1352r-dual-mode-tx-and-rx

器件型号:LPSTK-CC1352R
主题中讨论的其他器件:CC1352R

您好、专家!

目前、我使用的是 CC1352R 定制板、现在我尝试通过 BLE 和低于1GHz 发送数据、因此我只检查双模式 TX/RX 示例、两个 syscfg 文件中都有多个射频和 BLE 选项、 我不明白为什么示例中会出现多个选项、例如射频中的50kbps、200kbps、射频中的5kbps 以及 BLE 中的100kbps、200kbps、

我想知道,所以我只是搜索它,最后,我找到了这个链接

SysConfig 迁移—SimpleLink CC13x2/CC26x2 SDK 专有射频用户指南3.30.00文档

它显示了移民,在这里我有一个怀疑  

1.默认情况下,RF 传输数据时,通过何种设置50kbps、200kbps 或5kbps?

2.如果我使用5kbps 的 RF 数据包 RX 示例,是否可以单独接收射频数据?  

3.是否可以为 BLE 和 RF 选择每一种设置?

4.如果我要选择2.5kbps、我需要在 syscfg 中执行什么操作??

此致

Surya.