This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1352R:GPIO 读取不返回输出引脚的值

Guru**** 2484615 points
Other Parts Discussed in Thread: CC1352R, SYSCONFIG

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1200670/cc1352r-gpio-read-doesn-t-return-the-value-of-an-output-pin

器件型号:CC1352R
"Thread: SysConfig"中讨论的其他器件

大家好!

GPIO_READ ()函数不返回配置为输出的管脚的值?

旧引脚驱动程序具有用于此目的的特定功能、但 GPIO 库中似乎没有该功能。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Thies、

    我刚刚尝试过、它确实使用 GPIO_read 返回正确的状态。 下面是一个基于 timerled 项目的示例、其中 GpioState 是引脚的状态:

    /*
     * Copyright (c) 2016-2020, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    /*
     *  ======== timerled.c ========
     */
    
    #include <stddef.h>
    
    /* Driver Header files */
    #include <ti/drivers/GPIO.h>
    #include <ti/drivers/Timer.h>
    
    /* Board Header file */
    #include "ti_drivers_config.h"
    
    volatile uint_fast8_t GpioState = 0;
    
    /* Callback used for toggling the LED. */
    void timerCallback(Timer_Handle myHandle, int_fast16_t status);
    
    /*
     *  ======== mainThread ========
     */
    void *mainThread(void *arg0)
    {
        Timer_Handle timer0;
        Timer_Params params;
    
        /* Call driver init functions */
        GPIO_init();
        Timer_init();
    
        /* Configure the LED pin */
        GPIO_setConfig(CONFIG_GPIO_LED_0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);
    
        /* Turn off user LED */
        GPIO_write(CONFIG_GPIO_LED_0, CONFIG_GPIO_LED_OFF);
    
        /*
         * Setting up the timer in continuous callback mode that calls the callback
         * function every 1,000,000 microseconds, or 1 second.
         */
        Timer_Params_init(&params);
        params.period        = 1000000;
        params.periodUnits   = Timer_PERIOD_US;
        params.timerMode     = Timer_CONTINUOUS_CALLBACK;
        params.timerCallback = timerCallback;
    
        timer0 = Timer_open(CONFIG_TIMER_0, &params);
    
        if (timer0 == NULL)
        {
            /* Failed to initialized timer */
            while (1) {}
        }
    
        if (Timer_start(timer0) == Timer_STATUS_ERROR)
        {
            /* Failed to start timer */
            while (1) {}
        }
    
        return (NULL);
    }
    
    /*
     * This callback is called every 1,000,000 microseconds, or 1 second. Because
     * the LED is toggled each time this function is called, the LED will blink at
     * a rate of once every 2 seconds.
     */
    void timerCallback(Timer_Handle myHandle, int_fast16_t status)
    {
        GPIO_toggle(CONFIG_GPIO_LED_0);
        GpioState = GPIO_read(CONFIG_GPIO_LED_0);
    }
    

    此致、

    Arthur

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Arthur、您好!

    感谢您的快速回复。

    这仍然不起作用、GipioState 不会改变、我已经添加了一个计数器来显示 LED 的切换次数

    /*
     * Copyright (c) 2016-2020, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    /*
     *  ======== timerled.c ========
     */
    
    #include <stddef.h>
    
    /* Driver Header files */
    #include <ti/drivers/GPIO.h>
    #include <ti/drivers/Timer.h>
    
    /* Board Header file */
    #include "ti_drivers_config.h"
    
    volatile uint_fast8_t GpioState = 0;
    volatile uint8_t counter = 0;
    
    /* Callback used for toggling the LED. */
    void timerCallback(Timer_Handle myHandle, int_fast16_t status);
    
    /*
     *  ======== mainThread ========
     */
    void *mainThread(void *arg0)
    {
        Timer_Handle timer0;
        Timer_Params params;
    
        /* Call driver init functions */
        GPIO_init();
        Timer_init();
    
        /* Configure the LED pin */
        GPIO_setConfig(CONFIG_GPIO_LED_0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);
    
        /* Turn off user LED */
        GPIO_write(CONFIG_GPIO_LED_0, CONFIG_GPIO_LED_OFF);
    
        /*
         * Setting up the timer in continuous callback mode that calls the callback
         * function every 1,000,000 microseconds, or 1 second.
         */
        Timer_Params_init(&params);
        params.period        = 1000000;
        params.periodUnits   = Timer_PERIOD_US;
        params.timerMode     = Timer_CONTINUOUS_CALLBACK;
        params.timerCallback = timerCallback;
    
        timer0 = Timer_open(CONFIG_TIMER_0, &params);
    
        if (timer0 == NULL)
        {
            /* Failed to initialized timer */
            while (1) {}
        }
    
        if (Timer_start(timer0) == Timer_STATUS_ERROR)
        {
            /* Failed to start timer */
            while (1) {}
        }
    
        return (NULL);
    }
    
    /*
     * This callback is called every 1,000,000 microseconds, or 1 second. Because
     * the LED is toggled each time this function is called, the LED will blink at
     * a rate of once every 2 seconds.
     */
    void timerCallback(Timer_Handle myHandle, int_fast16_t status)
    {
        GPIO_toggle(CONFIG_GPIO_LED_0);
        GpioState = GPIO_read(CONFIG_GPIO_LED_0);
        counter++;
    }
    

    但当我进入 GPIO_Read 函数时、可以看到它正在从 GPIO DIN 寄存器读取、但该寄存器在写入或切换后不会更新

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    顺便说一下、我正在使用 SDK6.3

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您可以尝试绘制 GpioState 变量吗?

    我看到状态发生变化、您能否确认您也这么做(或不做)?

    我将使用6.40、但据我所知、GPIO 没有发生任何变化。

    此致、

    Arthur

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    所以我绘制了它、但它仍然保持为零

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    明白了、您能否将经过时间延迟的完整 CCS 项目发送给我?

    顺便说一下、您是使用自定义板还是 Launchpad?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我正在使用一个带有 DIO 15上 LED 的定制电路板

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我仍然看到 GpioState 变量被切换。

    但是、当按下 BTN1 (CC1352R Launchpad 上的 DIO15)时、它会停止切换并保持低电平状态。

    DIO15如何连接到电路板上? 我还建议在 SysConfig 中创建一个定制板、使其不会干扰现有的按钮定义。

    此致、

    Arthur

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、我发现了问题、我们当时正在调试电流消耗问题、发现输入使能位在输出端设置为高电平。 不过、我们制作了自己的位掩码来防止这种情况发生、IE 位必须允许更新 DIN 寄存器、从而将输出读取为输入。 我还忘了恢复 SDK、这就是为什么我有这个问题、我已经恢复了它、读取再次工作。

    很抱歉、感谢您的帮助