您好!
我使用的是高速( 1.5 CC1310上的 Mbps 4-FSK)数据包结构: RFC_CMD_HS_RX_s 和 RFC_CMD_HS_TX_s 。
现在出现的情况是、我的接收对讲机偶尔报告同步字检测、而另一个对讲机没有发射、并且一段时间(例如~10ms)( 请参阅随附的图像。 请注意、显示的信号直接来自射频内核、由 TI 通过覆盖项进行配置:
/* RF Core monitors */
(uint32_t)0x008F88B3, // For RAT_GPO1
// MOD (MCE_GPO0) to RFC_GPO0 DEMOD (MCE_GPO1) to RFC_GPO1 TX (RAT_GPO0) to RFC_GPO2 RX (RAT_GPO1) to RFC_GPO3
HW_REG_OVERRIDE(0x1110, RFC_DBELL_SYSGPOCTL_GPOCTL0_MCEGPO0 | RFC_DBELL_SYSGPOCTL_GPOCTL1_MCEGPO1 | RFC_DBELL_SYSGPOCTL_GPOCTL2_RATGPO0 | RFC_DBELL_SYSGPOCTL_GPOCTL3_RATGPO1),
)。
我没有实现地址滤波、因此我有一个 TI 已定义但无法更改的32位同步字。 因此、我预计平均每2^32 / 1.5 x 10^6次出现伪同步指示= 2863秒 (根据传输占空比进行调整、因此这是一个非常保守的估算值)。 在现实中,这一事件发生在一分钟内开始一个传输/接收序列,占空比约为1:2 (传输:噪音)。
我 可以启用地址过滤、这大概可以解决这个问题、但 a)当我尝试时、 这导致了其他问题(我将在另一个线程中讨论)和 b)由于我不希望经常看到同步字检测这种情况、我显然不明白稍后可能变得很重要的东西(我宁愿理解当前问题而不是简单地解决它)。
HS RX 命令的模板结构:
rfc_CMD_HS_RX_t RF_cmdRxHS =
{
.commandNo = CMD_HS_RX,
.status = 0x0000,
.pNextOp = 0x00000000,
.startTime = 0x00000000,
.startTrigger.triggerType = 0x0,
.startTrigger.bEnaCmd = 0x0,
.startTrigger.triggerNo = 0x0,
.startTrigger.pastTrig = 0x0,
.condition.rule = 0x1,
.condition.nSkip = 0x0,
.pktConf.bFsOff = 0,
.pktConf.bUseCrc = 0,
.pktConf.bVarLen = 0,
.pktConf.bRepeatOk = 0,
.pktConf.bRepeatNok = 0,
.pktConf.addressMode = 0,
.rxConf.bAutoFlushCrcErr = 0,
.rxConf.bIncludeLen = 0,
.rxConf.bIncludeCrc = 0,
.rxConf.bAppendStatus = 0,
.rxConf.bAppendTimestamp = 0,
.maxPktLen = 0,
.address0 = 0,
.address1 = 0,
.__dummy0 = 0,
.endTrigger.triggerType = 1,
.endTrigger.bEnaCmd = 0,
.endTrigger.triggerNo = 0,
.endTrigger.pastTrig = 0,
.endTime = 0,
.pQueue = 0,
.pOutput = 0,
};
PHY 贴片:
// TI-RTOS RF Mode Object (includes patches for high speed operation) // e2e.ti.com/.../2363574 static const RF_Mode RfSettings_RF_prop_hs_4fsk = { .rfMode = RF_MODE_PROPRIETARY_SUB_1, .cpePatchFxn = &rf_patch_cpe_ghs, .mcePatchFxn = &rf_patch_mce_ghs, .rfePatchFxn = &rf_patch_rfe_ghs, };
PHY 基本设置:
// 1.5Mbps // See SVS's post here for these trusted, official settings: // e2e.ti.com/.../2363574 const rfc_CMD_PROP_RADIO_DIV_SETUP_t Cc1310_Rf900vol_PHY_900M_750KSYM_4fsk_g = { // Use Smart RF Studio to generate rxBw, rateWord, deviation and preScale. // Refer to RD1155 Rev 1.1 Section 3.2.4.2 .commandNo = 0x3807, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .modulation.modType = 0x1, .modulation.deviation = 600, .symbolRate.preScale = 8, .symbolRate.rateWord = 262144, .rxBw = 0x30, .preamConf.nPreamBytes = 0x6, .preamConf.preamMode = 0x1, .formatConf.nSwBits = 0x20, .formatConf.bBitReversal = 0x0, .formatConf.bMsbFirst = 0x1, .formatConf.fecMode = 9, .formatConf.whitenMode = 0x0, .config.frontEndMode = 0x0, .config.biasMode = 0x1, .config.frontEndMode = 0x02, // Single-ended Mode RFN. .config.bNoFsPowerUp = 0x0, .txPower = 0x23F, .pRegOverride = (uint32_t*)PHY_900M_4_fsk_pOverrides, .centerFreq = 915, .intFreq = 0x0A66, .loDivider = 0x05, };
PHY 覆盖:
static const uint32_t PHY_900M_4_fsk_pOverrides[] =
{
// PHY: Use MCE RAM patch, RFE RAM patch
MCE_RFE_OVERRIDE(1, 0, 0, 1, 0, 0),
// Rx: Set anti-aliasing filter bandwidth to Maximum
ADI_HALFREG_OVERRIDE(0,61,0xF,0x0),
// Synth: Set recommended RTRIM to 7
HW_REG_OVERRIDE(0x4038,0x0037),
// Synth: Configure fine calibration setting
HW_REG_OVERRIDE(0x4020,0x7F00),
// Synth: Configure fine calibration setting
HW_REG_OVERRIDE(0x4064,0x0040),
// Synth: Set Fref to 4 MHz
(uint32_t)0x000684A3,
// Synth: Configure fine calibration setting
(uint32_t)0xC0040141,
(uint32_t)0x0533B107,
// Synth: Set loop bandwidth after lock
(uint32_t)0xA480583,
(uint32_t)0x7AB80603,
// Synth: Configure VCO LDO (in ADI1, set VCOLDOCFG=0x9F to use voltage input reference)
ADI_REG_OVERRIDE(1,4,0x9F),
// Synth: Configure synth LDO (in ADI1, set SLDOCTL0.COMP_CAP=1)
ADI_HALFREG_OVERRIDE(1,7,0x4,0x4),
// Rx: Set LNA bias current trim offset to 3
(uint32_t)0x00038883,
// Rx: Set RSSI offset to adjust reported RSSI
(uint32_t)0x00FB88A3,
// Synth: Use 24 MHz XOSC as synth clock, enable extra PLL filtering
(uint32_t)0x02010403,
// Synth: Configure extra PLL filtering
(uint32_t)0x00108463,
// Synth: Increase synth programming timeout (0x04B0 RAT ticks = 300 us)
(uint32_t)0x04B00243,
/* #### scc: See software-dl.ti.com/.../packet-format.html
* for a discussion of Sync Words.
*/
//Configure threshold for Sync word detection
HW_REG_OVERRIDE(0x5104,0x302B),
//Set FIFO threshold
(uint32_t) 0x002C82C3,
(uint32_t) 0x002882D3,
// Rx: Do not freeze RSSI on sync found event
HW_REG_OVERRIDE(0x6084,0x25F1),
// ****PA Ramping overrides
HW_REG_OVERRIDE(0x6088,0x4121),
HW_REG_OVERRIDE(0x608C,0x0A12),
// ****Length of CW tone
HW_REG_OVERRIDE(0x52B0,0x00F0),
// DC estimation
HW_REG_OVERRIDE(0x51F8,0x0F90),
//Zero IF in TX
(uint32_t) 0x00000343,
// Tx: Set PA trim to max (in ADI0, set PACTL0=0xF8)
ADI_REG_OVERRIDE(0,12,0xF8),
// Single-ended Operation
ADI_HALFREG_OVERRIDE(0, 16, 0x7, 1), // Output on RFP
/* RF Core monitors */
(uint32_t)0x008F88B3, // For RAT_GPO1
// MOD (MCE_GPO0) to RFC_GPO0 DEMOD (MCE_GPO1) to RFC_GPO1 TX (RAT_GPO0) to RFC_GPO2 RX (RAT_GPO1) to RFC_GPO3
HW_REG_OVERRIDE(0x1110, RFC_DBELL_SYSGPOCTL_GPOCTL0_MCEGPO0 | RFC_DBELL_SYSGPOCTL_GPOCTL1_MCEGPO1 | RFC_DBELL_SYSGPOCTL_GPOCTL2_RATGPO0 | RFC_DBELL_SYSGPOCTL_GPOCTL3_RATGPO1),
// End Override
(uint32_t)0xFFFFFFFF,
};
在发布接收命令之前进行的修改:
if(Cc1310_RfSettings_IsHighSpeedMode() || Cc1310_RfSettings_Is4fskMode()) // High Speed mode
{
/* Configure high speed TX command */
RF_cmdRxHS.pQueue = &RxQueue;
// CRC not applicable, since we are using infinite length transmission mode there is no
// * automatic CRC checking for us
RF_cmdRxHS.pktConf.bUseCrc = 0;
// According to software-dl.ti.com/.../structrfc___c_m_d___h_s___r_x__s.html,
// CC1310 must be considering the packet of VARIABLE length
RF_cmdRxHS.maxPktLen = 16;
RF_cmdRxHS.startTrigger.triggerType = TRIG_NOW;
RF_cmdRxHS.startTrigger.pastTrig = 1;
RF_cmdRxHS.startTime = 0;
RF_cmdRxHS.pOutput = &RxStatsHs;
// RF_cmdRxHS.rxConf.bAppendStatus = 1;
RxOperation = (RF_Op*)&RF_cmdRxHS;
}
else // Standard speed
{
射频队列设置:
static void SetupBlockQueue(uint8_t numBlocks, boolean_t highSpeed)
{
rfc_dataEntryPointer_t* pointerDataEntryPtr;
/* Although the RF core will only receive into a single entry and will
* not automatically move onto the next data entry, RxQueue and Data Entry Queue
* are still apparently necessary to get the RF Core working.
*/
RxQueue.pCurrEntry = RxEntryQueue; // Current entry is the first in the queue
RxQueue.pLastEntry = RxQueue.pCurrEntry;
RxEntryCurrent = (rfc_dataEntryPointer_t*)(RxQueue.pCurrEntry);
// Configuration of generic data entry header
pointerDataEntryPtr = (rfc_dataEntryPointer_t*)RxEntryQueue; // Re-interpretation of simple byte array
pointerDataEntryPtr->status = DATA_ENTRY_PENDING;
pointerDataEntryPtr->config.type = DATA_ENTRY_TYPE_PTR;
// Make the entry exactly the same size as an SPI transaction, thereby forcing the IRQ_RX_ENTRY_DONE interrupt.
pointerDataEntryPtr->length = 16;
// This will return a pointer to either the General Buffer or a Pipeline entry/vacancy.
pointerDataEntryPtr->pData = Cc1310_BbBlocks_GetBufferWrPtr(pointerDataEntryPtr->length, CC1310_BBBLOCKS_REGULAR, CCRF_MODE_RX_BLOCKS);
// Data entry queue is pointless for DATA_ENTRY_TYPE_PTR since pipelining of Rx is not possible for any entry type besides _PARTIAL_
pointerDataEntryPtr->pNextEntry = NULL;
}
接收命令:
RxHandle = RF_postCmd(
Cc1310_CcRf_RfHandle_g,
RxOperation,
RF_PriorityNormal,
&RxBlocksCallback,
RF_EventRxEntryDone
);
当 RxBlocksCallback ()被执行时,我看到 IRQ_RX_ENTRY_DONE 和 IRQ_LAST_COMMAND_DONE 真正的接收时所做的那样。 另外、我进行了一些调试、输出 RxEntryCurrent -> length、指示16个字节、根据我的要求-没有明显的迹象表明出现了任何问题。
我注意到、 https://software-dl.ti.com/simplelink/esd/simplelink_cc13x0_sdk/4.10.02.04/exports/docs/proprietary-rf/proprietary-rf-users-guide/proprietary-rf/packet-format.html 讨论了同步字阈值、这也讨论了设置两个相关器阈值的覆盖、但它没有指示 YY 和 ZZ 值的上限和下限以及它们实际对应的值:
HW_REG_OVERRIDE(0x5104,0x302B)
在32位同步字的上下文中、值0x30 (48)和0x2B (43)的实际含义是什么?
请建议和 TIA、
Sean。