This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1350:对于 CC1350和 CC1352R 无线电900MHz 频段、需要1Mbps 和2Mbps 覆盖、补丁和射频设置的专有模式

Guru**** 2589300 points
Other Parts Discussed in Thread: CC1312R, CC1352R, CC1350, CC1310

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1273439/cc1350-need-1mbps-and-2mbps-overrides-patches-and-rf-settings-for-propriety-mode-for-both-the-cc1350-and-cc1352r-radios-900mhz-bands

器件型号:CC1350
主题中讨论的其他器件:CC1352R、、 CC1310、CC1312R

我一直在寻找开发套件软件包以及这些论坛、为 CC1350和 CC1352R 无线电的专有模式寻找覆盖、补丁和射频设置。  我正在将这些对讲机设置为在900MHz - 930MHz 范围内运行。  您能否为这两个对讲机提供1Mbps 和2Mbps 设置以及相关补丁?

谢谢