This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1352P:可以/如何在写回调函数中关闭 UART2?

Guru**** 2768535 points

Other Parts Discussed in Thread: CC1352P, CC1310

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1298706/cc1352p-possible-how-to-close-uart2-in-write-callback-function

器件型号:CC1352P
主题中讨论的其他器件: CC1310

您好!

我正在 尝试在完成数据发送后关闭 UART 端口、以降低功耗、方法是使用以下代码:

static void uartWriteCallback(UART2_Handle _handle, void *_buf, size_t _size, void *_userArg, int_fast16_t _status)
{
    atUartTxSent += _size;
    if (atUartTxSent < atUartTxLen) {
        UART2_write(atUartHandle, (const void*)&(atUartTxBuff[atUartTxSent]), atUartTxLen - atUartTxSent, NULL);
    } else {
        SemaphoreP_post(atUartTxSem);
        // The following line of code sends system into perpetual reboot
        //atUartClose();
    }
}

static void atUartClose()
{
    if(atUartHandle)
    {
        UART2_readCancel(atUartHandle);
        // TODO: check if the equivalent of the following line is still needed
        //UART2_control(atUartHandle, UART_CMD_RXDISABLE, 0);
        UART2_writeCancel(atUartHandle);
        UART2_close(atUartHandle);
        atUartHandle = NULL;
    }
}

不涉及信号量的类似代码在具有 UART 驱动器的 CC1310/SDK4.2中效果很好。 但在 CC1352P/SDK v7.1中以某种方式调用该函数来关闭 UART 端口会使系统永久重新启动、并且在 CCS 控制台中会出现如下的 NONSTOP 错误消息:

Cortex_M4_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.12.0.00150) 
Cortex_M4_0: Trouble Halting Target CPU: (Error -2062 @ 0x0) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.12.0.00150) 
Cortex_M4_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.12.0.00150) 
Cortex_M4_0: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.12.0.00150) 
Cortex_M4_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.12.0.00150) 
Cortex_M4_0: Trouble Halting Target CPU: (Error -2062 @ 0x0) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.12.0.00150) 

我在这里遗漏了什么? 在写回调函数中删除 semaphore_post ()似乎能够避免永久重新启动,但这种方法有其自己的问题,任何超过 FIFO 缓冲区的数据都不能可靠地发送出去。

建议、谢谢、

ZL

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    UART2_CLOSE()似乎不能从写回调函数调用,尽管它的前一版本 UART_CLOSE()可以。 一旦我们在应用中将该函数从回调函数移动到任务例程、一切似乎都可以正常工作。