This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1352P:FCC 认证所允许的2.4GHz 频段最大传输功率

Guru**** 2481465 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1302274/cc1352p-maximum-allowed-transmission-power-in-2-4ghz-band-for-fcc-certification

器件型号:CC1352P

您好!

当 CC13xx 无线电配置为在900MHz 频段运行时、有关其 FCC 认证的字面量似乎很少。 有人能告诉我他们在2.4GHz 频段的使用和认证相关文献吗?

我假设它们只能配置为在非信标和信标模式下运行、2.4GHz 频段不实现跳频。 我在这里要问的是、数字调制是否在 SDK v7.10中即开即用实现。  

CFR 标题47 15.247状态:

(b)(1) For frequency hopping systems operating in the 2400–2483.5 MHz band employing at least 75 non-overlapping hopping channels, and all frequency hopping systems in the 5725–5850 MHz band: 1 watt. For all other frequency hopping systems in the 2400–2483.5 MHz band: 0.125 watts. 
(b)(3) For systems using digital modulation in the 902–928 MHz, 2400–2483.5 MHz, and 5725–5850 MHz bands: 1 Watt. As an alternative to a peak power measurement, compliance with the one Watt limit can be based on a measurement of the maximum conducted output power. Maximum Conducted Output Power is defined as the total transmit power delivered to all antennas and antenna elements averaged across all symbols in the signaling alphabet when the transmitter is operating at its maximum power control level. Power must be summed across all antennas and antenna elements. The average must not include any time intervals during which the transmitter is off or is transmitting at a reduced power level. If multiple modes of operation are possible (e.g., alternative modulation methods), the maximum conducted output power is the highest total transmit power occurring in any mode. 

如果我们可以在 CCS/SYSCFG 中设置0.15和1瓦的对应功率是多少?

请提供建议、谢谢。

ZL