This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1312R:队列无法删除元素

Guru**** 1379030 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1333776/cc1312r-queue-unable-to-delete-element

器件型号:CC1312R

嗨、大家好:

我正在使用 CC1312 15.4中的最新 SDK

我使用队列。 h 并使用其例程代码、如图所示:

这个示例代码不是问题、但是我的要求是在启动期间将一批数据存储在这个队列中。 因此、我已经对代码进行了以下修改:

但此时、代码将继续循环、而输出值将相同。 应如何解决此问题?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    问题、这是我的代码

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Faker:

    如果你查看 Queue.h、就会发现 Queue_enqueue 中没有发生存储器分配。 这意味着您必须自行分配和取消分配每个元素。

    在您发布的代码中、每个元素都是根据编译器的工作方式引用其自身的。

    以下是工作代码:

    /*
     * Copyright (c) 2015-2019, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     *Redistributions of source code must retain the above copyright
      notice, this list of conditions and the following disclaimer.
     *
     *Redistributions in binary form must reproduce the above copyright
      notice, this list of conditions and the following disclaimer in the
      documentation and/or other materials provided with the distribution.
     *
     *Neither the name of Texas Instruments Incorporated nor the names of
      its contributors may be used to endorse or promote products derived
      from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    /*
    ======== empty.c ========
     */
    
    /* For usleep() */
    #include <unistd.h>
    #include <stdint.h>
    #include <stdlib.h>
    #include <stddef.h>
    
    /* Driver Header files */
    #include <ti/drivers/GPIO.h>
    // #include <ti/drivers/I2C.h>
    // #include <ti/drivers/SPI.h>
    // #include <ti/drivers/Watchdog.h>
    // Import Display Driver definitions
    #include <ti/display/Display.h>
    
    /* Driver configuration */
    #include "ti_drivers_config.h"
    
    #include <ti/sysbios/knl/Queue.h>
    
    typedef struct Rec {
        Queue_Elem _elem;
        int data;
    } Rec;
    
    int mainThread(void)
    {
        Queue_Handle q;
        Rec r1, r2;
        Rec* rp;
        // Initialize optional Display parameters
        Display_Handle    handle;
        Display_Params    params;
        Display_Params_init(&params);
    
        // Open Display implementation
        handle = Display_open(Display_Type_UART, &params);
    
        if (handle == NULL) {
            // Display_open() failed
            while(1);
        }
    
        // create a Queue instance 'q'
        q = Queue_create(NULL, NULL);
    
        for (int i = 0; i < 3; i++)
        {
            Rec *r;
    
            r = malloc(sizeof(Rec));
            r->data = 300 * i;
    
            Queue_enqueue(q, &r->_elem);
        }
    
        // deQ the records and print their data values until Q is empty
        while ((Queue_Handle)(rp = Queue_dequeue(q)) != q) {
            Display_printf(handle, 0, 0, "%d\n", rp->data);
            free(rp);
        }
    
        return (0);
    }
    

    此致、

    亚瑟

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢、正是这个问题