This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1310:射频实际 TX 时间与计算出的时间不匹配

Guru**** 2611695 points
Other Parts Discussed in Thread: CC1310

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1339056/cc1310-rf-actual-tx-time-not-matches-calculated-one

器件型号:CC1310

您好!

我正在 CC1310芯片上解决一些奇怪的行为。 问题是实际传输时间与计算值不符。
我猜问题出在我的公式中、但请帮助我找出我的错误所在。

我正在使用9600波特速度。 数据包配置为:

4字节前导码

2字节同步字

11字节有效载荷(1字节大小+ 10个数据)

2字节 CRC (CRC-16-CCITT)

根据我的计算结果、我将以9600波特传输19个字节、即(19 * 8 / 9600)* 1000000 = 15833us

我将设置延迟的 TX (应发生在定义的时间戳上)并检查与 TX 完成中断时间的差异。 我想应该会有一些小的差异(大约几微秒)、

但结果我得到 879us 的差值、这太大了。  

我还尝试了检查不同的速度、但漂移仍然存在。

附加源代码:

/*
 * rfTxTest.c
 *
 *  Created on: Mar 19, 2024
 *      Author: ArchilPirmisashvili
 */


/***** Includes *****/
/* Standard C Libraries */
#include <stdlib.h>
#include <unistd.h>

/* TI Drivers */
#include <ti/drivers/rf/RF.h>
#include <ti/drivers/PIN.h>
#include <ti/drivers/pin/PINCC26XX.h>
/* Driverlib Header files */
#include DeviceFamily_constructPath(driverlib/rf_prop_mailbox.h)

/* Board Header files */
#include "Board.h"
#include "smartrf_settings/smartrf_settings.h"

#define BYTES_TO_US(x) (((x) + 8) * 8000000U / 9600)

/***** Variable declarations *****/
static RF_Object rfObject;
static RF_Handle rfHandle;

/* Pin driver handle */
static PIN_Handle ledPinHandle;
static PIN_State ledPinState;

static uint8_t tx_packet[] = { 10, 0, 1, 2, 3, 4, 5, 6, 7, 8, 9 };
static uint32_t startTXRatTime;
static uint32_t expectedEndTXRatTime;

int32_t diff = 0;

/*
 * Application LED pin configuration table:
 *   - All LEDs board LEDs are off.
 */
PIN_Config pinTable[] =
{
    Board_PIN_LED1 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    PIN_TERMINATE
};


static void TransmitCallback(RF_Handle h, RF_CmdHandle ch, RF_EventMask e)
{
    diff = RF_convertRatTicksToUs((int32_t)(RF_getCurrentTime() - expectedEndTXRatTime));
}

/***** Function definitions *****/

void *mainThread(void *arg0)
{
    RF_Params rfParams;
    RF_Params_init(&rfParams);

    /* Open LED pins */
    ledPinHandle = PIN_open(&ledPinState, pinTable);
    if (ledPinHandle == NULL)
    {
        while(1);
    }

    /* Set RF transmit indication led */
    PINCC26XX_setMux(ledPinHandle, Board_PIN_LED1, PINCC26XX_MUX_RFC_GPO3);

    /* Request access to the radio */
    rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);

    /* Set the frequency */
    RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);

    startTXRatTime = RF_getCurrentTime() + RF_convertMsToRatTicks(1000);
    /* Total sent bytes: 4 preamble + 2 sync word + 11 payload + 2 CRC = 19 bytes at 9600 = 15833 us */
    expectedEndTXRatTime = startTXRatTime + RF_convertUsToRatTicks(BYTES_TO_US(sizeof(tx_packet)));

    cmdTx.startTime = 0;
    cmdTx.pktLen = (uint16_t)sizeof(tx_packet);
    cmdTx.pPkt = tx_packet;
    cmdTx.startTime = startTXRatTime;
    cmdTx.startTrigger.triggerType = TRIG_ABSTIME;
    RF_postCmd(rfHandle, (RF_Op*) &cmdTx, RF_PriorityNormal, &TransmitCallback, 0);

    while(1)
    {

    }
}

射频配置:

//*********************************************************************************
// Generated by SmartRF Studio version 2.11.0 (build #122)
// Tested for SimpleLink SDK version: CC13x0 SDK 2.30.xx.xx
// Device: CC1310 Rev. 2.1
//
//*********************************************************************************


//*********************************************************************************
// Parameter summary
// Address: 0
// Address0: 0xAA
// Address1: 0xBB
// Frequency: 868.00000 MHz
// Data Format: Serial mode disable
// Deviation: 25.000 kHz
// pktLen: 30
// 802.15.4g Mode: 0
// Select bit order to transmit PSDU octets:: 1
// Packet Length Config: Variable
// Max Packet Length: 255
// Packet Length: 30
// Packet Data: 255
// RX Filter BW: 98 kHz
// Symbol Rate: 50.00000 kBaud
// Sync Word Length: 32 Bits
// TX Power: 14 dBm (requires define CCFG_FORCE_VDDR_HH = 1 in ccfg.c, see CC13xx/CC26xx Technical Reference Manual)
// Whitening: No whitening


#include <ti/devices/DeviceFamily.h>
#include DeviceFamily_constructPath(driverlib/rf_mailbox.h)
#include DeviceFamily_constructPath(driverlib/rf_common_cmd.h)
#include DeviceFamily_constructPath(driverlib/rf_prop_cmd.h)
#include <ti/drivers/rf/RF.h>
#include <ti/devices/cc13x0/inc/hw_rfc_dbell.h>
#include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_genfsk.h)
#include DeviceFamily_constructPath(rf_patches/rf_patch_rfe_genfsk.h)
#include "smartrf_settings.h"


// TI-RTOS RF Mode Object
RF_Mode RF_prop =
{
    .rfMode = RF_MODE_PROPRIETARY_SUB_1,
    .cpePatchFxn = &rf_patch_cpe_genfsk,
    .mcePatchFxn = 0,
    .rfePatchFxn = &rf_patch_rfe_genfsk,
};

// Overrides for CMD_PROP_RADIO_DIV_SETUP
uint32_t pOverrides[] =
{
 // override_use_patch_prop_genfsk.xml
      // PHY: Use MCE ROM bank 4, RFE RAM patch
      MCE_RFE_OVERRIDE(0,4,0,1,0,0),
      // override_synth_prop_430_510_div10.xml
      // Synth: Set recommended RTRIM to 7
      HW_REG_OVERRIDE(0x4038,0x0037),
      // Synth: Set Fref to 4 MHz
      (uint32_t)0x000684A3,
      // Synth: Configure fine calibration setting
      HW_REG_OVERRIDE(0x4020,0x7F00),
      // Synth: Configure fine calibration setting
      HW_REG_OVERRIDE(0x4064,0x0040),
      // Synth: Configure fine calibration setting
      (uint32_t)0xB1070503,
      // Synth: Configure fine calibration setting
      (uint32_t)0x05330523,
      // Synth: Set loop bandwidth after lock to 20 kHz
      (uint32_t)0x0A480583,
      // Synth: Set loop bandwidth after lock to 20 kHz
      (uint32_t)0x7AB80603,
      // Synth: Configure VCO LDO (in ADI1, set VCOLDOCFG=0x9F to use voltage input reference)
      ADI_REG_OVERRIDE(1,4,0x9F),
      // Synth: Configure synth LDO (in ADI1, set SLDOCTL0.COMP_CAP=1)
      ADI_HALFREG_OVERRIDE(1,7,0x4,0x4),
      // Synth: Use 24 MHz XOSC as synth clock, enable extra PLL filtering
      (uint32_t)0x02010403,
      // Synth: Configure extra PLL filtering
      (uint32_t)0x00108463,
      // Synth: Increase synth programming timeout (0x04B0 RAT ticks = 300 us)
      (uint32_t)0x04B00243,
      // override_synth_disable_bias_div10.xml
      // Synth: Set divider bias to disabled
      HW32_ARRAY_OVERRIDE(0x405C,1),
      // Synth: Set divider bias to disabled (specific for loDivider=10)
      (uint32_t)0x18000280,
      // override_phy_rx_aaf_bw_0xd.xml
      // Rx: Set anti-aliasing filter bandwidth to 0xD (in ADI0, set IFAMPCTL3[7:4]=0xD)
      ADI_HALFREG_OVERRIDE(0,61,0xF,0xD),
      // override_phy_gfsk_rx.xml
      // Rx: Set LNA bias current trim offset to 3
      (uint32_t)0x00038883,
      // Rx: Freeze RSSI on sync found event
      HW_REG_OVERRIDE(0x6084,0x35F1),
      // override_phy_gfsk_pa_ramp_agc_reflevel_0x1a.xml
      // Tx: Configure PA ramping setting (0x41). Rx: Set AGC reference level to 0x1A.
      HW_REG_OVERRIDE(0x6088,0x411A),
      // Tx: Configure PA ramping setting
      HW_REG_OVERRIDE(0x608C,0x8213),
      // override_phy_rx_rssi_offset_neg2db.xml
      // Rx: Set RSSI offset to adjust reported RSSI by -2 dB
      (uint32_t)0x000288A3,
      // TX power override
      // Tx: Set PA trim to max (in ADI0, set PACTL0=0xF8)
      ADI_REG_OVERRIDE(0,12,0xF8),
      // Compensate adjustRatTicks
      (uint32_t)((20000 << 16) | 0x02A3), // 48 bit @ 9600 = 5000 us = 20000 RAT ticks
      // Enabling syncword detection
      (uint32_t)0x008F88B3,
      //Configure new CRC16 polynom
      HW32_ARRAY_OVERRIDE(0x2004, 1),
      // The CRC16 polynome: CRC-16-CCITT normal form, 0x1021 is x^16 + x^15 + x^5 + 1
      0x10210000,
      // Configure new CRC init value
      0xC0040051,
      // The new init value
      0x00000000,
      // Set the SYSGPOCTL register
      HW_REG_OVERRIDE(0x1110, (RFC_DBELL_SYSGPOCTL_GPOCTL2_RATGPO1 | RFC_DBELL_SYSGPOCTL_GPOCTL3_MCEGPO0 | RFC_DBELL_SYSGPOCTL_GPOCTL0_CPEGPO0 | RFC_DBELL_SYSGPOCTL_GPOCTL1_CPEGPO1)),
      (uint32_t)0xFFFFFFFF,
};

// CMD_PROP_RADIO_DIV_SETUP
rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup =
{
     .commandNo = 0x3807,
     .status = 0x0000,
     .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)
     .startTime = 0x00000000,
     .startTrigger.triggerType = 0x0,
     .startTrigger.bEnaCmd = 0x0,
     .startTrigger.triggerNo = 0x0,
     .startTrigger.pastTrig = 0x0,
     .condition.rule = 0x1,
     .condition.nSkip = 0x0,
     .modulation.modType = 0x1,
     .modulation.deviation = 0x50,
     .symbolRate.preScale = 0xF,
     .symbolRate.rateWord = 0x1893, //9600 Baud
     .symbolRate.decimMode = 0x0,
     .rxBw = 0x24,
     .preamConf.nPreamBytes = 4,    // 4 Preamble bytes
     .preamConf.preamMode = 0x1,
     .formatConf.nSwBits = 0x10,    // 2 Sync word bytes
     .formatConf.bBitReversal = 0x0,
     .formatConf.bMsbFirst = 0x1,
     .formatConf.fecMode = 0x0,
     .formatConf.whitenMode = 0x0,
     .config.frontEndMode = 0x0,
     .config.biasMode = 0x1,
     .config.analogCfgMode = 0x0,
     .config.bNoFsPowerUp = 0x0,
     .txPower = 0x46CB,
     .pRegOverride = pOverrides,
     .centerFreq = 0x01B1,
     .intFreq = 0x8000,
     .loDivider = 0x0A,
};

// CMD_FS
rfc_CMD_FS_t RF_cmdFs =
{
     .commandNo = 0x0803,
     .status = 0x0000,
     .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)
     .startTime = 0x00000000,
     .startTrigger.triggerType = 0x0,
     .startTrigger.bEnaCmd = 0x0,
     .startTrigger.triggerNo = 0x0,
     .startTrigger.pastTrig = 0x0,
     .condition.rule = 0x0,
     .condition.nSkip = 0x0,
     .frequency = 0x01B1,
     .fractFreq = 0xEB4F,
     .synthConf.bTxMode = 0x0,
     .synthConf.refFreq = 0 ,
     .__dummy0 = 0x00,
     .__dummy1 = 0x00,
     .__dummy2 = 0x00,
     .__dummy3 = 0x0000,
};

rfc_CMD_PROP_TX_ADV_t cmdTx =
{
     .commandNo = 0x3803,
     .status = 0x0000,
     .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)
     .startTime = 0x00000000,
     .startTrigger.triggerType = TRIG_NOW,
     .startTrigger.bEnaCmd = 0x0,
     .startTrigger.triggerNo = 0x0,
     .startTrigger.pastTrig = 0x1,
     .condition.rule = TRIG_NEVER,
     .condition.nSkip = 0x0,
     .pktConf.bFsOff = 0x0,
     .pktConf.bUseCrc = 0x1,
     .pktConf.bCrcIncSw = 0x0,
     .pktConf.bCrcIncHdr = 0x0,
     .numHdrBits = 0x08,
     .pktLen = 0,
     .startConf.bExtTxTrig = 0x0,
     .startConf.inputMode = 0x0,
     .startConf.source = 0x0,
     .preTrigger.triggerType = TRIG_NOW,
     .preTrigger.bEnaCmd = 0x0,
     .preTrigger.triggerNo = 0x0,
     .preTrigger.pastTrig = 0x0,
     .preTime = 0,
     .syncWord = 0x00000000,
};

请提供建议。

提前感谢、

阿奇尔

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Archil:

    为了更准确地测量传播时间、我建议您使用 来自射频内核的 CPE_GPO1信号、该信号在 PA 启用时变为高电平、在禁用时变为低电平。

    您能否将器件配置为向 GPIO 输出 PA 信号、并使用逻辑分析仪或示波器测量该信号为高电平的时间?

    您可以在此处找到有关输出信号的指南: https://software-dl.ti.com/simplelink/esd/simplelink_cc13xx_cc26xx_sdk/5.40.00.40/exports/docs/proprietary-rf/proprietary-rf-users-guide/rf-core/signal-routing.html

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Diego:

    我已经像您说的那样对其进行了配置。 根据示波器测量结果、需要16.6ms。 我应该得到15.833ms。

    在示波器上附加屏幕截图:

    请建议:

    阿奇尔

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Archil:

    实际上、使用以下设置测量了18.3ms:

    此致。

    亚瑟

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Arthur、您好!

    请注意、我使用的 是 CRC-16-CCITT、它是2个字节。 我想您的设置默认配置为32位 CRC。

    根据我的计算、即使有4个字节的 CRC、也需要17.5ms、而不是18.3。 仍然相差约800us、这是相当大的。

    此致、

    阿奇尔

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Archil:

    传输开始时存在一些 LO 泄漏、并且 PA 信号在传输开始之前会稍微开启、之后会稍微开启、从而导致信号显示的时间比应有的长。  不过、实际发送的数据是正确的。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Diego、

    我明白了。 但我的问题是、这种时间差异是恒定的、还是取决于波特率或任何其他参数? 我如何知道/计算这些数字?

    在计算时隙计算所需的实际 TX 时间时隙中我需要的这个值。 例如、如果 TX 时间为20ms、根据计算得出是18ms、则应该会发生冲突。 因此、我需要知道在计算中应增加多少额外时间(尽可能减少这种时间以确保行为正确)。

    提前感谢、

    阿奇尔

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Archil:

    对于相同的 Phy 设置、时间差是常数。 它不随要传输的字节数而变化。 我建议计算时间、使用来自射频内核的 PA 信号或使用零跨度模式的频谱分析仪进行更精确的测量。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢!