This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1310:程序卡在定制电路板上的 RF_pendCmd 处

Guru**** 2609955 points
Other Parts Discussed in Thread: CC1190

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1343823/cc1310-program-stuck-at-rf_pendcmd-on-my-custom-board

器件型号:CC1310
主题中讨论的其他器件:CC1350CC1190

您好!

我有一个基于 LAUNCHXL CC13-90设计的定制电路板。 我一直在尝试使用 rfPacketTx 示例测试电路板、但我的代码挂起于 RF_pendCmd、我在单步执行 RF_runCmd 函数调用时发现了这一点。 具体来说、我发现它在 SemaphoreP_Pend 调用时一直等待。 在使用开发板时、代码运行良好、并且除了 LED 外、我还没有更改自定义板上的任何引脚分配、我已经确认 LED 可以正常工作。

我看到上一个线程建议在调试模式之外为其供电、但似乎没有这样做。 我已通过将其输出到 GPIO 引脚来验证我的32k 时钟是否能正常工作。 我不确定如何测试24M 时钟、但我的设计使用相同的24M 时钟器件、其连接方式也是相同的。 我想不出其他  的方法来解决这个问题,我很感激任何提示。 我已在下面提供了我的 rfPacketTx 代码:

/***** Includes *****/
/* Standard C Libraries */
#include <stdlib.h>
#include <unistd.h>

/* TI Drivers */
#include <ti/drivers/rf/RF.h>
#include <ti/drivers/PIN.h>
#include <ti/drivers/pin/PINCC26XX.h>

/* Driverlib Header files */
#include DeviceFamily_constructPath(driverlib/rf_prop_mailbox.h)

/* Board Header files */
#include "Board.h"
#include "smartrf_settings/smartrf_settings.h"

#include <ti/devices/cc13x0/driverlib/aon_ioc.h>

/***** Defines *****/

/* Do power measurement */
//#define POWER_MEASUREMENT

/* Packet TX Configuration */
#define PAYLOAD_LENGTH      8
#ifdef POWER_MEASUREMENT
#define PACKET_INTERVAL     5  /* For power measurement set packet interval to 5s */
#else
#define PACKET_INTERVAL     500000  /* Set packet interval to 500000us or 500ms */
#endif

#define Board_HGM             CC1310_LAUNCHXL_DIO28_ANALOG
#define Board_LNA_EN          CC1310_LAUNCHXL_DIO29_ANALOG
#define Board_PA_EN           CC1310_LAUNCHXL_DIO30_ANALOG
#define CUSTOM_LED2           CC1310_LAUNCHXL_DIO25_ANALOG

/***** Prototypes *****/

/***** Variable declarations *****/
static RF_Object rfObject;
static RF_Handle rfHandle;

/* Pin driver handle */
static PIN_Handle ledPinHandle;
static PIN_State ledPinState;

static uint8_t packet[PAYLOAD_LENGTH];
static uint16_t seqNumber;

/*
 * Application LED pin configuration table:
 *   - All LEDs board LEDs are off.
 */
PIN_Config pinTable[] =
{
    CUSTOM_LED2 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    Board_HGM | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    Board_LNA_EN | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    Board_PA_EN | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH | PIN_PUSHPULL | PIN_DRVSTR_MAX,
#ifdef POWER_MEASUREMENT
#if defined(Board_CC1350_LAUNCHXL)
    Board_DIO30_SWPWR | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH | PIN_PUSHPULL | PIN_DRVSTR_MAX,
#endif
#endif
    PIN_TERMINATE
};

/***** Function definitions *****/

void *mainThread(void *arg0)
{
    RF_Params rfParams;
    RF_Params_init(&rfParams);

    /* Open LED pins */
    ledPinHandle = PIN_open(&ledPinState, pinTable);
    PINCC26XX_setMux(ledPinHandle, Board_LNA_EN, PINCC26XX_MUX_RFC_GPO0);
    PIN_setOutputValue(ledPinHandle, CUSTOM_LED2,1);
    PINCC26XX_setMux(ledPinHandle, Board_PA_EN, PINCC26XX_MUX_RFC_GPO1);
    if (ledPinHandle == NULL)
    {
        while(1);
    }

    IOCPortConfigureSet(IOID_13, IOC_PORT_AON_CLK32K, IOC_STD_OUTPUT);
    AONIOC32kHzOutputEnable();

#ifdef POWER_MEASUREMENT
#if defined(Board_CC1350_LAUNCHXL)
    /* Route out PA active pin to Board_DIO30_SWPWR */
    PINCC26XX_setMux(ledPinHandle, Board_DIO30_SWPWR, PINCC26XX_MUX_RFC_GPO1);
#endif
#endif

    RF_cmdPropTx.pktLen = PAYLOAD_LENGTH;
    RF_cmdPropTx.pPkt = packet;
    RF_cmdPropTx.startTrigger.triggerType = TRIG_NOW;

    /* Request access to the radio */

    rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);

    /* Set the frequency */
    RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);

    while(1)
    {
        /* Create packet with incrementing sequence number and random payload */
        packet[0] = (uint8_t)(seqNumber >> 8);
        packet[1] = (uint8_t)(seqNumber++);
        uint8_t i;
        for (i = 2; i < PAYLOAD_LENGTH; i++)
        {
            packet[i] = rand();
        }

        /* Send packet */
        RF_EventMask terminationReason = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropTx,
                                                   RF_PriorityNormal, NULL, 0);

        switch(terminationReason)
        {
            case RF_EventLastCmdDone:
                // A stand-alone radio operation command or the last radio
                // operation command in a chain finished.
                break;
            case RF_EventCmdCancelled:
                // Command cancelled before it was started; it can be caused
            // by RF_cancelCmd() or RF_flushCmd().
                break;
            case RF_EventCmdAborted:
                // Abrupt command termination caused by RF_cancelCmd() or
                // RF_flushCmd().
                break;
            case RF_EventCmdStopped:
                // Graceful command termination caused by RF_cancelCmd() or
                // RF_flushCmd().
                break;
            default:
                // Uncaught error event
                while(1);
        }

        uint32_t cmdStatus = ((volatile RF_Op*)&RF_cmdPropTx)->status;
        switch(cmdStatus)
        {
            case PROP_DONE_OK:
                // Packet transmitted successfully
                break;
            case PROP_DONE_STOPPED:
                // received CMD_STOP while transmitting packet and finished
                // transmitting packet
                break;
            case PROP_DONE_ABORT:
                // Received CMD_ABORT while transmitting packet
                break;
            case PROP_ERROR_PAR:
                // Observed illegal parameter
                break;
            case PROP_ERROR_NO_SETUP:
                // Command sent without setting up the radio in a supported
                // mode using CMD_PROP_RADIO_SETUP or CMD_RADIO_SETUP
                break;
            case PROP_ERROR_NO_FS:
                // Command sent without the synthesizer being programmed
                break;
            case PROP_ERROR_TXUNF:
                // TX underflow observed during operation
                break;
            default:
                // Uncaught error event - these could come from the
                // pool of states defined in rf_mailbox.h
                while(1);
        }

#ifndef POWER_MEASUREMENT
        PIN_setOutputValue(ledPinHandle, CUSTOM_LED2,!PIN_getOutputValue(CUSTOM_LED2));
#endif
        /* Power down the radio */
        RF_yield(rfHandle);

#ifdef POWER_MEASUREMENT
        /* Sleep for PACKET_INTERVAL s */
        sleep(PACKET_INTERVAL);
#else
        /* Sleep for PACKET_INTERVAL us */
        usleep(PACKET_INTERVAL);
#endif

    }
}

谢谢!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    当您说您的电路板基于  LAUNCHXL CC13-90时、您意味着什么? 这是设计的副本还是您进行了任何更改? 如果是、会发生哪些变化?

    您是否验证了为 CC1190设置的控制引脚是否按预期工作?

    setup 命令和 FS 命令的状态是什么?

    Siri