This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1352R:在915MHz (低于1GHz)和蓝牙上同时使用 TI 15.4 Stack

Guru**** 2595770 points
Other Parts Discussed in Thread: BLE-STACK

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1393493/cc1352r-use-ti-15-4-stack-at-915mhz-sub-1ghz-and-bluetooth-at-the-same-time

器件型号:CC1352R
Thread 中讨论的其他器件:BLE-STACK

工具与软件:

你(们)好、

我有一个传感器器件、它在915MHz (PHY 132,200kbps)上运行修改版本的 TI 15.4 Stack 传感器应用程序。

是否可以使用同一个器件接收蓝牙信标并同时运行低于1GHz 的应用?

谢谢!

来自 Echo54.