请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TS5A2.3157万-Q1 您好,TI:
我是否可以直接连接IN1和IN2并仅使用一个GPIO切换I2C外壳的通道?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,TI:
我是否可以直接连接IN1和IN2并仅使用一个GPIO切换I2C外壳的通道?

是;请参阅 [FAQ]关于信号开关和多路复用器的更多常见问题。
Junsong您好!
不管怎样, IN1和IN2无疑可以绑定在一起,这只会使两个交换机同时发生变化。 此外,如果您愿意,也可以浮动NC1/2引脚,并且只要这是低频应用,它不会影响您的开关功能(否则建议将它们连接到接地的50欧姆电阻器)。
谢谢!
Bryan