This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMUX1209:如何计算稳定时间

Guru**** 2611705 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/switches-multiplexers-group/switches-multiplexers/f/switches-multiplexers-forum/1049026/tmux1209-how-do-i-calculate-settling-time

器件型号:TMUX1209

您好!

我想计算通道切换时多路复用器的16位稳定时间。 数据表指定了 VDD =5V 时的稳定时间为33ns。  稳定时间的定义为 "转换时间定义为器件输出在地址信号上升或下降超过逻辑阈值后上升或下降10%所需的时间。 10%转换测量被用来提供器件的时序、系统级时序可考虑从负载电阻和负载电容中增加的时间常数"

这是否意味着总稳定时间将为"33ns"+"负载电容和电阻的16位稳定时间"?  或者,我应该 通过考虑 Ron 和负载电路的 CDRAIN 来使用等效时间常数,然后计算16位稳定时间,最后加上33ns?

从16位稳定时间开始、我意味着输出稳定至小于1 LSB 误差(1/2^16)。

谢谢、

Shaury