This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CD4053B-Q1:此器件的电源电压范围是多少? 它可以与3.3V 电源配合使用吗?

Guru**** 2482425 points
Other Parts Discussed in Thread: TIDA-01527

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/switches-multiplexers-group/switches-multiplexers/f/switches-multiplexers-forum/921972/cd4053b-q1-what-is-the-power-supply-range-for-this-device-can-it-work-with-3-3-v-power-supply

器件型号:CD4053B-Q1
主题中讨论的其他器件:TIDA-01527

E2E、  

您能否帮助确认 CD4053-Q1是否可以在3.3V 电源条件下正常工作? 根据数据表、我们可以知道电源电压范围为3V~20V、但我们想与您再次确认、如果在 TIDA-01527系统中使用时、电源电压范围可在3.3V 电源下工作(如下链接所示)

谢谢、

Adam