This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TS3A27518E-Q1:Vcc 为1.8V 时控制输入的最大电压

Guru**** 2511985 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/switches-multiplexers-group/switches-multiplexers/f/switches-multiplexers-forum/928957/ts3a27518e-q1-max-voltage-of-control-inputs-when-vcc-is-1-8v

器件型号:TS3A27518E-Q1

您好!

VCC 为1.8V 时的电压。 控制输入的最大电压是多少:EN~、IN1、IN2。 (1.8V 或3.3V)?

 谢谢!

最棒的

Adam