This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] WL1835MOD:wlcore:启动时出现错误命令完成超时内核错误

Guru**** 2577385 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/1479933/wl1835mod-wlcore-error-command-complete-timeout-kernel-bug-at-startup

器件型号:WL1835MOD

工具与软件:

某些现场单位遇到此问题、以防止不关联。

多次重新启动固件后、如下图所示、固件似乎趋于稳定并与 AP 相关联。  但是、这会对客户体验产生负面影响。  非常感谢任何建议。

[    6.303486] wl18xx_driver wl18xx.0.auto: Direct firmware load for ti-connectivity/wl1271-nvs.bin failed with error -2
[    6.822676] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
[    6.837628] wlcore: loaded
[    7.104155] EXT4-fs: Warning: mounting with data=journal disables delayed allocation and O_DIRECT support!
[   25.080401] wlcore: PHY firmware version: Rev 8.2.0.0.246
[   25.175284] wlcore: firmware booted (Rev 8.9.0.0.90)
[   25.189383] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
[   27.381815] wlcore: ERROR command complete timeout
[   27.381830] ------------[ cut here ]------------
[   27.381984] WARNING: CPU: 0 PID: 275 at drivers/net/wireless/ti/wlcore/main.c:807 wl12xx_queue_recovery_work+0x2c/0x60 [wlcore]
[   27.381991] Modules linked in: wl18xx wlcore sensedaq_driver(O) wlcore_sdio sense_multicolor_led(O)
[   27.382021] CPU: 0 PID: 275 Comm: wpa_supplicant Tainted: G           O      4.19.325-cip116-rt40 #7
[   27.382025] Hardware name: Generic AM33XX (Flattened Device Tree)
[   27.382060] [<c010d798>] (unwind_backtrace) from [<c010b4f8>] (show_stack+0x10/0x14)
[   27.382085] [<c010b4f8>] (show_stack) from [<c0125fcc>] (__warn+0xc0/0xd4)
[   27.382108] [<c0125fcc>] (__warn) from [<c07429c4>] (warn_slowpath_null+0x38/0x48)
[   27.382173] [<c07429c4>] (warn_slowpath_null) from [<bf028c54>] (wl12xx_queue_recovery_work+0x2c/0x60 [wlcore])
[   27.382279] [<bf028c54>] (wl12xx_queue_recovery_work [wlcore]) from [<bf02b790>] (wlcore_cmd_send_failsafe+0x94/0x48c [wlcore])
[   27.382377] [<bf02b790>] (wlcore_cmd_send_failsafe [wlcore]) from [<bf02bba0>] (wl1271_cmd_send+0x18/0x24 [wlcore])
[   27.382475] [<bf02bba0>] (wl1271_cmd_send [wlcore]) from [<bf02d0d4>] (wl1271_cmd_template_set+0xd4/0x114 [wlcore])
[   27.382574] [<bf02d0d4>] (wl1271_cmd_template_set [wlcore]) from [<bf02d224>] (wl12xx_cmd_build_probe_req+0x110/0x14c [wlcore])
[   27.382703] [<bf02d224>] (wl12xx_cmd_build_probe_req [wlcore]) from [<bf05e8bc>] (wl18xx_scan_start+0x1a0/0x260 [wl18xx])
[   27.382795] [<bf05e8bc>] (wl18xx_scan_start [wl18xx]) from [<bf03a13c>] (wlcore_scan+0xc8/0xdc [wlcore])
[   27.382897] [<bf03a13c>] (wlcore_scan [wlcore]) from [<bf0240a8>] (wl1271_op_hw_scan+0xf0/0x120 [wlcore])
[   27.382957] [<bf0240a8>] (wl1271_op_hw_scan [wlcore]) from [<c06e1434>] (__ieee80211_start_scan+0x770/0x808)
[   27.382972] [<c06e1434>] (__ieee80211_start_scan) from [<c06e1fdc>] (ieee80211_request_scan+0x28/0x40)
[   27.382997] [<c06e1fdc>] (ieee80211_request_scan) from [<c06b3d4c>] (nl80211_trigger_scan+0x4d4/0x6bc)
[   27.383014] [<c06b3d4c>] (nl80211_trigger_scan) from [<c055fb80>] (genl_rcv_msg+0x2fc/0x37c)
[   27.383027] [<c055fb80>] (genl_rcv_msg) from [<c055e824>] (netlink_rcv_skb+0xa4/0x10c)
[   27.383037] [<c055e824>] (netlink_rcv_skb) from [<c055f2f0>] (genl_rcv+0x20/0x34)
[   27.383048] [<c055f2f0>] (genl_rcv) from [<c055e030>] (netlink_unicast+0x14c/0x20c)
[   27.383058] [<c055e030>] (netlink_unicast) from [<c055e4cc>] (netlink_sendmsg+0x34c/0x37c)
[   27.383071] [<c055e4cc>] (netlink_sendmsg) from [<c050c198>] (__sock_sendmsg+0x14/0x24)
[   27.383082] [<c050c198>] (__sock_sendmsg) from [<c050c734>] (___sys_sendmsg+0x1dc/0x22c)
[   27.383094] [<c050c734>] (___sys_sendmsg) from [<c050d63c>] (__sys_sendmsg+0x50/0x94)
[   27.383106] [<c050d63c>] (__sys_sendmsg) from [<c0101000>] (ret_fast_syscall+0x0/0x5c)
[   27.383113] Exception stack(0xdab5bfa8 to 0xdab5bff0)
[   27.383124] bfa0:                   00000000 bea30a70 00000006 bea30a70 00000000 00000001
[   27.383135] bfc0: 00000000 bea30a70 00000006 00000128 00000004 bea30af0 00000001 00000000
[   27.383143] bfe0: 00000128 bea30a30 b6c87bc5 b6c12536
[   27.383150] ---[ end trace 0000000000000002 ]---
[   27.383178] wlcore: WARNING cmd set_template failed: -110
[   27.383195] wlcore: ERROR 2.4GHz PROBE request template failed
[   29.051418] sched: RT throttling activated
[   29.051472] wlcore: Hardware recovery in progress. FW ver: Rev 8.9.0.0.90
[   29.102217] wlcore: pc: 0x115616, hint_sts: 0x00000200 count: 1
[   29.102573] wlcore: down
[   29.131916] ieee80211 phy0: Hardware restart was requested
[   29.812218] wlcore: PHY firmware version: Rev 8.2.0.0.246
[   29.875396] wlcore: firmware booted (Rev 8.9.0.0.90)
[   30.718403] wlan0: authenticate with fc:ec:da:a4:d3:58
[   30.762027] wlcore: ERROR SW watchdog interrupt received! starting recovery.
[   30.762043] ------------[ cut here ]------------
[   30.762198] WARNING: CPU: 0 PID: 177 at drivers/net/wireless/ti/wlcore/main.c:807 wl12xx_queue_recovery_work+0x2c/0x60 [wlcore]
[   30.762205] Modules linked in: wl18xx wlcore sensedaq_driver(O) wlcore_sdio sense_multicolor_led(O)
[   30.762235] CPU: 0 PID: 177 Comm: irq/50-wl18xx Tainted: G        W  O      4.19.325-cip116-rt40 #7
[   30.762239] Hardware name: Generic AM33XX (Flattened Device Tree)
[   30.762275] [<c010d798>] (unwind_backtrace) from [<c010b4f8>] (show_stack+0x10/0x14)
[   30.762300] [<c010b4f8>] (show_stack) from [<c0125fcc>] (__warn+0xc0/0xd4)
[   30.762324] [<c0125fcc>] (__warn) from [<c07429c4>] (warn_slowpath_null+0x38/0x48)
[   30.762392] [<c07429c4>] (warn_slowpath_null) from [<bf028c54>] (wl12xx_queue_recovery_work+0x2c/0x60 [wlcore])
[   30.762494] [<bf028c54>] (wl12xx_queue_recovery_work [wlcore]) from [<bf029398>] (wlcore_irq+0xf8/0x170 [wlcore])
[   30.762550] [<bf029398>] (wlcore_irq [wlcore]) from [<c0162190>] (irq_thread_fn+0x1c/0x58)
[   30.762562] [<c0162190>] (irq_thread_fn) from [<c0162404>] (irq_thread+0xdc/0x200)
[   30.762579] [<c0162404>] (irq_thread) from [<c01427e0>] (kthread+0x164/0x17c)
[   30.762594] [<c01427e0>] (kthread) from [<c01010f0>] (ret_from_fork+0x14/0x24)
[   30.762600] Exception stack(0xda20ffb0 to 0xda20fff8)
[   30.762609] ffa0:                                     00000000 00000000 00000000 00000000
[   30.762619] ffc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[   30.762628] ffe0: 00000000 00000000 00000000 00000000 00000013 00000000
[   30.762634] ---[ end trace 0000000000000003 ]---
[   30.762746] wlcore: Hardware recovery in progress. FW ver: Rev 8.9.0.0.90
[   30.763457] wlcore: pc: 0x115616, hint_sts: 0x00000000 count: 2
[   30.763835] wlcore: down
[   30.764016] ieee80211 phy0: Hardware restart was requested
[   30.774427] systemd-journald[136]: Data hash table of /run/log/journal/7c0f5db1e50445ce8b212b67dbbdd37e/system.journal has a fill level at 75.0 (1536 of 2047 items, 1048576 file size, 682 bytes per hash table item), suggesting rotation.
[   30.774478] systemd-journald[136]: /run/log/journal/7c0f5db1e50445ce8b212b67dbbdd37e/system.journal: Journal header limits reached or header out-of-date, rotating.
[   30.791794] wlan0: failed to insert STA entry for the AP (error -16)
[   31.358537] wlcore: PHY firmware version: Rev 8.2.0.0.246
[   31.435461] wlcore: firmware booted (Rev 8.9.0.0.90)