请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:CC3135 Thread 中讨论的其他器件: UNIFLASH
工具/软件:
我正在尝试使用 dslite.bat 将一些虚拟证书加载到 CC3135 (在我们的定制电路板上)。 当我看到 FS_WALTH_SIGNATURE 错误时。
以下是我为我的命令输入的内容和得到的输出:
C:\ti\uniflash_9.0.0>dslite.bat --mode cc32xx image program --file C:\ti\uniflash_9.0.0\prog.sli --port COM4 Executing the following command: > C:\ti\uniflash_9.0.0\simplelink\imagecreator\bin\SLImageCreator.exe image program --file C:\ti\uniflash_9.0.0\prog.sli --port COM4 For more details and examples, please refer to the UniFlash Quick Start guide. INFO:slbootloader.slbootloader:Connecting to device INFO:slbootloader.slbootloader:--- Please power off the device --- Press ENTER to continue INFO:slbootloader.slbootloader:Power off INFO:slbootloader.slbootloader:Set break signal INFO:slbootloader.slbootloader:--- Please power on the device --- INFO:slbootloader.slbootloader:Power on INFO:slbootloader.slbootloader:Clear break signal INFO:slbootloader.slbootloader:Connection succeeded INFO:slbootloader.slbootloader:Received storage list Image Programming: 94% (49152/52000)INFO:slbootloader.slbootloader:Received error : error number = -10289 , extended error = 2694 Traceback (most recent call last): File "SLImageCreator.py", line 5740, in <module> File "SLImageCreator.py", line 5735, in main File "SLImageCreator.py", line 5704, in cmdline File "SLImageCreator.py", line 4482, in command_image_program File "SLImageCreator.py", line 3058, in program_image_from_sli File "SLImageCreator.py", line 3221, in program_image File "slbootloader\slbootloader.py", line 824, in fs_programming slbootloader.slbootloader.BootLoaderError: Error: SLImageCreator.exe: fs_programming error: ret: -10289, ex_err: 2694 - FS_WRONG_SIGNATURE [23816] Failed to execute script 'SLImageCreator' due to unhandled exception!
有关如何解决此问题的任何建议都将非常有用!
谢谢!