This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC3200:什么是 NVIC 待装0-5寄存器位标志?为什么 Pend 5寄存器为0x1000?

Guru**** 2771175 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/1066624/cc3200-what-is-nvic-pend-0-5-registers-bit-signification-and-why-pend-5-register-is-0x1000

部件号:CC3200

您好,

我的问题是,当我打印寄存器 Pend_5的值时,我会得到0x1000和0x800 (有时都是0x1800)
Pend 寄存器用于160到191的中断,这些中断在 hw_ints.h 中定义如下:

//*****************************************************************************
//
// hw_ints.h - Macros that define the interrupt assignment on CC3200.
//
//*****************************************************************************

#ifndef __HW_INTS_H__
#define __HW_INTS_H__

//*****************************************************************************
//
// The following are defines for the fault assignments.
//
//*****************************************************************************
#define FAULT_NMI               2           // NMI fault
#define FAULT_HARD              3           // Hard fault
#define FAULT_MPU               4           // MPU fault
#define FAULT_BUS               5           // Bus fault
#define FAULT_USAGE             6           // Usage fault
#define FAULT_SVCALL            11          // SVCall
#define FAULT_DEBUG             12          // Debug monitor
#define FAULT_PENDSV            14          // PendSV
#define FAULT_SYSTICK           15          // System Tick

//*****************************************************************************
//
// The following are defines for the interrupt assignments.
//
//*****************************************************************************
#define INT_GPIOA0              16          // GPIO Port S0
#define INT_GPIOA1              17          // GPIO Port S1
#define INT_GPIOA2              18          // GPIO Port S2
#define INT_GPIOA3              19          // GPIO Port S3
#define INT_UARTA0              21          // UART0 Rx and Tx
#define INT_UARTA1              22          // UART1 Rx and Tx
#define INT_I2CA0               24          // I2C controller
#define INT_ADCCH0              30          // ADC Sequence 0
#define INT_ADCCH1              31          // ADC Sequence 1
#define INT_ADCCH2              32          // ADC Sequence 2
#define INT_ADCCH3              33          // ADC Sequence 3
#define INT_WDT                 34          // Watchdog Timer0
#define INT_TIMERA0A            35          // Timer 0 subtimer A
#define INT_TIMERA0B            36          // Timer 0 subtimer B
#define INT_TIMERA1A            37          // Timer 1 subtimer A
#define INT_TIMERA1B            38          // Timer 1 subtimer B
#define INT_TIMERA2A            39          // Timer 2 subtimer A
#define INT_TIMERA2B            40          // Timer 2 subtimer B
#define INT_FLASH               45          // FLASH Control
#define INT_TIMERA3A            51          // Timer 3 subtimer A
#define INT_TIMERA3B            52          // Timer 3 subtimer B
#define INT_UDMA                62          // uDMA controller
#define INT_UDMAERR             63          // uDMA Error
#define INT_SHA                 164         // SHA
#define INT_AES                 167         // AES
#define INT_DES                 169         // DES
#define INT_MMCHS               175         // SDIO
#define INT_I2S                 177         // McAPS
#define INT_CAMERA              179         // Camera
#define INT_NWPIC               187         // Interprocessor communication
#define INT_PRCM                188         // Power, Reset and Clock Module
#define INT_SSPI                191         // Shared SPI
#define INT_GSPI                192         // Generic SPI
#define INT_LSPI                193         // Link SPI

//*****************************************************************************
//
// The following are defines for the total number of interrupts.
//
//*****************************************************************************
#define NUM_INTERRUPTS          195 //The above number plus 2?


//*****************************************************************************
//
// The following are defines for the total number of priority levels.
//
//*****************************************************************************
#define NUM_PRIORITY            8
#define NUM_PRIORITY_BITS       3

并且数据表中的 Pend5位0对应于中断160,位31对应于中断191,因此对于0x1000 (即位12),它对应于中断号172,对于0x800 (即位11),它对应于中断号171, 但在.h 文件中,我没有这些中断

我做了一些关于 Pend_x 寄存器位标志的研究,在技术参考手册(链接)的第60页中,我找到了这份中断列表,在.h 文件中发现了这种情况(顺便说一下,标题来自示例)  (我注意到数字被偏移16)因此对于中断171,它是网络中断,但中断号172仍然不存在。  

这就是为什么我在寻找 Pend 0到5寄存器中每个位的正确位标识,特别是 Pend 5 (中断172)中的位12,或者至少是 Pend 5寄存器的值为0x1000的原因?

此致。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这就是 INT_PRCM

    171+16=187 (INT_NWPIC)

    172+16 = 188 (INT_PRCM)

    我不知道为什么这个数字被16位的位移,在待装功能中,我们的位移为16位,但我很确定这是我问题的答案。希望这有一天能帮助别人