This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC3235S:CC3235S 无法通过 SPI 发送和接收数据

Guru**** 2561820 points
Other Parts Discussed in Thread: CC3235S, MSP430FR5969

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/1118566/cc3235s-cc3235s-is-unable-to-transmit-and-receive-data-through-spi

器件型号:CC3235S
主题中讨论的其他器件: MSP430FR5969

我要尝试做的是、我使用寄存器级别(非基于 RTOS)对 MSP430FR5969进行了编程、并使用 TI-RTOS 对另一个 MCU - CC3235S 进行了编程。

我的目标是将数据从 MSP430 (主器件)传输到 CC3235S (从器件)、并从 CC3235S 接收数据。

我在 spimaster  和 spislave 示例中使用的相同方法是

第一个握手,然后准备主器件的 SPI,然后准备从器件的 SPI,当从器件指示 SPI_TRANSLT()值为 true 时,我从 MSP430发送数据。

但是,在使 SPI_TRANSF()正常后,由于数据传输 不正确,SPI 事务未正确进行。

我请求 TI 团队为我提供帮助。

代码-  

MSP430  

#include "driverlib.h"
#include <msp430.h>
int i,j;
char packet[] = {0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x7, 0x08, 0x09, 0x0A, 0x0B , 0x0C, 0x0D, 0x0E, 0x0F};
//char packet[] ={ 'Hello' , 'From', 'Tushar', 'Rathore', 'SAC'};
unsigned char position = 0;

char data = "HELLO ";
//char TxDATA[] ={ 'Hello' , 'From', 'Tushar', 'Rathore', 'SAC'};
int main(void)
{
    WDTCTL = WDTPW | WDTHOLD;   // stop watchdog timer
    FRCTL0 = FRCTLPW | NWAITS_1;
    PM5CTL0 &= ~LOCKLPM5;       // take out GPIO from LPM
    // ----- Setup Button and LED
    P1DIR |= BIT0;      //P1.0 is set as output
    P1OUT &= ~BIT0;     //P1.0 is set at LOW

    P4DIR |= BIT6;      //P4.6 is set as output
    P4OUT &= ~BIT6;     //P4.6 is set at LOW

    P1REN |= BIT1;      //Internal Resistor enable @ P1.1
    P1OUT |= BIT1;      //Pull Up Resistor
    P1IE  |= BIT1;      //Interrupt Enabled
    P1IFG &= ~BIT1;     //Interrupt Flag cleared
    P1IES |= BIT1;      //Interrupt Edge Selection HtoL

    P1DIR |= BIT4;      //P1.4 is set as output
    P1OUT &= ~BIT4;     //P1.4 is set at LOW

    /*    P3DIR &= ~BIT4;      //P3.4 is set as input
    P3REN |= BIT4;      //Internal Resistor enable @ P3.4
    P3OUT |= BIT4;      //Pull Up Resistor
    P3IE  |= BIT4;      //Interrupt Enabled
    P3IFG &= ~BIT4;     //Interrupt Flag cleared
    P3IES &= ~BIT4;      //Interrupt Edge Selection LtoH
*/
    GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P3,GPIO_PIN4);
    GPIO_enableInterrupt(GPIO_PORT_P3,GPIO_PIN4);  //Interrupt Enabled.
    GPIO_clearInterrupt(GPIO_PORT_P3,GPIO_PIN4);  //Interrupt Cleared.
    GPIO_selectInterruptEdge(GPIO_PORT_P3,GPIO_PIN4,GPIO_HIGH_TO_LOW_TRANSITION);  //Interrupt Edge Selection HtoL

    // ----- Setup Clock
    CSCTL0 = CSKEY;             //CSKEY password. Must always be written with A5h
    CSCTL1 = DCORSEL  ;         //DCO range select
    CSCTL1 = DCOFSEL_0;         //DCO frequency select
    CSCTL2 = SELS__DCOCLK  ;    //Selects the SMCLK source
    CSCTL3 = DIVS__1   ;        // SMCLK Source Divider f(SMCLK)/1
    CSCTL0_H = 0;

    // ----- Setup SPI
    UCB0CTLW0 |= UCSWRST ;   // Unlock software reset

    UCB0CTLW0 |=UCSTEM ;
    UCB0CTLW0 |= UCSSEL__SMCLK; // SMCLK as clock source
    UCB0CTLW0 |= UCSYNC;        // Synchronous - SPI Mode
    UCB0CTLW0 |= UCMODE_2;      //
    UCB0CTLW0 |= UCMST;         // SPI Master Mode
    UCB0CTLW0 &= ~UC7BIT;       // 8 BIT Mode
    UCB0CTLW0 |= UCMSB;         // MSB First
    UCB0CTLW0 |= UCCKPL;        // Clock Polarity = 1
    UCB0CTLW0 &= ~ UCCKPH;      // Clock Phase = 0
    UCB0BRW = 0x0010;           // SMCLK/10

    P1SEL1 |= BIT6;             // P1.6 as MOSI Pin
    P1SEL0 &= ~BIT6;

    P1SEL1 |= BIT7;             // P1.7 as MISO Pin
    P1SEL0 &= ~BIT7;

    P2SEL1 |= BIT2;             // P2.2 as SCLK Pin
    P2SEL0 &= ~BIT2;

    UCB0CTLW0 &= ~UCSWRST ;     // Lock software reset

    UCB0IE |= UCTXIE;           // Transmit interrupt enable
    UCB0IFG &= ~UCTXIFG;        // Clear Transmit interrupt flag
    UCB0IE |= UCRXIE;           // Transmit interrupt enable
    UCB0IFG &= ~UCRXIFG;        // Clear Transmit interrupt flag


    while(!(GPIO_getInputPinValue(GPIO_PORT_P3,GPIO_PIN4))){}
    GPIO_setOutputHighOnPin(GPIO_PORT_P1,GPIO_PIN4);

    GPIO_setOutputHighOnPin(GPIO_PORT_P1,GPIO_PIN0);  //LED
    // Handshake done

/*
    for(i=0; i<100; i++){

           while(GPIO_getInputPinValue(GPIO_PORT_P3,GPIO_PIN4)==1){}
            // Slave is ready for transfer (wait for low)

           if(UCTXIFG){
               UCB0TXBUF = data ;
           }
           while(!UCRXIFG){}
           for(j=0; j==1000; j++){}

           P4OUT ^= BIT6;       //Toggle the output @ P4.6

     }

*/
    __enable_interrupt();
    while(1){}

}


#pragma vector = PORT3_VECTOR
__interrupt void PORT_3(void){

 // Slave is ready for transfer (wait for low)

        UCB0TXBUF = packet[i] ;
        i++;

        P1OUT ^= BIT0;       //Toggle the output @ P1.0 (transfer completed)

    P3IFG &= ~BIT4;      //Interrupt Flag cleared
}

CC3235S

/* RTOS header files */
#include <ti/sysbios/BIOS.h>

#include <ti/drivers/Board.h>
#include <stddef.h>
#include <stdbool.h>
#include <stdint.h>
#include <string.h>

/* POSIX Header files */
#include <pthread.h>
#include <semaphore.h>
#include <unistd.h>

/* Driver Header files */
#include <ti/drivers/GPIO.h>
#include <ti/drivers/SPI.h>
#include <ti/display/Display.h>

/* Driver configuration */
#include "ti_drivers_config.h"

#define THREADSTACKSIZE (1024)

#define SPI_MSG_LENGTH  (30)
#define SLAVE_MSG       ("Hello from Slave, msg#: ")

#define MAX_LOOP        (10)

static Display_Handle display;
bool transferStatus;
sem_t slaveSem;
unsigned char slaveRxBuffer[SPI_MSG_LENGTH];
unsigned char slaveTxBuffer[SPI_MSG_LENGTH];

void transferCompleteFxn(SPI_Handle handle, SPI_Transaction *transaction);

void main(void)
{

    SPI_Handle      slaveSpi;
    SPI_Params      spiParams;
    SPI_Transaction transaction;
    uint32_t        i;
    bool            transferOK;
    int32_t         status;

    Board_init();
    Display_init();
    GPIO_init();
    SPI_init();

    display = Display_open(Display_Type_UART, NULL);
    if (display == NULL) {
        /* Failed to open display driver */
        while (1);
    }
    Display_printf(display, 0, 0, "Starting the SPI slave example");


    GPIO_setConfig(CONFIG_SPI_SLAVE_READY, GPIO_CFG_OUTPUT | GPIO_CFG_OUT_LOW);
    GPIO_setConfig(CONFIG_SPI_MASTER_READY, GPIO_CFG_INPUT);

    /*
     * Handshake - Set CONFIG_SPI_SLAVE_READY high to indicate slave is ready
     * to run.  Wait for CONFIG_SPI_MASTER_READY to be high.
     */
    GPIO_write(CONFIG_SPI_SLAVE_READY, 1);
    while (GPIO_read(CONFIG_SPI_MASTER_READY) == 0) {}
    Display_printf(display, 0, 0, "Handshake done !!");

    status = sem_init(&slaveSem, 0, 0);
    if (status != 0) {
        Display_printf(display, 0, 0, "Error creating slaveSem\n");

        while(1);
    }

    SPI_Params_init(&spiParams);
    spiParams.frameFormat = SPI_POL1_PHA0;
    spiParams.mode = SPI_SLAVE;
    spiParams.transferCallbackFxn = transferCompleteFxn;
    spiParams.transferMode = SPI_MODE_CALLBACK;

    slaveSpi = SPI_open(CONFIG_SPI_SLAVE, &spiParams);
    if (slaveSpi == NULL) {
        Display_printf(display, 0, 0, "Error initializing slave SPI\n");
        while (1);
    }
    else {
        Display_printf(display, 0, 0, "Slave SPI initialized\n");
    }

    /* Copy message to transmit buffer */
    //strncpy((char *) slaveTxBuffer, SLAVE_MSG, SPI_MSG_LENGTH);

    for (i = 0; i < MAX_LOOP; i++) {
            /* Initialize slave SPI transaction structure */
           //slaveTxBuffer[sizeof(SLAVE_MSG) - 1] = (i % 10) + '0';
            memset((void *) slaveRxBuffer, 0, SPI_MSG_LENGTH);
            transaction.count = SPI_MSG_LENGTH;
            //transaction.txBuf = (void *) slaveTxBuffer;
            transaction.rxBuf = (void *) slaveRxBuffer;

            /* Toggle on user LED, indicating a SPI transfer is in progress */
             GPIO_toggle(CONFIG_GPIO_LED_1);

            /*
             * Setup SPI transfer; CONFIG_SPI_SLAVE_READY will be set to notify
             * master the slave is ready.
             */
            transferOK = SPI_transfer(slaveSpi, &transaction);
            if (transferOK) {
                Display_printf(display, 0, 0, "Transfer OK : Ready to receive ");
                GPIO_write(CONFIG_SPI_SLAVE_READY, 0);

                Display_printf(display, 0, 0, "sem_wait");
                sem_wait(&slaveSem);
                // callback function will be called

                GPIO_write(CONFIG_SPI_SLAVE_READY, 1);

                if (transferStatus == false) {
                    Display_printf(display, 0, 0, "SPI transfer failed!");
                }
                else {
                    Display_printf(display, 0, 0, "Slave received: %s",
                            slaveRxBuffer);
                }
            }
            else {
                Display_printf(display, 0, 0, "Unsuccessful slave SPI transfer");
            }

    }
        SPI_close(slaveSpi);

        /* Example complete - set pins to a known state */
        GPIO_setConfig(CONFIG_SPI_MASTER_READY, GPIO_CFG_OUTPUT | GPIO_CFG_OUT_LOW);
        GPIO_write(CONFIG_SPI_SLAVE_READY, 0);

        Display_printf(display, 0, 0, "\nDone");

        return (NULL);
}

void transferCompleteFxn(SPI_Handle handle, SPI_Transaction *transaction)
{
    Display_printf(display, 0, 0, "callback fcn called : sem_post");

    if (transaction->status != SPI_TRANSFER_COMPLETED) {
        transferStatus = false;
    }
    else {
        transferStatus = true;
    }
    sem_post(&slaveSem);

}

从器件侧的结果-  

开始 SPI 从器件示例

握手完成!!

从器件 SPI 已初始化

传输正常:准备接收

SEM_WAIT

SPI 传输失败!

从器件 SPI 传输失败

从器件 SPI 传输失败

从器件 SPI 传输失败

从器件 SPI 传输失败

从器件 SPI 传输失败

从器件 SPI 传输失败

从器件 SPI 传输失败

从器件 SPI 传输失败

从器件 SPI 传输失败

完成

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Tushar、

    您是否已验证通过 MSP430 SPI 引脚发送的数据是否有效?

    谢谢、
    Jacob

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你(们)好雅各

    [引用 userid="456020" URL" URL"~支持/无线连接/wi-fi-group/wii/fi-fi-forum/1118566/cc3235s-cc3235s-is-无法发送和接收数据-通过 SPI/4147751#4147751"]您是否已通过 SPI/4147751#4147751"]引用了有效的 SPI/接收数据[?]

    是的、我已经使用示波器验证了数据、在那里我可以看到来自 MSP430的 MOSI 引脚1.6的正确数据。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    嗨、Tushar、

    您发布的此问题似乎已在 此处解决。 这是一个单独的问题吗?

    最棒的
    Jacob  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的,这是一个单独的问题,尚未解决!!!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Tushar、

    您能否从transactionSPI_Transaction结构中的*指针打印状态?  

    谢谢、
    Jacob