Other Parts Discussed in Thread: CC3235S, MSP430FR5969
主题中讨论的其他器件:CC3235S、 MSP430FR5969
您好、TI 团队、
我正在尝试在 MSP430FR5969 (作为主设备)和 CC3235S (作为从设备) Launchpad 之间建立 SPI 通信。
我已使用 spimaster 和 spislave TI-RTOS 示例作为项目的参考。
我的方法如下-
首先、我从两个器件之间的握手开始。
之后,我将在 MSP430处于等待状态时(在 MSP SPI 中是在之前启动的)在 CC3235S 中打开 SPI。
然后,我将向 MSP 发送“保存准备接收”信号。
在接收到上述信号数据传输后、应出现真正 的传输状态、用于显示结果。
问题:
我所面临的问题是,在第一次迭代中,SPI_TRANSF()提供了真值,但数据的传输和接收没有发生,因此也不调用回调函数。
而从第二次迭代 SPI_TRANSF()中,由于没有发生数据传输,因此会给出错误值。
我还在连接代码和输出。
TI 团队能否帮助我尽快解决问题。
/* CC3235S as a Slave */
/* RTOS header files */
#include <ti/sysbios/BIOS.h>
#include <ti/drivers/Board.h>
#include <stddef.h>
#include <stdbool.h>
#include <stdint.h>
#include <string.h>
/* POSIX Header files */
#include <pthread.h>
#include <semaphore.h>
#include <unistd.h>
/* Driver Header files */
#include <ti/drivers/GPIO.h>
#include <ti/drivers/SPI.h>
#include <ti/display/Display.h>
/* Driver configuration */
#include "ti_drivers_config.h"
#define THREADSTACKSIZE (1024)
#define SPI_MSG_LENGTH (30)
#define SLAVE_MSG ("Hello from Slave, msg#: ")
#define MAX_LOOP (10)
static Display_Handle display;
bool transferStatus;
sem_t slaveSem;
unsigned char slaveRxBuffer[SPI_MSG_LENGTH];
unsigned char slaveTxBuffer[SPI_MSG_LENGTH];
void transferCompleteFxn(SPI_Handle handle, SPI_Transaction *transaction);
void main(void)
{
SPI_Handle slaveSpi;
SPI_Params spiParams;
SPI_Transaction transaction;
uint32_t i;
bool transferOK;
int32_t status;
Board_init();
Display_init();
GPIO_init();
SPI_init();
display = Display_open(Display_Type_UART, NULL);
if (display == NULL) {
/* Failed to open display driver */
while (1);
}
Display_printf(display, 0, 0, "Starting the SPI slave example");
GPIO_setConfig(CONFIG_SPI_SLAVE_READY, GPIO_CFG_OUTPUT | GPIO_CFG_OUT_LOW);
GPIO_setConfig(CONFIG_SPI_MASTER_READY, GPIO_CFG_INPUT);
/*
* Handshake - Set CONFIG_SPI_SLAVE_READY high to indicate slave is ready
* to run. Wait for CONFIG_SPI_MASTER_READY to be high.
*/
GPIO_write(CONFIG_SPI_SLAVE_READY, 1);
while (GPIO_read(CONFIG_SPI_MASTER_READY) == 0) {}
Display_printf(display, 0, 0, "Handshake done !!");
status = sem_init(&slaveSem, 0, 0);
if (status != 0) {
Display_printf(display, 0, 0, "Error creating slaveSem\n");
while(1);
}
SPI_Params_init(&spiParams);
spiParams.frameFormat = SPI_POL1_PHA0;
spiParams.mode = SPI_SLAVE;
spiParams.transferCallbackFxn = transferCompleteFxn;
spiParams.transferMode = SPI_MODE_CALLBACK;
slaveSpi = SPI_open(CONFIG_SPI_SLAVE, &spiParams);
if (slaveSpi == NULL) {
Display_printf(display, 0, 0, "Error initializing slave SPI\n");
while (1);
}
else {
Display_printf(display, 0, 0, "Slave SPI initialized\n");
}
/* Copy message to transmit buffer */
//strncpy((char *) slaveTxBuffer, SLAVE_MSG, SPI_MSG_LENGTH);
for (i = 0; i < MAX_LOOP; i++) {
/* Initialize slave SPI transaction structure */
//slaveTxBuffer[sizeof(SLAVE_MSG) - 1] = (i % 10) + '0';
memset((void *) slaveRxBuffer, 0, SPI_MSG_LENGTH);
transaction.count = SPI_MSG_LENGTH;
//transaction.txBuf = (void *) slaveTxBuffer;
transaction.rxBuf = (void *) slaveRxBuffer;
/* Toggle on user LED, indicating a SPI transfer is in progress */
GPIO_toggle(CONFIG_GPIO_LED_1);
/*
* Setup SPI transfer; CONFIG_SPI_SLAVE_READY will be set to notify
* master the slave is ready.
*/
transferOK = SPI_transfer(slaveSpi, &transaction);
if (transferOK) {
Display_printf(display, 0, 0, "Transfer OK : Ready to receive ");
GPIO_write(CONFIG_SPI_SLAVE_READY, 0);
Display_printf(display, 0, 0, "sem_wait");
sem_wait(&slaveSem);
// callback function will be called
GPIO_write(CONFIG_SPI_SLAVE_READY, 1);
if (transferStatus == false) {
Display_printf(display, 0, 0, "SPI transfer failed!");
}
else {
Display_printf(display, 0, 0, "Slave received: %s",
slaveRxBuffer);
}
}
else {
Display_printf(display, 0, 0, "Unsuccessful slave SPI transfer");
}
}
SPI_close(slaveSpi);
/* Example complete - set pins to a known state */
GPIO_setConfig(CONFIG_SPI_MASTER_READY, GPIO_CFG_OUTPUT | GPIO_CFG_OUT_LOW);
GPIO_write(CONFIG_SPI_SLAVE_READY, 0);
Display_printf(display, 0, 0, "\nDone");
return (NULL);
}
void transferCompleteFxn(SPI_Handle handle, SPI_Transaction *transaction)
{
Display_printf(display, 0, 0, "callback fcn called : sem_post");
if (transaction->status != SPI_TRANSFER_COMPLETED) {
transferStatus = false;
}
else {
transferStatus = true;
}
sem_post(&slaveSem);
}
/*MSP430FR5969 as a Master */
#include "driverlib.h"
#include <msp430.h>
int i,j;
char packet[] = {0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x7, 0x08, 0x09, 0x0A, 0x0B , 0x0C, 0x0D, 0x0E, 0x0F};
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer
FRCTL0 = FRCTLPW | NWAITS_1;
PM5CTL0 &= ~LOCKLPM5; // take out GPIO from LPM
// ----- Setup Button and LED
P1DIR |= BIT0; //P1.0 is set as output
P1OUT &= ~BIT0; //P1.0 is set at LOW
P4DIR |= BIT6; //P4.6 is set as output
P4OUT &= ~BIT6; //P4.6 is set at LOW
P1REN |= BIT1; //Internal Resistor enable @ P1.1
P1OUT |= BIT1; //Pull Up Resistor
P1IE |= BIT1; //Interrupt Enabled
P1IFG &= ~BIT1; //Interrupt Flag cleared
P1IES |= BIT1; //Interrupt Edge Selection HtoL
P1DIR |= BIT4; //P1.4 is set as output
P1OUT &= ~BIT4; //P1.4 is set at LOW
/* P3DIR &= ~BIT4; //P3.4 is set as input
P3REN |= BIT4; //Internal Resistor enable @ P3.4
P3OUT |= BIT4; //Pull Up Resistor
P3IE |= BIT4; //Interrupt Enabled
P3IFG &= ~BIT4; //Interrupt Flag cleared
P3IES &= ~BIT4; //Interrupt Edge Selection LtoH
*/
GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P3,GPIO_PIN4);
GPIO_enableInterrupt(GPIO_PORT_P3,GPIO_PIN4); //Interrupt Enabled.
GPIO_clearInterrupt(GPIO_PORT_P3,GPIO_PIN4); //Interrupt Cleared.
GPIO_selectInterruptEdge(GPIO_PORT_P3,GPIO_PIN4,GPIO_HIGH_TO_LOW_TRANSITION); //Interrupt Edge Selection HtoL
// ----- Setup Clock
CSCTL0 = CSKEY; //CSKEY password. Must always be written with A5h
CSCTL1 = DCORSEL ; //DCO range select
CSCTL1 = DCOFSEL_0; //DCO frequency select
CSCTL2 = SELS__DCOCLK ; //Selects the SMCLK source
CSCTL3 = DIVS__1 ; // SMCLK Source Divider f(SMCLK)/1
CSCTL0_H = 0;
// ----- Setup SPI
UCB0CTLW0 |= UCSWRST ; // Unlock software reset
UCB0CTLW0 |=UCSTEM ;
UCB0CTLW0 |= UCSSEL__SMCLK; // SMCLK as clock source
UCB0CTLW0 |= UCSYNC; // Synchronous - SPI Mode
UCB0CTLW0 |= UCMODE_2; //
UCB0CTLW0 |= UCMST; // SPI Master Mode
UCB0CTLW0 &= ~UC7BIT; // 8 BIT Mode
UCB0CTLW0 |= UCMSB; // MSB First
UCB0CTLW0 |= UCCKPL; // Clock Polarity = 1
UCB0CTLW0 &= ~ UCCKPH; // Clock Phase = 0
UCB0BRW = 0x0010; // SMCLK/10
P1SEL1 |= BIT6; // P1.6 as MOSI Pin
P1SEL0 &= ~BIT6;
P1SEL1 |= BIT7; // P1.7 as MISO Pin
P1SEL0 &= ~BIT7;
P2SEL1 |= BIT2; // P2.2 as SCLK Pin
P2SEL0 &= ~BIT2;
UCB0CTLW0 &= ~UCSWRST ; // Lock software reset
UCB0IE |= UCTXIE; // Transmit interrupt enable
UCB0IFG &= ~UCTXIFG; // Clear Transmit interrupt flag
UCB0IE |= UCRXIE; // Transmit interrupt enable
UCB0IFG &= ~UCRXIFG; // Clear Transmit interrupt flag
while(!(GPIO_getInputPinValue(GPIO_PORT_P3,GPIO_PIN4))){}
GPIO_setOutputHighOnPin(GPIO_PORT_P1,GPIO_PIN4);
GPIO_setOutputHighOnPin(GPIO_PORT_P1,GPIO_PIN0); //LED
// Handshake done
__enable_interrupt();
while(1){}
}
#pragma vector = PORT3_VECTOR
__interrupt void PORT_3(void){
// Slave is ready for transfer (wait for low)
UCB0TXBUF = packet[i] ;
i++;
P1OUT ^= BIT0; //Toggle the output @ P1.0 (transfer completed)
P3IFG &= ~BIT4; //Interrupt Flag cleared
}
结果-
|
开始 SPI 从器件示例 握手完成!! 从器件 SPI 已初始化 传输正常:准备接收 SEM_WAIT SPI 传输失败! 从器件 SPI 传输失败 从器件 SPI 传输失败 从器件 SPI 传输失败 从器件 SPI 传输失败 从器件 SPI 传输失败 从器件 SPI 传输失败 从器件 SPI 传输失败 从器件 SPI 传输失败 从器件 SPI 传输失败 完成 |
此致-
Tushar Rathore