This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC3220S:次级引导加载程序(SDK2.10)无法与新版本的应用程序(SDK6.10)配合使用

Guru**** 2811595 points

Other Parts Discussed in Thread: CC3220S

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/1118631/cc3220s-secondary-bootloader-sdk2-10-cannot-work-with-new-version-of-application-sdk6-10

器件型号:CC3220S

客户在 CC3220S 上开发了一个次级引导加载程序、如所述的相关博文 SDK2.10、并且运行良好。 现在、该应用程序已使用 SDK6.10进行更新、但更新后的应用程序无法使用旧的引导加载程序。

新应用程序和旧应用程序都使用相同的 CMD 文件、如下所示。

/*
 * Copyright (c) 2016, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

/*
 *  ======== CC3220S_LAUNCHXL.cmd ========
 */

/*
 * The starting address of the application.  Normally the interrupt vectors
 * must be located at the beginning of the application.
 */
  /*
#define SRAM_BASE 0x20004000
#define SRAM0_BASE 0x20000000

#define SRAM_BASE 0x2001E800
#define SRAM0_BASE 0x20000000
*/
//#define SRAM_BASE 0x20004000
#define SRAM_BASE 0x2001E800
#define SRAM0_BASE 0x20000000

--stack_size=1024   /* C stack is also used for ISR stack */

HEAPSIZE = 0x8000;  /* Size of heap buffer used by HeapMem */

MEMORY
{
/*
    SRAM0 (RWX) : origin = 0x20000000, length = 0x4000
    SRAM  (RWX) : origin = 0x20004000, length = 0x00040000 - 0x4000

        SRAM0 (RWX) : origin = 0x2001A400, length = 0x4000
    SRAM  (RWX) : origin = 0x2001E400, length = 0x00025C00 - 0x4000

    SRAM0 (RWX) : origin = 0x20004000, length = 0x4000
    SRAM  (RWX) : origin = 0x20008000, length = 0x00025C00

    SRAM0 (RWX) : origin = 0x20000000, length = 0x4000
    SRAM  (RWX) : origin = 0x20008000, length = 0x00025C00

    SRAM0 (RWX) : origin = 0x20000000, length = 0x4000
    SRAM  (RWX) : origin = 0x2001E800, length = 0x00040000 - 0x1E800
     */

    SRAM0 (RWX) : origin = 0x20000000, length =  0x1E800
    SRAM  (RWX) : origin = 0x2001E800, length = 0x00040000 - 0x1E800
}

/* Section allocation in memory */
/*
SECTIONS
{
    .text       : > SRAM
    .bss        : > SRAM
    .TI.ramfunc : > SRAM
    .data       : > SRAM
    .const      : > SRAM

    .sysmem     : > SRAM
    .cinit      : > SRAM
    .pinit      : > SRAM
    .init_array : > SRAM

    /* Heap buffer used by HeapMem
    .priheap    : {
        __primary_heap_start__ = .;
        . += HEAPSIZE;
        __primary_heap_end__ = .;
    } > SRAM align 8

    .stack      : > SRAM0(HIGH)
}
*/

SECTIONS
{
    .intvecs:   > SRAM_BASE
    .init_array : > SRAM
    .vtable :   > SRAM
    .text   :   > SRAM
    .const  :   > SRAM
    .cinit  :   > SRAM
    .pinit  :   > SRAM
    .data   :   > SRAM0
    .bss    :   > SRAM0
    .sysmem :   > SRAM0
    .priheap    : {
        __primary_heap_start__ = .;
        . += HEAPSIZE;
        __primary_heap_end__ = .;
    } > SRAM align 8
    .stack  :   > SRAM0(HIGH)
}

次级引导加载程序加载到0x20004000、应用程序从0x2001E800启动。 次级引导加载程序负责跳转到相关帖子中所述的应用程序。

使用默认 CMD 文件时、新应用可以在没有引导加载程序的情况下工作。 我想知道 SDK 更新之间是否存在可能导致此问题的更改?  

此致、

水阳

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!  

    查看 SDK 6.10中的 CMD 文件、我可以看到一些差异、例如对.resetVecs 的引用。 因此、我想您的客户将不得不使用新的 CMD 文件来使旧的引导加载程序正常工作。