This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] WL1807MOD:连接到 Wifi 失败。 错误显示发生了看门狗恢复、之后无法连接

Guru**** 2538930 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/1104584/wl1807mod-connecting-to-wifi-failed-error-shows-watchdog-recovery-happened-and-couldnt-connect-thereafter

器件型号:WL1807MOD
Thread 中讨论的其他器件:BQ25790WL1271

Linux 版本5.4.56

我们的一个系统在启用和连接 WiFi 方面存在困难。 查看日志显示。

第331行:5月24日00:33:11内核:[ 23.829857] wlcore:wl18xx HW:183x 或180x、PG 2.2 (ROM 0x11)
第332行:5月24日00:33:11内核:[23.880433] wlcore:已加载
第693行:[23.829857] wlcore:wl18xx 硬件:183x 或180x、PG 2.2 (ROM 0x11)
第694行:[23.880433] wlcore:已加载
第1361行:5月24日00:33:20内核:[41.41086] wlcore:PHY 固件版本:版本8.2.0.245
第1386行:5月24日00:33:20内核:[41.600476] wlcore:固件已启动(版本8.9.0.0.88)
第3629行:5月24日00:33:32内核:[53.439970] wlcore:down
第4138行:5月24日00:33:35内核:[56.462205] wlcore:down
第4907行:5月24日00:35:56内核:[197.459106] wlcore:PHY 固件版本:版本8.2.0.245
第4908行:5月24日00:35:56内核:[197.633314] wlcore:固件已启动(版本8.9.0.0.88)
第11122行:5月24日00:36:43内核:[244.003814] wlcore:收到错误软件看门狗中断! 正在开始恢复。
第11124行:5月24日00:36:43内核:[244.014096]警告:CPU:1 PID:391 at drivers/net/wireless/ti/wlcore/main.c:794 wl12xx_queue_recovery_work+0x5c/0x60 [wlcore]
第11124行:5月24日00:36:43内核:[244.014096]警告:CPU:1 PID:391 at drivers/net/wireless/ti/wlcore/main.c:794 wl12xx_queue_recovery_work+0x5c/0x60 [wlcore]
第11125行:5月24日00:36:43内核:[ 244.025562 ]链接的模块:AF_PACKET CAN_RAW CAN AES_ARM_BS crypto_SIMD cryptd wl18xx wlcore mac80211 libarc4 cfg80211 rfkill STM32_ADC STM32_timer_trigger industrialio_trigger_trigger_buffer ko_fiftcharge_barge_barge_barge_barge_barge_core_pl
第11132行:5月24日00:36:43内核:[244.106453][ ](warn_slowpath_fmt)、来自[ ](wl12xx_queue_recovery_work + 0x5c/0x60 [wlcore])
第11133行:5月24日00:36:43内核:[244.116466][ ](wl12xx_queue_recovery_work [wlcore])、来自[ ](wlcore_IRQ+0x108/0x188 [wlcore])
第11133行:5月24日00:36:43内核:[244.116466][ ](wl12xx_queue_recovery_work [wlcore])、来自[ ](wlcore_IRQ+0x108/0x188 [wlcore])
第11133行:5月24日00:36:43内核:[244.116466][ ](wl12xx_queue_recovery_work [wlcore])、来自[ ](wlcore_IRQ+0x108/0x188 [wlcore])
第11134行:5月24日00:36:43内核:[244.126773][ ](wlcore_IRQ [wlcore])、来自[ ](IRQ_THREAD_Fn+0x1C/0x78)
第11134行:5月24日00:36:43内核:[244.126773][ ](wlcore_IRQ [wlcore])、来自[ ](IRQ_THREAD_Fn+0x1C/0x78)
第11144行:5月24日00:36:43内核:[244.195294] wlcore:正在进行硬件恢复。 固件版本:版本8.9.0.0.88
第11145行:5月24日00:36:43内核:[ 244.209304] wlcore:PC:0x108282、HINT_STS:0x00000000计数:1.
第11146行:5月24日00:36:43内核:[244.214077] wlcore:down
第11147行:5月24日00:36:43内核:[244.216295] wlcore:down
第11153行:5月24 00:36:43内核:[244.523058]警告:CPU:0 PID:105 at drivers/net/wireless/ti/wlcore/SDIO.c:131 wl12xx_SDIO_raW_write+0x168/0x1c4 [wlcore_SDIO]
第11153行:5月24 00:36:43内核:[244.523058]警告:CPU:0 PID:105 at drivers/net/wireless/ti/wlcore/SDIO.c:131 wl12xx_SDIO_raW_write+0x168/0x1c4 [wlcore_SDIO]
第11154行:5月24日00:36:43内核:[ 244.537345]链接的模块:AF_PACKET CAN_RAW CAN AES_ARM_BS crypto_SIMD cryptd wl18xx wlcore mac80211 libarc4 cfg80211 rfkill STM32_ADC STM32_timer_trigger industrialio_bufferkgerkfagram_bufgerko_25790 (fug_bufb)
第11164行:5月24日00:36:43内核:[244.625067][ ](warn_slowpath_fmt)、来自[ ](wl12xx_SDIO_RAW_WRITE+0x168/0x1c4 [wlcore_SDIO])
第11165行:5月24日00:36:43内核:[244.635311][ ](wl12xx_SDIO_RAW_WRITE [wlcore_SDIO])从[ ](wlcore_set_partition+0xd8/0x540 [wlcore])
第11165行:5月24日00:36:43内核:[244.635311][ ](wl12xx_SDIO_RAW_WRITE [wlcore_SDIO])从[ ](wlcore_set_partition+0xd8/0x540 [wlcore])
第11165行:5月24日00:36:43内核:[244.635311][ ](wl12xx_SDIO_RAW_WRITE [wlcore_SDIO])从[ ](wlcore_set_partition+0xd8/0x540 [wlcore])
第11166行:5月24日00:36:43内核:[244.6425][ ](wlcore_set_partition [wlcore])、来自[ ](wl12xx_set_power_ON+0x6c/0x144 [wlcore])
第11166行:5月24日00:36:43内核:[244.6425][ ](wlcore_set_partition [wlcore])、来自[ ](wl12xx_set_power_ON+0x6c/0x144 [wlcore])
第11166行:5月24日00:36:43内核:[244.6425][ ](wlcore_set_partition [wlcore])、来自[ ](wl12xx_set_power_ON+0x6c/0x144 [wlcore])
第11167行:5月24日00:36:43内核:[244.656941][ ](wl12xx_set_power_on [wlcore])、来自[ ](wl12xx_chip_wakeup+0x28/0x244 [wlcore])
第11167行:5月24日00:36:43内核:[244.656941][ ](wl12xx_set_power_on [wlcore])、来自[ ](wl12xx_chip_wakeup+0x28/0x244 [wlcore])
第11168行:5月24日00:36:43内核:[244.667291][ ](wl12xx_chip_wakeup [wlcore])、来自[ ](wl1271_op_add_interface+0x6cc/0x9b4 [wlcore])
第11168行:5月24日00:36:43内核:[244.667291][ ](wl12xx_chip_wakeup [wlcore])、来自[ ](wl1271_op_add_interface+0x6cc/0x9b4 [wlcore])
第11169行:5月24日00:36:43内核:[244.678219][ ](wl1271_op_add_interface [wlcore])、来自[ ](drv_add_interface+0x4c/0x208 [mac80211])
第11175行:5月24日00:36:44内核:[245.015755]警告:CPU:0 PID:105 at drivers/net/wireless/ti/wlcore/SDIO.c:131 wl12xx_SDIO_raW_write+0x168/0x1c4 [wlcore_SDIO]
第11175行:5月24日00:36:44内核:[245.015755]警告:CPU:0 PID:105 at drivers/net/wireless/ti/wlcore/SDIO.c:131 wl12xx_SDIO_raW_write+0x168/0x1c4 [wlcore_SDIO]
第11176行:5月24日00:36:44内核:[245.027694]链接的模块:AF_PACK_RAW CAN AES_ARM_BS crypto_SIMD cryptd wl18xx wlcore mac80211 libarc4 cfg80211 rfkill STM32_ADC STM32_timer_trigger industrialio_trigger_bufferkger_bucharge_barge_barge_barge_core_pl 25790 (fift_buqf)
第11184行:5月24日00:36:44内核:[245.113882][ ](warn_slowpath_fmt)、来自[ ](wl12xx_SDIO_RAW_WRITE+0x168/0x1c4 [wlcore_SDIO])
第11185行:5月24日00:36:44内核:[245.124108][ ](wl12xx_SDIO_RAW_WRITE [wlcore_SDIO])从[ ](wlcore_set_partition+0xd8/0x540 [wlcore])
第11185行:5月24日00:36:44内核:[245.124108][ ](wl12xx_SDIO_RAW_WRITE [wlcore_SDIO])从[ ](wlcore_set_partition+0xd8/0x540 [wlcore])
第11185行:5月24日00:36:44内核:[245.124108][ ](wl12xx_SDIO_RAW_WRITE [wlcore_SDIO])从[ ](wlcore_set_partition+0xd8/0x540 [wlcore])
第11186行:5月24日00:36:44内核:[245.135238][ ](wlcore_set_partition [wlcore])、来自[ ](wl12xx_set_power_ON+0x6c/0x144 [wlcore])
第11186行:5月24日00:36:44内核:[245.135238][ ](wlcore_set_partition [wlcore])、来自[ ](wl12xx_set_power_ON+0x6c/0x144 [wlcore])
第11186行:5月24日00:36:44内核:[245.135238][ ](wlcore_set_partition [wlcore])、来自[ ](wl12xx_set_power_ON+0x6c/0x144 [wlcore])
第11187行:5月24日00:36:44内核:[245.145752][ ](wl12xx_set_power_on [wlcore])、来自[ ](wl12xx_chip_wakeup+0x28/0x244 [wlcore])
第11187行:5月24日00:36:44内核:[245.145752][ ](wl12xx_set_power_on [wlcore])、来自[ ](wl12xx_chip_wakeup+0x28/0x244 [wlcore])
第11188行:5月24日00:36:44内核:[245.156099][ ](wl12xx_chip_wakeup [wlcore])、来自[ ](wl1271_op_add_interface+0x6cc/0x9b4 [wlcore])
第11188行:5月24日00:36:44内核:[245.156099][ ](wl12xx_chip_wakeup [wlcore])、来自[ ](wl1271_op_add_interface+0x6cc/0x9b4 [wlcore])
第11189行:5月24日00:36:44内核:[245.166996][ ](wl1271_op_add_interface [wlcore])、来自[ ](drv_add_interface+0x4c/0x208 [mac80211])
11195行:5月24 00:36:44内核:[245.493018]警告:CPU:0 PID:105 at drivers/net/wireless/ti/wlcore/SDIO.c:131 wl12xx_SDIO_raW_write+0x168/0x1c4 [wlcore_sdio]
11195行:5月24 00:36:44内核:[245.493018]警告:CPU:0 PID:105 at drivers/net/wireless/ti/wlcore/SDIO.c:131 wl12xx_SDIO_raW_write+0x168/0x1c4 [wlcore_sdio]
11196行:5月24 00:36:44内核:[245.505228]链接的模块:AF_PACK_RAW CAN AES_ARM_BS crypto_SIMD cryptd wl18xx wlcore mac80211 libarc4 cfg80211 rfkill STM32_ADC STM32_timer_trigger industrialio_trigger_bufferkger_bufgerko_barge_chargeador_begrocore_pl 25790 (fift_buf
第11204行:5月24日00:36:44内核:[245.591934][ ](warn_slowpath_fmt)、来自[ ](wl12xx_SDIO_RAW_WRITE+0x168/0x1c4 [wlcore_SDIO])
第11205行:5月24日00:36:44内核:[245.602162][ ](wl12xx_SDIO_RAW_WRITE [wlcore_SDIO])从[ ](wlcore_set_partition+0xd8/0x540 [wlcore])
第11205行:5月24日00:36:44内核:[245.602162][ ](wl12xx_SDIO_RAW_WRITE [wlcore_SDIO])从[ ](wlcore_set_partition+0xd8/0x540 [wlcore])
第11205行:5月24日00:36:44内核:[245.602162][ ](wl12xx_SDIO_RAW_WRITE [wlcore_SDIO])从[ ](wlcore_set_partition+0xd8/0x540 [wlcore])
第11206行:5月24日00:36:44内核:[245.613282][ ](wlcore_set_partition [wlcore])、来自[ ](wl12xx_set_power_ON+0x6c/0x144 [wlcore])
第11206行:5月24日00:36:44内核:[245.613282][ ](wlcore_set_partition [wlcore])、来自[ ](wl12xx_set_power_ON+0x6c/0x144 [wlcore])
第11206行:5月24日00:36:44内核:[245.613282][ ](wlcore_set_partition [wlcore])、来自[ ](wl12xx_set_power_ON+0x6c/0x144 [wlcore])
第11207行:5月24日00:36:44内核:[245.623794][ ](wl12xx_set_power_on [wlcore])、来自[ ](wl12xx_chip_wakeup+0x28/0x244 [wlcore])
第11207行:5月24日00:36:44内核:[245.623794][ ](wl12xx_set_power_on [wlcore])、来自[ ](wl12xx_chip_wakeup+0x28/0x244 [wlcore])
第11208行:5月24日00:36:44内核:[245.634149][ ](wl12xx_chip_wakeup [wlcore])、来自[ ](wl1271_op_add_interface+0x6cc/0x9b4 [wlcore])
第11208行:5月24日00:36:44内核:[245.634149][ ](wl12xx_chip_wakeup [wlcore])、来自[ ](wl1271_op_add_interface+0x6cc/0x9b4 [wlcore])
第11209行:5月24日00:36:44内核:[245.645046][ ](wl1271_op_add_interface [wlcore])、来自[ ](drv_add_interface+0x4c/0x208 [mac80211])
11213行:5月24 00:36:44内核:[245.675057] wlcore:错误固件引导失败,尽管重试3次

导致此问题的原因是什么以及如何恢复?

此致、

Johncy。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Johncy、

    您能否探测 WLAN_EN 并确认在发现此问题时它已切换。

    最好

    序列号

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这种情况发生在 FT 系统中、因此无法 轻松地传输信号。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Johncy

    您是否能够在本地实验室设置中重现此问题。

    这将帮助我们更有效地解决问题。

    最棒的

    序列号

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    到目前为止、这仅发生在 FT 系统中、我们尚未在实验设置中看到此问题。 在上述情况下、发生此问题后、会尝试关闭链接、然后启动并重新启动 wpa_supplicant、但它不能帮助恢复。 它总是以结束  

    [3422.636487] wlan0:使用0e:02:8e:96:D8:25进行身份验证
    第16923行:5月24日01:29:41内核:[ 3422.643206] wlan0:将验证发送到0e:02:8e:96:D8:25 (请尝试1/3)
    第16935行:5月24日01:29:43内核:[ 3424.007631] wlan0:将验证发送到0e:02:8e:96:D8:25 (请尝试2/3)
    第16938行:5月24日01:29:44内核:[3425.032350] wlan0:将验证发送到0e:02:8e:96:D8:25 (请尝试3/3)
    第16945行:5月24日01:29:45内核:[ 3426.088608] wlan0:通过0e:02:8e:96:D8:25进行身份验证超时

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这表明 DUT 正在尝试连接到 AP、但身份验证超时。 在不参考无线监听器日志的情况下、很难评论导致这种情况的原因。