This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] WL1835MOD:4.19.94-rt39+内核的 wlcore 问题

Guru**** 1826200 points
Other Parts Discussed in Thread: WL1835MODCOM8B
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/983047/wl1835mod-wlcore-issue-with-4-19-94-rt39-kernel

器件型号:WL1835MOD
Thread 中讨论的其他器件:WL1835

您好!

我在与 IDK574x 类似的定制板上使用 Wifi WL1835器件。

我能够检测到它并将固件发送到 WL1835器件、但当发生中断时、如果使用4.19.94-rt39+内核和 preemst-RT、中断处理程序可能会卡住。
我尝试使用相同的内核版本、但没有 preem-RT、我能够连接到 WiFi 网络。

请参阅启用调试的 dmesg:

root@am57xx-EVM:~ ifconfig wlan0 up
[ 32.507068] wlcore:mac80211 start
[ 32.10499] wlcore:mac80211 add 接口类型2 Mac 04:79:b7:fe:42:52
[ 32.5017160] wlcore:分配硬件队列基址:0
[ fre86480] wlcore、32.9120] wlcore、b7:32.95] wlcore、bt、32.95] wlcore、bt:32.95] wl18xx-fw-4.bin

芯片 ID 0x6030111
[32.933840] wlcore:要上载的固件块:15[32.939007]
wlcore:块14 addr 0x0 len 120468
[32.943647] wlcore:正在启动固件上载
[32.947936] wlcore:f_data_chunk 120468_size 16384
[ 32.954674] wlcore 上载32.94793] wlore:wlore 0x60936024] wl] wlcore:正在上载 wlore wlore:
上载 FW 块0x354ca603至0x4000
[ 32.967637] wlcore:上载 FW 块0x9e971062至0x8000
[ 32.974247] wlcore:上载 FW 块0x2dc04252至0xc000
[ 32.982304] wlcore:上载 FW 块0x99b5c42e 至0x10000
[ 32.988247] wlcore:上载 FW 32.74614000] wlcore:上载 wleclcore 0x99000[ 32.78248]
上载 FW 块0x98b0ae97到0x18000
[ 33.002401] wlcore:上载 FW 最后


一个块(5780 B) 0x4c980a42到0x1c000 [ 33.00998] wlcore:3.313 addr 0x100000 131068 [ 33.015060] wlcore:开始固件上载[ 3.033.019350] wlcore
:3.01310451] wlen_lcore:3.3len_131068[ 3.3len_len_wlcore: 上载 FW 块0x77d733d1至0x100000
[ 33.035674] wlcore:上载 FW

块0x41ce16e6至0x104000 [ 33.043952] wlcore:上载 FW 0xd4ac73d5至0x108000 [ 33.052128] wlcore:上载 FW 0xf9a81403至0x3.060000]
wlcore:上载 FW 0x3.010001w3000[ 0x000] w3lcore:上载0x300001w3l531] wlcore
上载固件块0x7003858e 到0x114000
[ 33.076722] wlcore:上载固件

块0x0350c043到0x118000 [ 33.083516] wlcore:上载固件最后一个块(16380 B) 0x60a6e211到0x11c000 [ 33.091773] wlcore:33.12 addr 0x20400000 b]
wlcore:上载33.091264]固件:启动 wlcore [ 33.091264]
fw_data_len 52600 chunch_size 16384
[ 33.109238] wlcore:上载 FW chunt 0xa9bc61c6至0x20400000
[ 33.609] wlcore:上载 FW chunt 0xd78c43ea 至0x20404000
[ 33.126006] wlcore:上载 FW 0x069d35bc 至0x204074]
wlcore:上载 FW 0x33.204074] wmunchun块0x33.404824000[ 33.4074] wlcore:上载0x33.4074] wlcore:上载 FW 0x204024000] w24000[33.4074
块11 addr 00bb2000 len 536
[33.145521] wlcore:正在启动固件上载
[33.149811] wlcore:f_data_len 536 chunch_size 16384
[33.156231] wlcore:正在上传固件最后

一次上载(33.148b285bd5至 b00000 [33.163549] wlcore:正在启动 wl8536 bunchun块2836]固件:33.12bd
fw_data_len 28120 chunk_size 16384
[ 33.180826] wlcore:将 FW chun块0x5e99c387上载到 b0ae40
[ 33.187606] wlcore:上载 FW 上次

上载(11736 B) 0xe519a281到0b20 [bdr 195667] wlcore:33.9 adchunk_100366] wlcore:33.19363r_wlunk_16361] wlcore:33.2136 bunchunk_wlen_wlcore:33.163632]

上载 FW 块0x1328dd08至0x80900000
[ 33.218592] wlcore:上载 FW 块0x4dc6bd39至0x80904000
[ 33.225562] wlcore:上载 FW 块0xdcc5d1d0至0x80908000
[ 33.232533] wlcore:上载 FW 最后一个块(11984 B) 0x8024000] 0x80240008
bc6400] 0x8024000[33.240003bd24000]
开始固件上载
[33.250131] wlcore:f_data_len 31992 chunch_size 16384
[ 33.256737] wlcore:上载 FW chun块0xf45ef64a 至0x809000[
33.26369] wlcore:上载 FW 最后一个
块(15608 B) 0x8de003c0至0x80924000 [ 33.272024000] wlcore
:33.27806778] wlcore 上载0x33.452024000] wlcore:33.4524000[33.4524000] wlcore:33.27800]
fw_data_len 6144 chune_size 16384
[ chunch_287868] wlcore:上载 FW 最后一个块(6144 B) 0x3efa51bf 至0x80940000
[ 33.295561] wlcore:wl6 addr 0x80944000 len 6144
[ 33.144300546] wlcore:开始固件上载
[ 33.304838] wlcore:33.3646] wlen_lcore:wlen_f_163646] wlcore:wlcore
上载 FW 最后


一个块(6144 B) 33.08952bc 至0x80944000 [ b319020] wlcore:块5地址0x80948000 len 6144 [ 33.3244012] wlcore:开始固件上载[ 33.328300] wlcore:f_data_6144 lsize 16384
[ 334806] wlore:0x33.948lore:w333948b] wlore:上载0x33948lore
块4 addr 0x8094c000 len 6144
[ 33.347477] wlcore:正在启动固件上载
[ 33.351766] wlcore:fw_data_len 6144_size 16384
[ 33.358296] wlcore:正在上传固件最后一个块(6144 B) 0x5befbc27至0x8094c000
[ 0x3659192] wlcore
上载:33.36937955] wlunc:正在启动 wlcore
fw_data_len 8192 chune_size 16384
[ 33.381750] wlcore:上载 FW 最后一个块(8192 B) 0x2d713ca2至0x80950000
[ 33.389523] wlcore:


上载461地址0x80960000 21260 [ 33.39384] wlcore:启动固件 len [ 33.3988888] wlcore:上载0x809460] wlunchunk_lore:0x8093_lcore:0x809460[33.4960] wlunk_l] wlcore:上载0x8093_lcore
上载 FW 最后一个块(4876 B) 0x0d5f7d8f 至0x80964000
[ 33.420247] wlcore:chunk 1 addr 0x80953000 len 1536
[ 33.425235] wlcore:正在启动固件上载
[ 33.429524] wlcore:fw_data_db1536 lsize 16384[0x436036]
wlcore (33.4536] wdlore:上载0x436038436] wdlore [33.6436 bl)
块0地址0x80958000 len 24576
[ 33.449614] wlcore:开始固件上载
[ 33.453907] wlcore:fw_data_len 24576_size 16384
[ 33.460511] wlcore:上载 FW 0x3350f8cd 至0x80958000
[ 33.467464] wlcore
:上载块后0x44809292]块固件:0x384b] wlcore (33.458492] wlcore:上载块0x33458492b] 0x6030111
[33.500250] wlcore:cmd_box_addr b007f8
[33.504460] wlcore:mbox ptrs:bbbb00adc b0090
[33.509286] wlcore:PHY 固件版本:版本8.387 2.0.243[33.514716]
wlcore:unbevent:b333.5032]] wlcore 掩码[33.53x bx mb:w核心:w3mf
cr 32.24]

ACx cfg bitmap 89 blk 256 SPARE 1字段15
[33.535889] wlcore:cmd configure (57)[
33.540774] wlcore:ACx 动态 FW 跟踪配置0
[ 33.545596] wlcore:cmd configure (90)[
33.550485] wlcore:cmd template_set 2 (role 255)
[ 33.556535] wlcore:33.563md 模板 lcore (n3= 33.5355256] wlcore)[33.536255] wlcore (md)模板:mcmd3[33.526255] w
cmd template_set 19 (Role 255)
[ 33.568775] wlcore:cmd template_set 20 (Role 255)
[ 33.57498] wlcore:cmd template_set 0 (Role 255)
[ 33.580948] wlcore:cmd template_set 6 (Role 255)
[ 33.587000] wlcore:cmd template_set 5 (role 255)
[ 33.59125] wlcore:mcd template_set 5 (role 33.99125] wlcore (Role)[33.59125] wlcore:mcle 3mcle 5125] wlcore (le_set
cmd template_set 1 (Role 255)
[ 33.605172] wlcore:cmd template_set 15 (Role 255)
[ 33.611304] wlcore:cmd template_set 14 (Role 255)
[ 33.617442] wlcore:cmd template_set 13 (Role 255)
[ 33.623585] wlcore:
cmd template_set 16 (role 255)[ 33.6372] wlcore:mcd template_set 16 (role 6372] wlcore [33.6255] wlcore [33.6255] wlcore:mcd wlcore [33.6255
cmd template_set 7 (Role 255)
[ 33.641775] wlcore:cmd template_set 7 (Role 255)
[ 33.647827] wlcore:cmd template_set 7 (Role 255)
[ 33.1899 653872] wlcore:wl1271 mem cfg
[ 33.657293] wlcore:cmd configure (1)
[ 33.6672291][ 33.667291] wlcore config
:cmd firmware reg:wlcore config:wlcore:wlcore:33.667294] wlcore logger:wlcore
cmd reg 域 bitmap1:0x000007ff、bitmap2:0x00000000
[ 33.747296] wlcore:acx sg cfg
[ 33.750368] wlcore:cmd configure (22)
[ 33.759061] wlcore:acx sg enable
[ 33.762393] wlcore:cmd configure (21)
[ 33.767536] wlcore

块:wlcore 可用[33.767526] wlcore:wlcore:wldx 命令参考:wlcore:33.7377x] wlcore 块 44
[33.779451] wlcore:ACX Rx MSDU 寿命
[ 33.783482] wlcore:cmd configure (60)
[33.788495] wlcore:ACX DCO itrim 参数
[ 33.792789] wlcore:cmd configure (55)
[33.797797717] wlcore:ACX TX 配置选项
[ 33.806748]
wlcore:33.8034] wlcore: wl1271 Rx 中断配置
[ 33.811200] wlcore:cmd 配置(39)
[ 33.816138] wlcore:ACx CCA 阈值
[ 33.819818] wlcore:cmd 配置(16)
[ 33.824786] wlcore:ACX frag 阈值:2352
[ 829077] wlcore:cmd 配置(40)
wlcore 数据路径
[ 33.8340] wlcore:33.8338521] wlcore 数据路径 Rx START cmd channel 1
[ 33.843862] wlcore:TX START cmd channel 1
[ 33.847980] wlcore:acx pm config
[ 33.851311] wlcore:cmd configure (64)
[ 33.8563141] wlcore:acx set rate mgmt params
[ hang86060606060607] wlcore:cmd configure (52)
[ 33.856591] wlcore:33.8646 wlcore:wlcore:
配置命令(66)
[ 33.874418] wlcore:启动固件(版本8.9.0.0.81)
[ 33.879408] wlcore:支持11A
[ 33.883010] wlcore:启用命令角色
[ 33.887745] wlcore:ACX 睡眠验证2
[ 33.891341] wlcore:配置命令(29)
[ 33.99643]
wlcore:配置命令3[33.8980] wlcore [ 33.908963] wlcore:33.80] wlcore
ACx FM COEX 设置
[ 33.908437] wlcore:cmd configure (23)
[ 33.913403] wlcore:ACx rate Policies
[ 33.917086] wlcore:basic_rate:0x3、full_rate:0x3
[ 33.921985] wlcore:cmd configure (27)
[ 33.926982] wlcore:
配置33.9327] wlcore (33.9327)
ACx 组地址 tbl
[33.940836] wlcore:cmd configure (63)[
33.945773] wlcore:ACX 连接监视器参数:禁用
[ 33.951720] wlcore:cmd configure (18)
[33.956791] wlcore:ACX 信

标筛选器表[33.960998] wlcore:cmd configure (24)[33.96000] wlcore:启用 AClcore 筛选
器[33.9781] CMD 配置(11)
[ 33.975790] wlcore:ACX BCN DTIM 选项
[ 33.9733] wlcore:CMD 配置(20)
[ 33.984664] wlcore:ACX SNR 平均权重
[

CMD 988956] wlcore:CMD 配置(43)[ 33.993959] wlcore:ACX RSSI 平均值[ 33.6854] wlcore:配置(33.3Md)插槽33.6854] 

之后没有任何内容、该过程也不会返回。

一段时间后、dmesg 日志中有一个回溯跟踪:

[789.56034] RCU: 0级 RCU_node (CPU 0-1)上阻止的任务:P23 P1171
[789.60943] RCU: (由1检测、t=2102 Jiffies、g=3953、q=8693)
[789.560953] ktimersoftD/1 R 正在运行的任务 0 23. 2 0x00000000 


我可以看到一些 IRQ 已由驱动程序处理

# cat /proc/interrupts | grep wl18
CPU0 CPU1
178: 14. 0 4ae1000.GPIO 23边缘 wl18xx

我可以看到 ifconfig、wpa_supican 甚至 kworker 线程卡住、并且100%使用 CPU

# top -n1
PID 用户 PR NI virt RES SHR S %CPU %MEM time+命令
104 root -50 0 0 0 0 R 94.4 0.0 3:49.19 kwork/1:2+事件 

在 IRQ 线路上、当 IRQ 线程被卡住时、信号处于高电平。
一旦 IRQ 被处理(被叠层)、IRQ 信号应该处于低电平。

我没有可与 WL1835器件进行比较的评估板。

是否存在已知问题?

此致、
Romain

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!  

    是否可以使用最新的 WiLink 驱动程序 R8.8检查此问题? 有关版本详细信息、请访问 https://www.ti.com/tool/download/WILINK8-WIFI-NLCP。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    感谢您的回复。

    我从这一部门申请了专利系列:
    https://git.ti.com/cgit/wilink8-wlan/build-utilites/tree/patches/kernel_patches/4.19.38?h=r8.8

    wlcore 驱动程序需要最新的固件版本(版本8.9.0.0.83)、因此我在/lib/firmware/.中更新了它

    [21.040456] wlcore:wl18xx HW:183x 或180x、PG 2.2 (ROM 0x11)
    [21.087862] wlcore:已加载
    [21.087899] wlcore:驱动程序版本:R8.8 

    我注意到打印驱动程序版本的新行。

    然后我尝试运行命令 ifconfig wlan0 up。

    root@am57xx-evm:~./debug_wifi.sh;ifconfig wlan0 up
    [51.813286] wlcore:mac80211 start
    [51.81673] wlcore:mac80211 add 接口类型2 Mac 04:79:b7:fe:42:52
    [51.824167] wlcore:分配硬件队列基址:0
    [52.83120] wlcore 启动[56539] w83lcore、w8313 wl18xx-fw-4.bin
    :w4013]
    芯片 ID 0x6030111
    [52.433819] wlcore:要上载的固件块:15[52.438995]
    wlcore:块14 addr 0x0 len 122512
    [52.444849] wlcore:正在启动固件上载
    [52.449150] wlcore:fw_data_len 122512121250_size 16384[52.444849] wlcore
    上载到块0x65384[wlcore [0x458064] wlcore:从块0x458064] wlcore
    上载 FW 块0xdf366537到0x4000
    [52.469666] wlcore:上载 FW 块0x14e3328a 到0x8000
    [52.476347] wlcore:上载 FW 块0x84443866到0xc000
    [52.485217] wlcore:上载 FW 块0xfb7786F2到0x10000 wlcore
    [0x2.549C:上载 w19000] wlcore [52.4852172]
    上载 FW 块0xd2a38dc1至0x18000
    [52.505449] wlcore:上载 FW 最后
    
    
    一个块(7824 B) 0x1c000 [52.513279] wlcore:块13 addr 0x100000 131068 [52.518370] wlcore:开始固件上载[52.52132668]
    wlcore:len 1364] wlen [52.5238_en_en_zh_data. 上载 FW 0x863dd88f 至0x100000
    [52.541276] wlcore:上载 FW
    块0x87b1ffc9至0x104000 [52.550264] wlcore:上载 FW 0x4964b4cf 至0x108000
    [52.559264] wlcore:上载 FW 0x7719361a 至0x10258b4100]
    wlcore [0x25842998b] wlcore:上载 FW 0x258b2c10024000[0x258b[0x258b] wlcore:上载0x258b2410421024] w24b] w24b]
    上载 FW 0xc11707c9至0x114000
    [52.586354] wlcore:上载 FW
    
    块0xc519a9ce 至0x118000 [52.593187] wlcore:上载 FW 最后一个块(16380 B) 0x06642965至0x11c000 [52.601593] wlcore:0x1296296]
    wlcore 固件:上载 w266077]从0x67642965]开始
    fw_data_len 53296 chunch_size 16384
    [52.620585] wlcore:上载 FW chunt 0x1bef9380至0x20400000
    [52.629747] wlcore:上载 FW 块0x374d8516至0x20404000
    [52.639053] wlcore:上载 FW 0x24929747] wlcore 0x2040245248] wlcore
    :上载0x206424524024[0x2040246424](w245240246424] w24x 2.524x 2.524x 2.524x 2.524x 2.5x 2.5x 2.5x 2.5x 2.5x 2.5x 2.5x 2.5x)
    块11 addr 00000 len 512
    [52.658847] wlcore:正在启动固件上载
    [52.663146] wlcore:fw_data_len 512 chune_size 16384
    [52.670246] wlcore:正在上传固件最后一个块(52.658847) 0x725aae32至00000
    [52.677502] wlcore
    :正在启动 wlunc 2.56840] wlcore:
    fw_data_len 28432 chune_size 16384
    [52.696437] wlcore:将 FW bunk 79c7799上传到 b0ae40
    [52.703270] wlcore:上传 FW 上次
    
    上传(12048 B) 0x12456f3c 至0bbx 40 [52.711458] wlcore:7209 adlh 2.900136] wlcore [wlen_zh_datore64136] bu:启动 wlcore:5bh 2.61len_zh-64136]
    
    上载 FW 块0x16c4a45e 到0x80900000
    [52.735180] wlcore:上载 FW
    
    
    块0x45c28381到0x80904000 [52.742173] wlcore:上载 FW 块0xe6c40ea 到0x80908000 [52.749274] wlcore:上载 FW 最后20000 (1.2.742173] wlcore 0x80652bx 8080808] wldr 3bt:0x80652bt 5652[0x80362b] wlunt 5803bdr
    开始固件上载
    [52.767049] wlcore:f_data_len 31992 chune_size 16384
    [52.774372] wlcore:上传 FW 块0xa55998b8至0x80920000
    [52.781394] wlcore:上传 FW 最后一个块(15608 B) 0xe29eac9f 至0x809249b8至0x80920000 [52.78954]
    wlcore
    :w9524599742] wlcore 上载 wldr 599599245lcore:w95] wl核心:w9524599245ldr
    fw_data_len 6144 chune_size 16384
    [52.806455] wlcore:上载 FW 最后
    
    
    一个块(6144 B) 0x1cf22292至0x80940000 [52.814205] wlcore:6 addr 0x80944000 len 6144 [52.819201] wlcore:开始固件上载[52.8145] wlcore:52.5384] wlen_64245len_lcore:wlen_6435245l] wlen
    上载 FW 最后一个块(6144 B) 0x9e114e7e 到0x80944000
    [52.838503] wlcore:chunk 5 addr 0x80948000
    
    chun块6144 [52.843519] wlcore:正在启动固件上载[52.8478171] wlcore:f_data_len 6144_size 16384bu [ 52.843519] wlcore
    (0x8524548245b] wl] wlcore:正在上载0x85244bx 644b] wl] wlcore (0x85244bw)
    块4地址0x8094c000 len 6144
    [52.867879] wlcore:开始固件上载
    [52.872179] wlcore:fw_data_chunk 6144 chune_size 16384
    [52.879433] wlcore:上载 FW 最后
    一个块(6144 B) 0x996c6625至0x8094c000 wlunchune_size 16384 [52.879433] wlcore
    :5lunc:启动 w891894len [5lunc:5lore 5lunc:5lunc:518941942]
    fw_data_len 8192 chune_size 16384
    [52.903786] wlcore:上载 FW 最后
    
    
    一个块(8192 B) 0x480de405至0x80950000 [52.911630] wlcore:块2 addr 0x80960000 21260 [52.916754] wlcore:开始固件上载[52.921052] wlcore:0x809560_wlen_wlcore 数据:0x8052] wlenf 5365dsn
    
    上载 FW 最后一个块(4876 B) 0x9a1409a0至0x80964000
    [52.943432] wlcore:块1地址0x80953000
    
    块1536 [52.948428] wlcore:开始固件上载[52.952728] wlcore:fw_data_len 1536 len_size 16384 [52.9548428] wlcore
    上载[0x809536] wlcore (w9536] wlunc)
    块0地址0x80958000 len 24576
    [52.973715] wlcore:开始固件上载
    [52.978015] wlcore:fw_data_len 24576 chune_size 16384
    [52.985404] wlcore:上载 FW 块0x97ce0f8b 至0x80958000
    [52.992422] wlcore:0x59000b
    固件上载后 wlid 0x8064b] 0x6030111
    [53.027379] wlcore:cmd_box_addr b007f8
    [53.031680] wlcore:mbox ptrs:bbb00adc b0090
    [53.036596] wlcore:PHY 固件版本:版本8.2.0.243[53.042030]
    wlcore:unb00adc b00b90 [53.06596] wlcore 掩码:rm 3.053.05017] wlcore
    
    (mcr mf) wlcore:v3.05.3.04510726.026.24]] wlcore (wlcore:undl核心:unm)
    ACx cfg bitmap 89 blk 256 SPARE 1字段15
    [53.064687] wlcore:cmd configure (57)[
    53.070108] wlcore:ACx 动态 FW 跟踪配置0
    [53.04939] wlcore:cmd configure (90)[53.080385]
    wlcore:cmd template_set 2 (Role 255)
    [ 53.084958] wlcore:w3053.03553.03550.085] wlcore [wlcore (template_lcore:mcd 模板:lcore 53.03553.03553.0455] wlcore (lcore)
    cmd template_set 19 (Role 255)
    [53.100535] wlcore:cmd template_set 20 (Role 255)
    [53.107304] wlcore:cmd template_set 0 (Role 255)
    [53.114140] wlcore:cmd template_set 6 (Role 255)
    [53.120820] wlcore:
    cmd template_set 5 (Role 255)[53.1140] wlcore [3.5128] wlcore:cmd template_set 5 (le51.51255] wcore [3.4[wcore:mcle 1255] wlcore [3.4[3.51255]
    cmd template_set 1 (Role 255)
    [ 53.140953] wlcore:cmd template_set 15 (Role 255)
    [ 53.147717] wlcore:cmd template_set 14 (Role 255)
    [ 53.154573] wlcore:cmd template_set 13 (Role 255)
    [ 53.161339] wlcore:cmd template_set 14 (Role 255
    )[ 3.154573] wlcore (Role 255:mcd 模板53.1607] wlcore (le] wlcore:mcd mcle 536255] wlcore (le] wlcore (le_lcore)[3.
    cmd template_set 7 (Role 255)
    [53.181544] wlcore:cmd template_set 7 (Role 255)
    [53.188254] wlcore:cmd template_set 7 (Role 255)
    [53.195079] wlcore:wl1271 mem cfg
    [53.1985175] wlcore:cmd configure (1)[53.195079] wlcore
    config
    :wlcore 53.5210036:wlcore 53.5210036:wlcore 53.5210] wlcore 53.5210036:wlcore 5r]
    cmd reg 域 bitmap1:0x000007ff、bitmap2:0x00000000
    [54.329099] wlcore:ACX SG cfg
    [54.332185] wlcore:cmd configure (22)
    [54.341232] wlcore:ACX SG enable
    [54.344578] wlcore:cmd configure (21) wlcore [54.341232] wlcore
    [4.52] wldx
    dx bt:wldx bt bt:534353dx
    bt:wlcore [4.354mt:wldx bt bt:54913] 44
    [54.362426] wlcore:ACX Rx MSDU 寿命
    [54.366463] wlcore:cmd configure (60)
    [54.371825] wlcore:ACX DCO itrim 参数
    [54.376128] wlcore:cmd configure (55)
    [54.381479] wlcore:ACX DCO itrim 参数[54.385515] wlcore 配置[5395lcore 选项[4.15] wlcore (
    5lcore 配置)
    wl1271 Rx 中断配置
    [ 54.395419] wlcore:cmd configure (39)
    [ 54.400826] wlcore:ACX CCA 阈值
    [ 54.404519] wlcore:cmd configure (16)
    [ 54.409945] wlcore:ACX frag 阈值:2352
    [ 54.414246A] wlcore:4.41963d
    数据路径[ 4.4463] wlcore:wlcore:wl446364] wlcore (wlcore:4.4md) 446364] wlcore 数据路径:4.4md:wl446364] wlcore
    Rx START cmd channel 1
    [54.430275] wlcore:TX START cmd channel 1
    [54.434402] wlcore:ACx pm config
    [54.437741] wlcore:cmd configure (64)
    [54.443163] wlcore:ACX set rate mgmt params
    [54.447466] wlcore:configure (45x wlcore
    :配置[54.4552] wlcore:wlhang454.455466])
    cmd configure (66)
    [54.462150] wlcore:firmware booted (Rev 8.9.0.0.83)
    [54.467150] wlcore:11A is supported
    [54.470764] wlcore:cmd role enable
    [ 54.475901] wlcore:ACX sleep auth 0
    [ 54.479505] wlcore:配置
    4.4865]
    wlcore [ 4.4865](配置4.4865] wlcore [4.4865] wlcore:配置4.4865] wlcore [4.4865] wlcore [4.4865](配置)
    ACx FM COEX 设置
    [54.497479] wlcore:cmd configure (23)
    [54.502799] wlcore:ACx 速率策略
    [54.506490] wlcore:basic_rate:0x3、full_rate:0x3
    [54.511398] wlcore:cmd configure (27)
    [54.5165299] wlcore
    :配置(w5227) wlcore (w5227)
    ACx 组地址 tbl
    [54.531570] wlcore:cmd configure (63)[54.536981]
    wlcore:ACX 连接监控器参数:禁用
    [54.542941] wlcore:cmd configure (18)
    [54.548315] wlcore:ACX
    
    信标筛选器表[54.552531] wlcore:禁用[54.542941] wlcore:CMD 配置[54.548315] wlcore:启用 wlcore (514424] wlcore:wl514524] wlcore:wl524]
    CMD 配置(11)
    [54.568153] wlcore:ACX BCN DTIM 选项
    [54.572105] wlcore:CMD 配置(20)
    [54.577520] wlcore:ACX RSSI SNR 权重
    [54.581821] wlcore:CMD 配置(43)
    [54.587244] wlcore:
    配置(559150) wlcore:4.5474] wlcore (54954)
    ACX 服务周期超时
    [54.599950] wlcore:cmd configure (33)
    [54.605374] wlcore:ACX RTS 阈值:2353
    [54.609589] wlcore:cmd configure (62)
    [54.615007] wlcore:ACX ac cfg 0 CW_ming 15 CW_max 63 aifs 3 op (wlcore
    :54612) wlcore (wlcore):4.54612)
    acx tid config
    [54.630043] wlcore:cmd configure (9)
    [54.635363] wlcore:acx ac cfg 1 CW_ming 15 CW_max 63 aifs 7 txop 0
    [54.641670] wlcore:cmd configure (3)
    [54.647003] wlcore:acx tid_max 63 aifs 7 txop 0 [54.641670] wlcore
    :配置[54.65432:wlcore (4.5659419] wlcore:wld] wlcore (4.5md)
    ACx ac cfg 2 cw_ming 15 cw_max 63 aifs 1 txop 3008
    [54.662287] wlcore:cmd configure (3)
    [54.667636] wlcore:acx tid config
    [ 54.671064] wlcore:cmd configure (9)
    [54.676396] wlcore:acx cfg 1566] wlcore:acx cw
    c 1566_cw 1 l酷 睿[5461064] wlunc 1 cw 1.5cw 12_lunc 1566] wming 1 cmd configure (3)
    [54.688345] wlcore:acx tid config
    [54.691776] wlcore:cmd configure (9)
    [54.697109] wlcore:acx feature cfg
    [54.700625] wlcore:cmd configure (67)
    [54.706043] wlcore:acx keep alive mode (wlcore:
    w4741074] wlcore:wl54.7150] wlcore (配置)
    ACx BA 启动器策略
    [54.719800] wlcore:cmd configure (46)
    [54.725242] wlcore:mac80211 BSS 信息角色0已更改0xe
    [ 54.725247] wlcore:IRQ work
    [ 54.725498] wlcore:INTR:0x4 (FW_Rx_COUNTER = 0、WL725247] wlcore:[4.525498] wlcore:wlcore = 0x4 (wv_r_rx = 0、wv_r_tr = 0)[4.5489_lcore =
    w245r_w_r_r_r_rt = 0]
    mbox 0 [54.725749]
    wlcore 上的事件:mbox 矢量:0x80000
    [54.753700] wlcore:ACX 插槽
    [54.756605] wlcore:cmd configure (2)
    [54.761969] wlcore:ACX_SET_PREAMARY
    [54.766287] wlcore:cmd configure (4.756605] wlcore [4.7730]
    wlcore [4.5141] wlcore:wlset [4.778241] wlcore [4.171591]
    
    mac80211 conf TX 0
    [54.785380] wlcore:acx ac cfg 3 cw_ming 15 cw_max 1023 aifs 2 txop 0
    [54.791862] wlcore:cmd configure (3)
    [54.797187] wlcore:acx tid config
    [54.800614] wlcore:configure (4.791862] wlcore
    :配置[54.598052] wlcore [4.80521] wlcore [wlcore [4.80521] wlcore [wlcore:wlcore 580521] wlcore 580521] wlcore
    ACx ac cfg 2 cw_ming 15 cw_max 1023 aifs 2 txop 0
    [54.816242] wlcore:cmd configure (3)
    [54.821572(2004) wlcore:acx tid config
    [54.825117] wlcore:cmd configure (9)
    [54.830467] wlcore:mac80211 conf 2 tx
    wlcore [54.8255] ACx ac cfg 0 CW_ming 15 CW_max 1023 aifs 2 txop 0
    [54.840736] wlcore:cmd configure (3)
    [54.846053] wlcore:ACX tid config
    [54.849482] wlcore:cmd configure (9)
    [54.854878] wlcore:mac80211 l558360] wlcore:wlcore 54.5486x 54660]
    ACX ac cfg 1 CW_ming 15 CW_max 1023 aifs 2 txop 0
    [54.865175] wlcore:cmd configure (3)
    [54.870508] wlcore:ACX tid config
    [ 54.873957] wlcore:cmd configure (9)
    [54.879294] wlcore:mac80211 bss
    config [ 54.873957] wlcore:CMD 配置(9)[54.879294] wlcore:mac8024]更改了 IP 地址:wlcore 0x4815 IP 地址:wlcore (4) 0
    [ 54.889562] wlcore:cmd configure (25)
    [ 54.894984] wlcore:mac80211 config PSM off power 0 idle changed 0xffffff9f
    [ 54.902036] wlcore:mac80211 configure filter changed 0 total 8000000
    [54.905749] ipv6:ADDRCONF (NETDEV_UP) wlcore:wlan59069 wlcore:wlcore not ready:wlan0
    mac80211 config PSM off power 0 idle changed 0x10
    root@am57xx-EVM:~#[54.926801] wlcore:acx 组地址 tbl
    [54.932472] wlcore:cmd configure (63)[54.937985]
    wlcore:mac80211 configure filter 0 total 80000000
    [54.94463] wlcore
    :配置4663] wlcore (wl646x 组地址)
    
    偶然(我猜)命令成功执行、因此我启动了 wpa_supplicant:
    root@am57xx-EVM:~次 wpa_supplicant -I wlan0 -c /etc/wpa_supplicant.conf 成功初始化 wpa_supplicant [77.509575] wlcore:mac80211 HW 扫描 [77.513224] wlcore:n_pactive_ch = 1 [77.516832] wlcore:频率2467、ch.12/250/最大值、0x112_power、0x112_bs/min NO-IR [77.525884] wlcore:n_pactive_ch = 2 [77.529491] wlcore:频率2472、通道13、标志0x112、功率20、最小/最大_dwell 25/50、 NO-IR [77.538125] wlcore:n_pactive_ch = 3 [77.541730] wlcore:频率2484、通道14、标志0x1f2、功率20、最小/最大_dwell 25/50、 NO-IR [77.550392] wlcore:频率2412、ch. 1、标志0x1a0、power 20、min/max_dwell 25/50 [77.558083] wlcore:频率2417、ch. 2、标志0x1a0、power 20、min/max_dwell 25/50 [77.565790] wlcore:频率2417、ch.2、flags 0x1a0、功率20、功率20/最大停留255/50 [77.5725] FREQ 2427、CH4、FLAGS 0x1a0、POWER 20、MIN/max_Dwell 25/50 [77.581018] wlcore:Freq 2432、ch5、FLAGS 0x180、POWER 20、MIN/max_Dwell 25/50 [77.588994] wlcore:Freq 2437、ch. 6、flags 0x180、 wlcore、dwell 25/50 [77.588994] wlcore:wlcore:7ldwell 25/50] FREQ 2442、CH7、FLAGS 0x180、POWER 20、MIN/max_Dwell 25/50 [77.604711] wlcore:Freq 2447、CH.8、FLAGS 0x180、POWER 20、MIN/max_Dwell 25/50 [77.612154] wlcore:FREQ 2452、CH.9、FLAGS 0x180、POWER 20、POWER_Dwell 25/50 [77.612154] wlcore :FREQ 2452、WELL:20125/46] FREQ 2457、CH.10、FLAGS 0x190、POWER 20、MIN/max_Dwell 25/50 [77.627996] wlcore:Freq 2462、CH.11、FLAGS 0x190、POWER 20、MIN/max_Dwell 25/50 [77.635818] wlcore: 2.4GHz:有源11无源3 [77.640730] wlcore: 5GHz:有源0无源0 [77.645844] wlcore: dfs:0 [77.648926] wlcore:生成探测器请求带0 [77.653951] wlcore:cmd template_set 2 (角色0) [77.965225] wlcore:IRQ work [ 77.968396] wlcore:INTR:0x40 (FW_Rx_COUNTER = 1、drv_9652X] wlcore: IRQ work [ 7.968Rx] wlcore:0x7812969r_t_r_tr :0x78_tr = 0x77_tr = 0x7870r_r_tr = 0x7870r_r_tr = 7.78_r_tr = 7.78_tr = 7.78_r_tl tr = 412序列1605 hlid 0 [77.987460] wlcore:IRQ 工作 [77.990610] wlcore:INTR:0x40 (FW_Rx_COUNTER = 2、drv_Rx_counter = 0、TX_Results_counter = 0) [77.999273] wlcore:WL1271_ACX_INTR_INTR_Rdr :w990]] wlcore 数据:0x7684rx 1006.00249r] wlcore [w128] wlrf rt:rf 78249r_r_r_r_rt:w249r] wrf [ wr_rt:wrf rf rf rf rf rf 0x8 (FW_Rx_COUNTER = 2、drv_Rx_counter = 0、TX_Results_counter = 0) [78.277761] wlcore:WL1271_ACX_INTR_EVENT_B [78.281974] wlcore:mbox 1上的事件 [78.285722] wlcore:mbox vector:0x78.298100] wlcore 扫描[w29384r] wlcore [wlcore:w293878.100] wlcore:w2938728384r] wlcore 扫描[wlcore [w29387387r] wlcore [wlcore:w29387r29384r] wlcore mac80211 HW 扫描 [78.304531] wlcore:频率5180、通道36、标志0x22、电源20、最小/最大_dwell 25/50、 NO-IR [78.312585] wlcore:频率5190、通道38、标志0x22、电源20、最小/最大_dwell 25/50、 NO-IR [78.320681] wlcore:频率5200、通道40、标志0x2、电源20、最小值/最大值_dwell 25/50、 NO-IR [78.328652] wlcore:频率5210、通道42、标志0x2、电源20、最小值/最大值_dwell 25/50、 NO-IR [78.336625] wlcore:频率5220、通道44、标志0x2、电源20、最小值/最大值驻留25/50、 NO-IR [78.344594] wlcore:频率5230、通道46、标志0x12、电源20、最小/最大_dwell 25/50、 NO-IR [78.352645] wlcore:频率5240、通道48、标志0x2、电源20、最小值/最大值驻留25/50、 NO-IR [78.360618] wlcore:频率5745、通道149、标志0x122、电源20、最小值/最大值_dwell 25/50、 NO-IR [78.36882] wlcore:频率5765、通道153、标志0x102、电源20、最小/最大_dwell 25/50、 NO-IR [78.377086] wlcore:频率5785、通道157、标志0x102、电源20、最小/最大_dwell 25/50、 NO-IR [78.385320] wlcore:频率5805、通道161、标志0x102、电源20、最小/最大_dwell 25/50、 NO-IR [78.393552] wlcore:频率5825、通道165、标志0x112、电源20、最小/最大_dwell 25/50、 NO-IR [78.401780] wlcore:频率5260、通道52、标志0xA、电源20、最小/最大_dwell 25/50、 DFS、无 IR [78.410184] wlcore:频率5280、通道56、标志0xA、电源20、最小/最大_dwell 25/50、 DFS、无 IR [78.418593] wlcore:频率5300、通道60、标志0xA、电源20、最小/最大_dwell 25/50、 DFS、无 IR [78.427001] wlcore:频率5320、通道64、标志0x1a、电源20、最小/最大_dwell 25/50、 DFS、无 IR [78.435496] wlcore:频率5500、通道100、标志0x2a、电源20、最小值/最大值驻留25/50、 DFS、无 IR [78.444076] wlcore:频率5520、通道104、标志0xA、电源20、最小/最大_dwell 25/50、 DFS、无 IR [78.452565] wlcore:频率5540、通道108、标志0xA、电源20、最小/最大_dwell 25/50、 DFS、无 IR [78.462168] wlcore:频率5560、通道112、标志0xA、电源20、最小/最大_dwell 25/50、 DFS、NO-IR [78.470664] wlcore:频率5580、通道116、标志0xA、电源20、最小/最大_dwell 25/50、 DFS、无 IR [78.479160] wlcore:频率5600、通道120、标志0xA、电源20、最小/最大_dwell 25/50、 DFS、无 IR [78.487652] wlcore:频率5620、通道124、标志0xA、电源20、最小/最大_dwell 25/50、 DFS、无 IR [78.496148] wlcore:频率5640、通道128、标志0xA、电源20、最小/最大_dwell 25/50、 DFS、无 IR [78.504641] wlcore:频率5660、通道132、标志0xA、功率20、最小/最大_dwell 25/50、 DFS、无 IR [78.513137] wlcore:频率5680、通道136、标志0xA、电源20、最小/最大_dwell 25/50、 DFS、无 IR [78.521625] wlcore:频率5700、通道140、标志0x1a、电源20、最小/最大_dwell 25/50、 DFS、无 IR [78.530203] wlcore: 2.4GHz:主动0被动0 [78.535034] wlcore: 5GHz:有源0无源12 [78.539769] wlcore: dfs:15 [78.542938] wlcore:构建探测器请求带1 [78.547416] wlcore:cmd template_set 3 (角色0) [80.426971] wlcore:IRQ work [80.430145] wlcore:INTR:0x40 (FW_Rx_COUNTER = 3、drv_82691] wlcore:[WL4812_rink = 0x48r_r_rink = 0x48r_r_rink = 0x48r_r_rink = 0x48r_rx = 0x4rink = 0x48r_r_rink = 0.4rink = 0x48r_r_rink = 0.4r_rink = 0.4r_rink 476 2.0910 hlid 0 [80.449261] wlcore:MGMT - Rx skb 0xebd48aa6:476 SEQ 910 hlid 0 [82.003122] wlcore:IRQ work [82.006289] wlcore:INTR:0x4 (FW_TR_COUNTER = 3、drv_Rx_counter = 2、WL18071] wlcore :[WL148866_r_wlcore:0x000866_r_wr_r_wr_r_r_r_rink = 3、[WL148866_wr_wr_wr_wr_r_r_ mbox 0 [82.022823] wlcore 上的事件:mbox 矢量:0x100 [82.026638] wlcore:扫描结果:1 [82.030179] wlcore:扫描完成 [ 82.033877] wlcore:cmd reg domain config [82.037919] wlcore:cmd reg domain map1:0x002.033877] wlcore:0x82150002 bitlcore :82.01500042] wlcore:82.037942] wlcore 0x8 (FW_Rx_COUNTER = 3、drv_Rx_counter = 2、TX_Results_counter = 0) [82.160182] wlcore:WL1271_ACX_INTR_EVENT_B [82.164404] wlcore:mbox 1上的事件
    wlan0:sme:尝试使用 myMAC 进行身份验证(ssid='msid' freq=2412 MHz)

    [82.173625] wlan0:使用 myMAC [82.173745] wlcore 进行身份验证 wlcore:mbox 矢量:0x80000 [82.185387] wlcore:mac80211 config PSM 关闭电源0正在使用中已更改0x100 [82.192134] wlcore:mac80211添加 chanc1 (类型1) [ 82.197054 wlcore:mac80211:wlcore mac80211分配 chanctx (角色0) 1 (类型1)(雷达0 dfs_state 0) [82.204941] wlcore:mac80211 BSS 信息角色0已更改0x40000 [82.210638] wlcore:acx dot11_cur_tx_pwr 20 [82.214296] wlcore:配置(32.21061] wlcore 更改[826101] wlcore 类型:更改后1 mac802108581] wlcore (mac801) mac80211 BSS 信息角色0已更改0x4000 [82.232225] wlcore:mac80211 BSS 信息角色0已更改0xe0 [82.237669] wlcore:changed_BSSID:myMAC、AID:0、BCN_int:100、brates:0xf RATE RATE _SET:0x0 [82.247469] wlcore:0x254[wlcore: 0x254RX:wlcore:0x254RX:wlcores:wlcores:0x601rate_rate] cmd configure (27) [82.261496] wlcore:cmd configure (27) [82.266948] wlcore:cmd configure (27) [82.272378] wlcore:cmd template_set 0 (Role 0) [82.278897] wlcore:cmd template_set 5 (Role 0)[82.285378] wlcore:cmd template_set 0 (Role 0) [82.28407_leid :rid:rf rle rid:rate、start rid:rid:rid:rid:x64_lecore = 0x28407_rid:rid:rle rid:rate rate rate rate rate 1、rid: 0x1 [82.300559] wlcore:mac80211 sta 0 state=0->1 [82.304954] wlcore:cmd ROC 1 (0) [82.310200] wlan0:将验证发送到 myMAC (try 1/3) [82.315908] wlcore:queue skb lid hlid 1 q 3 q 3 x 3 30[82.310200] wlan0:tr :tf 2:tr:tf 2 lid:tr:tf 2:tf 2:tf cid:tf:tf:tf 2 1 len:46 life:2000 mem:2 [82.332817] wlcore:IRQ work [82.33593] wlcore:INTR:0x44 (FW_Rx_counter = 3、drv_Rx_counter = 2、TX_Results_counter = 0) [82.344679] wlcore:上次发布的 desc = 0、当前350x [ 1 lcore:1、wlid = 1、wlcore TX 状态 id 0 skb 0x7209f610成功1 [82.3555908] wlcore:WL1271_ACX_INTR_DATA [82.359861] wlcore:WL1271_ACX_INTR_EVENT_A [82.364070] wlcore:mbox 0上的事件 [82.3667961] wlcore:wlcore_vector [82.43765] wlcore:wlcore:w387_vector :wlcore [82.387_wlcore:w248] wlcore:wlcore:wlcore:wlcore [82.3782.4248] wlcore:wlcore:wlcore:wlcore:wm:wm:wm:wlcore 0x40 (FW_Rx_COUNTER = 5、drv_Rx_counter = 3、TX_Results_counter = 0) [82.389050] wlcore:WL1271_ACX_INTR_DATA [82.393291] wlcore:Mgmt - Rx skb 0x4997dseq 1:30 9953 h1 [8393291] wlcore [经身份验证的 wlid:8993bt:0x993493b] wlid rf cabs:0x993bt 243bq 1 [0x993bt:0x993bt 243b] wlid 243b] wlid 243b] wlid rt mac80211 sta 0 state=1->2 [82.413270] wlcore:Mgmt - Rx skb 0xd99f5a77:311 seq 1654 hlid 1.
    wlan0:尝试与 myMAC 关联(ssid='msid' freq=2412 MHz)
    [82.431043] wlcore:queue skb hlid 1 q 3 len 127 [82.437723] wlcore:TX_ALLOCATE:Size:143、blocks:2、id:0 [82.443468] wlcore:TX_FLOAD_HDR:htr:1 len:143 life:2000 mem:2 [82.452543] wlcore:wlore :81.868] wlid:wlid:wlid:wlid:wlid:wlid:wlid:wlid 0x40 (FW_Rx_COUNTER = 6、drv_Rx_counter = 5、TX_Results_counter = 0) [82.464396] wlcore:上次发布的 desc = 1、电流 idx = 2 [82.470008] wlcore:TX 状态 id 0 skb 0x826715c0 Success 1 [82.475626] wlcore :0x9978_wltrl 数据:0x9978_wdr_lcore:0x9978_ltrl 235序列1656 hlid 1 [82.485985] wlcore:IRQ 工作 [ 82.486025] wlan0:从 myMAC 接收等频响应(capab=0x1411状态= 0 AID=1) [82.486044] wlcore:mac80211 sta 0 state=2->3 [ 82.501272] wacr_lcore = 0x486044] wlcore = 0x2.5r_r_tr = w40_lcore (wv_tr = w40_ltr = w40_ltr = w24_lcore = w24_ltr = v_ltr = w24_ltr = w24_ltr = w_ltr = w_ltr = w24_l 信标- Rx skb 0x4997dca1:311 seq 1655 hlid 1 [82.520477] wlcore:Mgmt - Rx skb 0x4997dca1:311 seq 1655 hlid 1 [82.526625] wlcore:data - Rx skb 0x7356616e:155 seq 0 hkb 1 [82.532541] wlcore:wlcf:wlcf cf 0x7356435] wlcore ACx ac cfg 3 cw_ming 3 cw_max 7 aifs 2 txop 1504 [82.542856] wlcore:cmd configure (3) [82.548182] wlcore:acx tid config [82.551610] wlcore:cmd configure (9) [82.558167] wlcore:mac80211 tx 2.511] wlcore [wlcore:w951955] ACx ac cfg 2 cw_ming 7 cw_max 15 aifs 2 txop 3008 [82.568437] wlcore:cmd configure (3) [82.573731] wlcore:ACx tid config [82.577163] wlcore:cmd configure (9) [82.582498] wlcore:IRQ work [82.5845] wlcore:intrr:wlcore 0x40 (FW_Rx_COUNTER = 9、drv_Rx_counter = 8、TX_Results_counter = 0) [82.594308] wlcore:WL1271_ACX_INTR_DATA [82.598522] wlcore:beacon - Rx skb 0x7356616e:SEQ 1657 hmGMT 1 [82.608311] wlcore [82.5381] wlcord:rf 801f trl trl trl trl trl:tf cf 0x73566168616311 :tx 801f cf cf [ 32.76351f 1:tl 1:tf 801f 801f 801f 801f 80 ACx ac cfg 0 CW_ming 15 CW_max 1023 aifs 3 txop 0 [82.621345] wlcore:cmd configure (3) [82.626741] wlcore:ACX tid config [82.630173] wlcore:cmd configure (9) [82.635537] wlcore:mac80211 tf 32.6393]] wlcore:wlcore ACX ac cfg 1 CW_ming 15 CW_max 1023 aifs 7 txop 0 [82.645848] wlcore:cmd configure (3) [82.651176] wlcore:ACX tid config [82.654613] wlcore:cmd configure (9) [82.659940] wlcore:[82.651176] wlcore:wlcore:0x802460866]更改了 wlcore [0x2938] wlcore 信息[0x200lcore 0] wlcore:w24608266024[wlcore 0x40 (FW_Rx_COUNTER = 10、drv_Rx_counter = 9、TX_Results_counter = 0) [82.663190] wlcore:WL1271_ACX_INTR_DATA [82.663451] wlcore:beacon - Rx skb 0xebd48aa6:seq 1658 hmgmt 1 [82.66342] wlcore [826968] wlb:rink 0x36961[8ax lcore [2.66458] wdlore:rb wlb:rb cmd configure (2) [82.701781] wlcore:ACX_SET_PREAMARY [82.705406] wlcore:cmd configure (30) [82.710806] wlcore:cmd template_set 6 (Role 0) [82.717305] wlcore:set ap probe request template [82.722042] wlcore: set 2模板:wlcore connection: md 2.736] wlcore parameters:w2.726] wlcore (wlcore connection: set 模板:w2.7362.7x 模板:wlcore connection: w2.726x 模板:wlcore connection CMD 配置(18) [82.740014] wlcore:ACX 保持活动模式:1 [82.744176] wlcore:CMD 配置(44) [82.749588] wlcore:ACX AID [82.752407] wlcore:CMD 配置(5) [82.7577368] wlcore:template 2.74960]设置 wlcore [ CMD 配置 (w2.7248] wlcore:wlcore = w2.7294] wlcore 设置 wlcore (w2.768x)[82.7294] wlcore = wlcore = wlcore = cmd configure (45) [82.773696] wlcore:leaving PSM [82.776865] wlcore:ACX bet enable [82.780294] wlcore:cmd configure (41) [82.785614] wlcore:cmd set ps mode [82.790642] wlcore:ACX rate policies [82.7980267] wlcore :配置(41)[82.785614] wlcore:配置 wlcore [0x8032] wlcore:0x8032] wlrate:配置 wlcore [0x99899899842] wlcore:wlrate:wlcore [2.7924] wlcore [0x8032]基本: cmd configure (27) [82.810320] wlcore:cmd configure (27) [82.815653] wlcore:ACX set cap HT_supp:1 HT_cap:6188发生率:0x1ffeff [82.822311] wlcore:cmd configure (86) [82.8276354] wlcore:ACX HT information:0x1ffeff [82.822311] wlcore: 配置(832352] wlcore (82.832x )[832352] wlcore:配置(832x lcore:832x) 0 [82.842093] wlcore:cmd configure (25) [82.847501] wlcore:IRQ work wlan0:关联到 myMAC [82.847955] wlan0:关联 的[82.857288] wlan0:将 TX 功率限制为 myMAC [82.425]标称的30 (30 - 0) dBm IN857TR
    然后 IRQ 被卡住(kworker 线程) 

    PID 用户 PR NI virt RES SHR S %CPU %MEM TIME+命令
    57 root -50 0 0 0 0 0 R 100.0 0.0 31:53.13 kworker/1:1+事件

    是否可以使用应用的 preemper-RT 修补程序进行测试?

    我认为这是一个与此驱动程序使用 preemper-RT 的自旋锁相关的问题。

    此致、
    Romain

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!  

    与 R8.8关联的最新固件为8.9.0.0.86。  

    Romain Naour 说:
    是否可以使用应用的 preeme-RT 修补程序进行测试?

    您能不能告诉我此处的请求是什么?  

    新版本是否还包括请求补丁?   有关 R8.8中组件的详细信息、请参阅 www.ti.com/.../swru561a.pdf  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我查看了 Yocto 方法所使用的存储库、以获取最新固件  8.9.0.0.83。

    我更新到了  8.9.0.0.86。

    但是、即使不使用 wpa_supplicant、我也会重现此问题:

    $ ifconfig wlan0 up

    我将 TI SDK 6.3用作 AM574x 的基础、应  使用预编译6.03 Linux-RT 映像在具有 WL1835MODCOM8B 器件的 IDK574x 电路板上轻松重现此问题。

    我有一个 am574x 板、但我没有模块 WL1835MODCOM8B
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!  

    R8.8通过 LTS 内核进行了验证、运行正常。默认情况下、wlan0接口应处于启动状态、而无需发出"ifconfig wlan0 up"命令。 我将在内部进行检查、并再次与您进行检查。  

    此致、  

    Sudharshan K N   

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!  

    此外、您能否尝试在 wlan0接口启动后禁用 ELP 并检查行为?  

    iw wlan0将 power_save 设置为 off

    echo 0 >/sys/kernel/debug/ieee80211/phy0/wlcore/sleep_auth

    此致、  

    Sudharshan K N  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    谢谢、我已经尝试禁用 ELP 功能。

    我使用 ftrace 来调试 wlcore 驱动程序、并在发生错误后注意到 hrtimer 有一些奇怪的情况。

    我从 preemst-RT v4.19-RT 稳定分支回退此提交:

    应用此承诺后、WiFi 将按预期工作!

    在内核 4.19.115-rt50中修复了该错误、但 TI SDK 6.3使用了内核4.19.94-rt39、其中引入了该错误。

    关于适用于 AM57xx 器件的 TI SDK 7.x 您是否有正式发布日期?

    此致、
    Romain

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!  

    我很高兴知道问题已经解决!! 有关处理器 SDK 的发布日期、请向处理器团队提交另一个 E2E 申请。 他们很乐意为您提供帮助。  

    此致、  

    Sudharshan K N