This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHXL-CC3235SF:将 MQTT 客户端添加到 Open Box 演示应用

Guru**** 2581345 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/996678/launchxl-cc3235sf-adding-mqtt-client-to-open-box-demo-application

器件型号:LAUNCHXL-CC3235SF

您好!

我正在尝试将 MQTT 客户端代码与 Open Box 应用程序合并。 我已经为 MQTT 客户端创建了单独的线程、并在连接到 AP 并获取 IP 地址后初始化 MQTT 连接。 我可以通过运行单独的代码连接到 MQTT 代理、但在合并代码 MQTT 客户端后无法正常工作。 我在这里附上了我的 MQTT 代码文件。 合并此代码的主要目的是在配置 WiFi 网络后启动 MQTT 连接。

/*
 * Copyright (c) 2016, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

/*****************************************************************************

   Application Name     -   Getting started with OUT_OF_BOX
   Application Overview -    This application demonstrates the Out of Box 
   Experience with CC32xx LaunchPad.
                                      It highlights the following features:
                          1. easy and straight-forward provisioning methods
                          2. easy access to CC32xx Using internal HTTP server
                          3. attractive Demos showing LAN communication

   Application Details  - Refer to 'Out of box' README.html

*****************************************************************************/

//****************************************************************************
//
//! \addtogroup out_of_box
//! @{
//
//****************************************************************************

/* Example/Board Header files */
#include "out_of_box.h"
#include "provisioning_task.h"
#include "link_local_task.h"
#include "ota_task.h"

/* TI-DRIVERS Header files */
#include <ti/drivers/net/wifi/simplelink.h>
#include <ti/drivers/SPI.h>
#include <ti_drivers_config.h>

/* driverlib Header files */
#include <ti/devices/cc32xx/inc/hw_types.h>
#include <ti/devices/cc32xx/inc/hw_memmap.h>
#include <ti/devices/cc32xx/driverlib/rom.h>
#include <ti/devices/cc32xx/driverlib/rom_map.h>
#include <ti/devices/cc32xx/driverlib/prcm.h>

/* POSIX Header files */
#include <mqueue.h>

int wifi_flag = 0;  // check the wifi connection

//************************************MQTT Files***************************************
#include <unistd.h>
#include <stdint.h>
#include <stddef.h>
#include <stdlib.h>

#include <pthread.h>
#include <ti/drivers/net/wifi/simplelink.h>

/* TI Driver Includes */
#include <ti/drivers/GPIO.h>
#include <ti/drivers/SPI.h>

/* Application Headers */
//#include "network_if.h"
#include "mqtt_if.h"
#include "debug_if.h"

/* Driver configuration */
#include "ti_drivers_config.h"


#define MQTT_MODULE_TASK_PRIORITY   9
 #define MQTT_MODULE_TASK_STACK_SIZE 4096

 #define MQTT_WILL_TOPIC             "cc32xx_will_topic"
 #define MQTT_WILL_MSG               "will_msg_works"
 #define MQTT_WILL_QOS               MQTT_QOS_0
 #define MQTT_WILL_RETAIN            false

 #define MQTT_CLIENT_PASSWORD        NULL
 #define MQTT_CLIENT_USERNAME        NULL
 #define MQTT_CLIENT_KEEPALIVE       0
 #define MQTT_CLIENT_CLEAN_CONNECT   true
 #define MQTT_CLIENT_MQTT_V3_1       false
 #define MQTT_CLIENT_BLOCKING_SEND   true

 #define MQTT_CONNECTION_FLAGS           MQTTCLIENT_NETCONN_URL | MQTTCLIENT_NETCONN_SEC //|MQTTCLIENT_NETCONN_SKIP_CERTIFICATE_CATALOG_VERIFICATION |MQTTCLIENT_NETCONN_SKIP_DOMAIN_NAME_VERIFICATION //MQTTCLIENT_NETCONN_URL | MQTTCLIENT_NETCONN_SEC // MQTTCLIENT_NETCONN_IP4 | MQTTCLIENT_NETCONN_SEC
 #define MQTT_CONNECTION_ADDRESS         "test.mosquitto.org"
 #define MQTT_CONNECTION_PORT_NUMBER     1883

#define SL_TASKSTACKSIZE            2048
#define SPAWN_TASK_PRIORITY         9

char ClientId[13] = {'piggy'};

MQTT_IF_InitParams_t mqttInitParams =
{
     MQTT_MODULE_TASK_STACK_SIZE,   // stack size for mqtt module
     MQTT_MODULE_TASK_PRIORITY      // thread priority for MQTT
};

MQTTClient_Will mqttWillParams =
{
     MQTT_WILL_TOPIC,    // will topic
     MQTT_WILL_MSG,      // will message
     MQTT_WILL_QOS,      // will QoS
     MQTT_WILL_RETAIN    // retain flag
};

MQTT_IF_ClientParams_t mqttClientParams =
{
     ClientId,                  // client ID
     MQTT_CLIENT_USERNAME,      // user name
     MQTT_CLIENT_PASSWORD,      // password
     MQTT_CLIENT_KEEPALIVE,     // keep-alive time
     MQTT_CLIENT_CLEAN_CONNECT, // clean connect flag
     MQTT_CLIENT_MQTT_V3_1,     // true = 3.1, false = 3.1.1
     MQTT_CLIENT_BLOCKING_SEND, // blocking send flag
     &mqttWillParams            // will parameters
};

MQTTClient_ConnParams mqttConnParams =
{
     MQTT_CONNECTION_FLAGS,         // connection flags
     MQTT_CONNECTION_ADDRESS,       // server address
     MQTT_CONNECTION_PORT_NUMBER,   // port number of MQTT server
     0,                             // method for secure socket
     0,                             // cipher for secure socket
     0,                             // number of files for secure connection
     NULL                           // secure files
};


int32_t SetClientIdNamefromMacAddress()
{
    int32_t ret = 0;
    uint8_t Client_Mac_Name[2];
    uint8_t Index;
    uint16_t macAddressLen = SL_MAC_ADDR_LEN;
    uint8_t macAddress[SL_MAC_ADDR_LEN];

    /*Get the device Mac address */
    ret = sl_NetCfgGet(SL_NETCFG_MAC_ADDRESS_GET, 0, &macAddressLen,
                       &macAddress[0]);

    /*When ClientID isn't set, use the mac address as ClientID               */
    if(ClientId[0] == '\0')
    {
        /*6 bytes is the length of the mac address                           */
        for(Index = 0; Index < SL_MAC_ADDR_LEN; Index++)
        {
            /*Each mac address byte contains two hexadecimal characters      */
            /*Copy the 4 MSB - the most significant character                */
            Client_Mac_Name[0] = (macAddress[Index] >> 4) & 0xf;
            /*Copy the 4 LSB - the least significant character               */
            Client_Mac_Name[1] = macAddress[Index] & 0xf;

            if(Client_Mac_Name[0] > 9)
            {
                /*Converts and copies from number that is greater than 9 in  */
                /*hexadecimal representation (a to f) into ascii character   */
                ClientId[2 * Index] = Client_Mac_Name[0] + 'a' - 10;
            }
            else
            {
                /*Converts and copies from number 0 - 9 in hexadecimal       */
                /*representation into ascii character                        */
                ClientId[2 * Index] = Client_Mac_Name[0] + '0';
            }
            if(Client_Mac_Name[1] > 9)
            {
                /*Converts and copies from number that is greater than 9 in  */
                /*hexadecimal representation (a to f) into ascii character   */
                ClientId[2 * Index + 1] = Client_Mac_Name[1] + 'a' - 10;
            }
            else
            {
                /*Converts and copies from number 0 - 9 in hexadecimal       */
                /*representation into ascii character                        */
                ClientId[2 * Index + 1] = Client_Mac_Name[1] + '0';
            }
        }
    }
    return(ret);
}

void MQTT_EventCallback(int32_t event)
{
    switch(event){
        case MQTT_EVENT_CONNACK:
        {
            LOG_INFO("MQTT_EVENT_CONNACK\r\n");
            break;
        }
        case MQTT_EVENT_CLIENT_DISCONNECT:
        {
            LOG_INFO("MQTT_EVENT_CLIENT_DISCONNECT\r\n");
            break;
        }
        case MQTT_EVENT_SERVER_DISCONNECT:
        {
            LOG_INFO("MQTT_EVENT_SERVER_DISCONNECT\r\n");
            break;
        }
        case MQTT_EVENT_DESTROY:
        {
            LOG_INFO("MQTT_EVENT_DESTROY\r\n");
            break;
        }
        default:
        {
            LOG_INFO("Unknown MQTT event\r\n");
            break;
        }
    }
}

#define SSID_NAME "katahdin"
#define SECURITY_KEY "civicfortunercrvdiscovery"
/* Security type (OPEN or WEP or WPA)                                         */
#define SECURITY_TYPE           SL_WLAN_SEC_TYPE_WPA_WPA2

int WifiInit(){
     int32_t ret;
     SlWlanSecParams_t security_params;
     pthread_t spawn_thread = (pthread_t) NULL;
     pthread_attr_t pattrs_spawn;
     struct sched_param pri_param;

     pthread_attr_init(&pattrs_spawn);
     pri_param.sched_priority = SPAWN_TASK_PRIORITY;
     ret = pthread_attr_setschedparam(&pattrs_spawn, &pri_param);
     ret |= pthread_attr_setstacksize(&pattrs_spawn, SL_TASKSTACKSIZE);
     ret |= pthread_attr_setdetachstate(&pattrs_spawn, PTHREAD_CREATE_DETACHED);
     ret = pthread_create(&spawn_thread, &pattrs_spawn, sl_Task, NULL);
     if(ret != 0){
         LOG_ERROR("could not create simplelink task\n\r");
         while(1);
     }

/*     Network_IF_ResetMCUStateMachine();

     Network_IF_DeInitDriver();

     ret = Network_IF_InitDriver(ROLE_STA);
     if(ret < 0){
         LOG_ERROR("Failed to start SimpleLink Device\n\r");
         while(1);
     }*/

     SetClientIdNamefromMacAddress();

     /*security_params.Key = (signed char*)SECURITY_KEY;
     security_params.KeyLen = strlen(SECURITY_KEY);
     security_params.Type = SECURITY_TYPE;

     ret = Network_IF_ConnectAP(SSID_NAME, security_params);
     if(ret < 0){
         LOG_ERROR("Connection to an AP failed\n\r");
     }
     else{
         ret = sl_WlanProfileAdd((signed char*)SSID_NAME, strlen(SSID_NAME), 0, &security_params, NULL, 7, 0);
         if(ret < 0){
             LOG_ERROR("failed to add profile %s\r\n", SSID_NAME);
         }
         else{
             LOG_INFO("profile added %s\r\n", SSID_NAME);
         }
     }*/

     return ret;
 }

//*************************************************************************




/****************************************************************************
                      LOCAL FUNCTION PROTOTYPES
****************************************************************************/
//*****************************************************************************
//
//! Application Boarders display on UART
//!
//! \param  ch - Character to be displayed , n - number of time to display
//!
//! \return none
//!
//*****************************************************************************
void printBorder(char ch,
                 int n);
//*****************************************************************************
//
//! Application startup display on UART
//!
//! \param  none
//!
//! \return none
//!
//*****************************************************************************
int32_t DisplayBanner(char * AppName,
                      char * AppVer);

//*****************************************************************************
//
//! This function initializes the application variables
//!
//! \param    None
//!
//! \return None
//!
//*****************************************************************************
static void InitializeAppVariables(void);

//*****************************************************************************
//
//! This  function clears and enables a GPIO pin interrupt flag
//!
//! \param    index - GPIO index
//!
//! \return None
//!
//*****************************************************************************
static void GPIO_clearAndEnable(uint8_t index);

/****************************************************************************
                      GLOBAL VARIABLES
****************************************************************************/
pthread_t gProvisioningThread = (pthread_t)NULL;
pthread_t gLinklocalThread = (pthread_t)NULL;
pthread_t gControlThread = (pthread_t)NULL;
pthread_t gOtaThread = (pthread_t)NULL;
pthread_t gSpawnThread = (pthread_t)NULL;
pthread_t mq_thread = (pthread_t)NULL;
pthread_t aws_thread = (pthread_t)NULL;

/* message queue for control messages */
mqd_t controlMQueue;

OutOfBox_CB OutOfBox_ControlBlock;

/*****************************************************************************
                  Callback Functions
*****************************************************************************/

//*****************************************************************************
//
//! The Function Handles WLAN Events
//!
//! \param[in]  pWlanEvent - Pointer to WLAN Event Info
//!
//! \return None
//!
//*****************************************************************************
void SimpleLinkWlanEventHandler(SlWlanEvent_t *pWlanEvent)
{
    switch(pWlanEvent->Id)
    {
    case SL_WLAN_EVENT_CONNECT:
    {
        SET_STATUS_BIT(OutOfBox_ControlBlock.status, AppStatusBits_Connection);
        CLR_STATUS_BIT(OutOfBox_ControlBlock.status, AppStatusBits_IpAcquired);
        CLR_STATUS_BIT(OutOfBox_ControlBlock.status,
                       AppStatusBits_Ipv6lAcquired);
        CLR_STATUS_BIT(OutOfBox_ControlBlock.status,
                       AppStatusBits_Ipv6gAcquired);

        /*
           Information about the connected AP (like name, MAC etc) will be
           available in 'slWlanConnectAsyncResponse_t'-Applications
           can use it if required:

           slWlanConnectAsyncResponse_t *pEventData = NULL;
           pEventData = &pWlanEvent->EventData.STAandP2PModeWlanConnected;
         */

        /* Copy new connection SSID and BSSID to global parameters */
        memcpy(OutOfBox_ControlBlock.connectionSSID,
               pWlanEvent->Data.Connect.SsidName,
               pWlanEvent->Data.Connect.SsidLen);

        OutOfBox_ControlBlock.ssidLen = pWlanEvent->Data.Connect.SsidLen;

        memcpy(OutOfBox_ControlBlock.connectionBSSID,
               pWlanEvent->Data.Connect.Bssid,
               SL_WLAN_BSSID_LENGTH);

        UART_PRINT(
            "[WLAN EVENT] STA Connected to the AP: %s ,"
            "BSSID: %x:%x:%x:%x:%x:%x\n\r",
            OutOfBox_ControlBlock.connectionSSID,
            OutOfBox_ControlBlock.connectionBSSID[0],
            OutOfBox_ControlBlock.connectionBSSID[1],
            OutOfBox_ControlBlock.connectionBSSID[2],
            OutOfBox_ControlBlock.connectionBSSID[3],
            OutOfBox_ControlBlock.connectionBSSID[4],
            OutOfBox_ControlBlock.connectionBSSID[5]);

        wifi_flag = 1;
        sem_post(&Provisioning_ControlBlock.connectionAsyncEvent);
    }
    break;

    case SL_WLAN_EVENT_DISCONNECT:
    {
        SlWlanEventDisconnect_t*    pEventData = NULL;

        CLR_STATUS_BIT(OutOfBox_ControlBlock.status, AppStatusBits_Connection);
        CLR_STATUS_BIT(OutOfBox_ControlBlock.status, AppStatusBits_IpAcquired);
        CLR_STATUS_BIT(OutOfBox_ControlBlock.status,
                       AppStatusBits_Ipv6lAcquired);
        CLR_STATUS_BIT(OutOfBox_ControlBlock.status,
                       AppStatusBits_Ipv6gAcquired);

        pEventData = &pWlanEvent->Data.Disconnect;

        /*  If the user has initiated 'Disconnect' request,
            'reason_code' is SL_WLAN_DISCONNECT_USER_INITIATED.
         */
        if(SL_WLAN_DISCONNECT_USER_INITIATED == pEventData->ReasonCode)
        {
            UART_PRINT(
                "[WLAN EVENT]Device disconnected from the "
                "AP: %s, BSSID: %x:%x:%x:%x:%x:%x "
                "on application's request \n\r",
                OutOfBox_ControlBlock.connectionSSID,
                OutOfBox_ControlBlock.connectionBSSID[0],
                OutOfBox_ControlBlock.connectionBSSID[1],
                OutOfBox_ControlBlock.connectionBSSID[2],
                OutOfBox_ControlBlock.connectionBSSID[3],
                OutOfBox_ControlBlock.connectionBSSID[4],
                OutOfBox_ControlBlock.connectionBSSID[5]);
        }
        else
        {
            UART_PRINT(
                "[WLAN ERROR]Device disconnected from the AP AP: %s,"
                "BSSID: %x:%x:%x:%x:%x:%x on an ERROR..!! \n\r",
                OutOfBox_ControlBlock.connectionSSID,
                OutOfBox_ControlBlock.connectionBSSID[0],
                OutOfBox_ControlBlock.connectionBSSID[1],
                OutOfBox_ControlBlock.connectionBSSID[2],
                OutOfBox_ControlBlock.connectionBSSID[3],
                OutOfBox_ControlBlock.connectionBSSID[4],
                OutOfBox_ControlBlock.connectionBSSID[5]);
        }
        memset(OutOfBox_ControlBlock.connectionSSID, 0,
               sizeof(OutOfBox_ControlBlock.connectionSSID));
        memset(OutOfBox_ControlBlock.connectionBSSID, 0,
               sizeof(OutOfBox_ControlBlock.connectionBSSID));
    }
    break;

    case SL_WLAN_EVENT_STA_ADDED:
    {
        UART_PRINT(
            "[WLAN EVENT] External Station connected to SimpleLink AP\r\n");

        UART_PRINT("[WLAN EVENT] STA BSSID: %02x:%02x:%02x:%02x:%02x:%02x\r\n",
                   pWlanEvent->Data.STAAdded.Mac[0],
                   pWlanEvent->Data.STAAdded.Mac[1],
                   pWlanEvent->Data.STAAdded.Mac[2],
                   pWlanEvent->Data.STAAdded.Mac[3],
                   pWlanEvent->Data.STAAdded.Mac[4],
                   pWlanEvent->Data.STAAdded.Mac[5]);
    }
    break;

    case SL_WLAN_EVENT_STA_REMOVED:
    {
        UART_PRINT(
           "[WLAN EVENT] External Station disconnected from SimpleLink AP\r\n");
    }
    break;

    case SL_WLAN_EVENT_PROVISIONING_PROFILE_ADDED:
    {
        UART_PRINT("[WLAN EVENT] Profile Added\r\n");
    }
    break;

    case SL_WLAN_EVENT_PROVISIONING_STATUS:
    {
        uint16_t status =
            pWlanEvent->Data.ProvisioningStatus.ProvisioningStatus;
        switch(status)
        {
        case SL_WLAN_PROVISIONING_GENERAL_ERROR:
        case SL_WLAN_PROVISIONING_ERROR_ABORT:
        {
            UART_PRINT("[WLAN EVENT] Provisioning Error status=%d\r\n",status);
            SignalProvisioningEvent(PrvnEvent_Error);
        }
        break;
        case SL_WLAN_PROVISIONING_ERROR_ABORT_INVALID_PARAM:
        case SL_WLAN_PROVISIONING_ERROR_ABORT_HTTP_SERVER_DISABLED:
        case SL_WLAN_PROVISIONING_ERROR_ABORT_PROFILE_LIST_FULL:
        {
            UART_PRINT("[WLAN EVENT] Provisioning Error status=%d\r\n",status);
            SignalProvisioningEvent(PrvnEvent_StartFailed);
        }
        break;
        case SL_WLAN_PROVISIONING_ERROR_ABORT_PROVISIONING_ALREADY_STARTED:
        {
            UART_PRINT("[WLAN EVENT] Provisioning already started");
        }
        break;

        case SL_WLAN_PROVISIONING_CONFIRMATION_STATUS_FAIL_NETWORK_NOT_FOUND:
        {
            UART_PRINT("[WLAN EVENT] Confirmation fail: network not found\r\n");
            SignalProvisioningEvent(PrvnEvent_ConfirmationFailed);
        }
        break;

        case SL_WLAN_PROVISIONING_CONFIRMATION_STATUS_FAIL_CONNECTION_FAILED:
        {
            UART_PRINT("[WLAN EVENT] Confirmation fail: Connection failed\r\n");
            SignalProvisioningEvent(PrvnEvent_ConfirmationFailed);
        }
        break;

        case
            SL_WLAN_PROVISIONING_CONFIRMATION_STATUS_CONNECTION_SUCCESS_IP_NOT_ACQUIRED
            :
        {
            UART_PRINT(
                "[WLAN EVENT] Confirmation fail: IP address not acquired\r\n");
            SignalProvisioningEvent(PrvnEvent_ConfirmationFailed);
        }
        break;

        case SL_WLAN_PROVISIONING_CONFIRMATION_STATUS_SUCCESS_FEEDBACK_FAILED:
        {
            UART_PRINT(
                "[WLAN EVENT] Connection Success "
                "(feedback to Smartphone app failed)\r\n");
            SignalProvisioningEvent(PrvnEvent_ConfirmationFailed);
        }
        break;

        case SL_WLAN_PROVISIONING_CONFIRMATION_STATUS_SUCCESS:
        {
            UART_PRINT("[WLAN EVENT] Confirmation Success!\r\n");
            SignalProvisioningEvent(PrvnEvent_ConfirmationSuccess);
        }
        break;

        case SL_WLAN_PROVISIONING_AUTO_STARTED:
        {
            UART_PRINT("[WLAN EVENT] Auto-Provisioning Started\r\n");
            /* stop auto provisioning - 
                 may trigger in case of returning to default */
            SignalProvisioningEvent(PrvnEvent_Stopped);
        }
        break;

        case SL_WLAN_PROVISIONING_STOPPED:
        {
            UART_PRINT("[WLAN EVENT] Provisioning stopped\r\n");
            if(ROLE_STA == pWlanEvent->Data.ProvisioningStatus.Role)
            {
                UART_PRINT(" [WLAN EVENT] - WLAN Connection Status:%d\r\n",
                           pWlanEvent->Data.ProvisioningStatus.WlanStatus);

                if(SL_WLAN_STATUS_CONNECTED ==
                   pWlanEvent->Data.ProvisioningStatus.WlanStatus)
                {
                    UART_PRINT(" [WLAN EVENT] - Connected to SSID:%s\r\n",
                               pWlanEvent->Data.ProvisioningStatus.Ssid);

                    memcpy (OutOfBox_ControlBlock.connectionSSID,
                            pWlanEvent->Data.ProvisioningStatus.Ssid,
                            pWlanEvent->Data.ProvisioningStatus.Ssidlen);
                    OutOfBox_ControlBlock.ssidLen =
                        pWlanEvent->Data.ProvisioningStatus.Ssidlen;

                    /* Provisioning is stopped by the device and
                       provisioning is done successfully */
                    SignalProvisioningEvent(PrvnEvent_Stopped);

                    break;
                }
                else
                {
                    CLR_STATUS_BIT(OutOfBox_ControlBlock.status,
                                   AppStatusBits_Connection);
                    CLR_STATUS_BIT(OutOfBox_ControlBlock.status,
                                   AppStatusBits_IpAcquired);
                    CLR_STATUS_BIT(OutOfBox_ControlBlock.status,
                                   AppStatusBits_Ipv6lAcquired);
                    CLR_STATUS_BIT(OutOfBox_ControlBlock.status,
                                   AppStatusBits_Ipv6gAcquired);

                    /* Provisioning is stopped by the device and provisioning 
                    is not done yet, still need to connect to AP */
                    SignalProvisioningEvent(PrvnEvent_WaitForConn);

                    break;
                }
            }
        }

            SignalProvisioningEvent(PrvnEvent_Stopped);

            break;

        case SL_WLAN_PROVISIONING_SMART_CONFIG_SYNCED:
        {
            UART_PRINT("[WLAN EVENT] Smart Config Synced!\r\n");
        }
        break;

        case SL_WLAN_PROVISIONING_CONFIRMATION_WLAN_CONNECT:
        {
            SET_STATUS_BIT(OutOfBox_ControlBlock.status,
                           AppStatusBits_Connection);
            CLR_STATUS_BIT(OutOfBox_ControlBlock.status,
                           AppStatusBits_IpAcquired);
            CLR_STATUS_BIT(OutOfBox_ControlBlock.status,
                           AppStatusBits_Ipv6lAcquired);
            CLR_STATUS_BIT(OutOfBox_ControlBlock.status,
                           AppStatusBits_Ipv6gAcquired);

            UART_PRINT("[WLAN EVENT] Connection to AP succeeded\r\n");


        }
        break;

        case SL_WLAN_PROVISIONING_CONFIRMATION_IP_ACQUIRED:
        {
            SET_STATUS_BIT(OutOfBox_ControlBlock.status,
                           AppStatusBits_IpAcquired);

            UART_PRINT("[WLAN EVENT] IP address acquired\r\n");
            wifi_flag = 1;



        }
        break;

        case SL_WLAN_PROVISIONING_SMART_CONFIG_SYNC_TIMEOUT:
        {
            UART_PRINT("[WLAN EVENT] Smart Config Sync timeout\r\n");
        }
        break;

        default:
        {
            UART_PRINT("[WLAN EVENT] Unknown Provisioning Status: %d\r\n",
                       pWlanEvent->Data.ProvisioningStatus.ProvisioningStatus);
        }
        break;
        }
    }
    break;

    default:
    {
        UART_PRINT("[WLAN EVENT] Unexpected event [0x%x]\n\r",
                   pWlanEvent->Id);

        SignalProvisioningEvent(PrvnEvent_Error);
    }
    break;
    }
}

//*****************************************************************************
//
//! The Function Handles the Fatal errors
//!
//! \param[in]  slFatalErrorEvent - Pointer to Fatal Error Event info
//!
//! \return None
//!
//*****************************************************************************
void SimpleLinkFatalErrorEventHandler(SlDeviceFatal_t *slFatalErrorEvent)
{
    uint8_t msg = 4;
    int32_t msgqRetVal;

    switch(slFatalErrorEvent->Id)
    {
    case SL_DEVICE_EVENT_FATAL_DEVICE_ABORT:
    {
        UART_PRINT("[ERROR] - FATAL ERROR: Abort NWP event detected: "
                   "AbortType=%d, AbortData=0x%x\n\r",
                   slFatalErrorEvent->Data.DeviceAssert.Code,
                   slFatalErrorEvent->Data.DeviceAssert.Value);
    }
    break;

    case SL_DEVICE_EVENT_FATAL_DRIVER_ABORT:
    {
        UART_PRINT("[ERROR] - FATAL ERROR: Driver Abort detected. \n\r");
    }
    break;

    case SL_DEVICE_EVENT_FATAL_NO_CMD_ACK:
    {
        UART_PRINT("[ERROR] - FATAL ERROR: No Cmd Ack detected "
                   "[cmd opcode = 0x%x] \n\r",
                   slFatalErrorEvent->Data.NoCmdAck.Code);
    }
    break;

    case SL_DEVICE_EVENT_FATAL_SYNC_LOSS:
    {
        UART_PRINT("[ERROR] - FATAL ERROR: Sync loss detected n\r");
    }
    break;

    case SL_DEVICE_EVENT_FATAL_CMD_TIMEOUT:
    {
        UART_PRINT("[ERROR] - FATAL ERROR: Async event timeout detected "
                   "[event opcode =0x%x]  \n\r",
                   slFatalErrorEvent->Data.CmdTimeout.Code);
    }
    break;

    default:
        UART_PRINT("[ERROR] - FATAL ERROR: Unspecified error detected \n\r");
        break;
    }

    msgqRetVal = mq_send(controlMQueue, (char *)&msg, 1, 0);
    if(msgqRetVal < 0)
    {
        UART_PRINT("[Control task] could not send element to msg queue\n\r");
        while(1)
        {
            ;
        }
    }
}

//*****************************************************************************
//
//! This function handles network events such as IP acquisition, IP
//!           leased, IP released etc.
//!
//! \param[in]  pNetAppEvent - Pointer to NetApp Event Info
//!
//! \return None
//!
//*****************************************************************************
void SimpleLinkNetAppEventHandler(SlNetAppEvent_t *pNetAppEvent)
{
    SlNetAppEventData_u *pNetAppEventData = NULL;

    if(NULL == pNetAppEvent)
    {
        return;
    }

    pNetAppEventData = &pNetAppEvent->Data;

    switch(pNetAppEvent->Id)
    {
    case SL_NETAPP_EVENT_IPV4_ACQUIRED:
    {
        SlIpV4AcquiredAsync_t   *pEventData = NULL;

        SET_STATUS_BIT(OutOfBox_ControlBlock.status, AppStatusBits_IpAcquired);

        /* Ip Acquired Event Data */
        pEventData = &pNetAppEvent->Data.IpAcquiredV4;

        /* Gateway IP address */
        OutOfBox_ControlBlock.gatewayIP = pEventData->Gateway;

        UART_PRINT("[NETAPP EVENT] IP Acquired: IP=%d.%d.%d.%d , "
                   "Gateway=%d.%d.%d.%d\n\r",
                   SL_IPV4_BYTE(pNetAppEvent->Data.IpAcquiredV4.Ip,3),
                   SL_IPV4_BYTE(pNetAppEvent->Data.IpAcquiredV4.Ip,2),
                   SL_IPV4_BYTE(pNetAppEvent->Data.IpAcquiredV4.Ip,1),
                   SL_IPV4_BYTE(pNetAppEvent->Data.IpAcquiredV4.Ip,0),
                   SL_IPV4_BYTE(pNetAppEvent->Data.IpAcquiredV4.Gateway,3),
                   SL_IPV4_BYTE(pNetAppEvent->Data.IpAcquiredV4.Gateway,2),
                   SL_IPV4_BYTE(pNetAppEvent->Data.IpAcquiredV4.Gateway,1),
                   SL_IPV4_BYTE(pNetAppEvent->Data.IpAcquiredV4.Gateway,0));

        sem_post(&Provisioning_ControlBlock.connectionAsyncEvent);
    }
    break;

    case SL_NETAPP_EVENT_IPV6_ACQUIRED:
    {
        if(!GET_STATUS_BIT(OutOfBox_ControlBlock.status,
                           AppStatusBits_Ipv6lAcquired))
        {
            SET_STATUS_BIT(OutOfBox_ControlBlock.status,
                           AppStatusBits_Ipv6lAcquired);
            UART_PRINT("[NETAPP EVENT] Local IPv6 Acquired\n\r");
        }
        else
        {
            SET_STATUS_BIT(OutOfBox_ControlBlock.status,
                           AppStatusBits_Ipv6gAcquired);
            UART_PRINT("[NETAPP EVENT] Global IPv6 Acquired\n\r");
        }

        sem_post(&Provisioning_ControlBlock.connectionAsyncEvent);
    }
    break;

    case SL_NETAPP_EVENT_DHCPV4_LEASED:
    {
        SET_STATUS_BIT(OutOfBox_ControlBlock.status, AppStatusBits_IpLeased);

        UART_PRINT(
            "[NETAPP EVENT] IPv4 leased %d.%d.%d.%d for "
            "device %02x:%02x:%02x:%02x:%02x:%02x\n\r", \
            (uint8_t)SL_IPV4_BYTE(pNetAppEventData->IpLeased.IpAddress,3), \
            (uint8_t)SL_IPV4_BYTE(pNetAppEventData->IpLeased.IpAddress,2), \
            (uint8_t)SL_IPV4_BYTE(pNetAppEventData->IpLeased.IpAddress,1), \
            (uint8_t)SL_IPV4_BYTE(pNetAppEventData->IpLeased.IpAddress,0), \
            pNetAppEventData->IpLeased.Mac[0], \
            pNetAppEventData->IpLeased.Mac[1], \
            pNetAppEventData->IpLeased.Mac[2], \
            pNetAppEventData->IpLeased.Mac[3], \
            pNetAppEventData->IpLeased.Mac[4], \
            pNetAppEventData->IpLeased.Mac[5]);
    }
    break;

    case SL_NETAPP_EVENT_DHCPV4_RELEASED:
    {
        CLR_STATUS_BIT(OutOfBox_ControlBlock.status, AppStatusBits_IpLeased);

        UART_PRINT(
            "[NETAPP EVENT] IPv4 released %d.%d.%d.%d for "
            "device %02x:%02x:%02x:%02x:%02x:%02x\n\r", \
            (uint8_t)SL_IPV4_BYTE(pNetAppEventData->IpReleased.IpAddress,
                                  3), \
            (uint8_t)SL_IPV4_BYTE(pNetAppEventData->IpReleased.IpAddress,
                                  2), \
            (uint8_t)SL_IPV4_BYTE(pNetAppEventData->IpReleased.IpAddress,
                                  1), \
            (uint8_t)SL_IPV4_BYTE(pNetAppEventData->IpReleased.IpAddress,
                                  0), \
            pNetAppEventData->IpReleased.Mac[0], \
            pNetAppEventData->IpReleased.Mac[1], \
            pNetAppEventData->IpReleased.Mac[2], \
            pNetAppEventData->IpReleased.Mac[3], \
            pNetAppEventData->IpReleased.Mac[4], \
            pNetAppEventData->IpReleased.Mac[5]);

        UART_PRINT("Reason: ");
        switch(pNetAppEventData->IpReleased.Reason)
        {
        case SL_IP_LEASE_PEER_RELEASE: UART_PRINT("Peer released\n\r");
            break;

        case SL_IP_LEASE_PEER_DECLINE: UART_PRINT("Peer declined\n\r");
            break;

        case SL_IP_LEASE_EXPIRED: UART_PRINT("Lease expired\n\r");
            break;
        }
    }
    break;

    case SL_NETAPP_EVENT_DHCP_IPV4_ACQUIRE_TIMEOUT:
    {
        UART_PRINT("[NETAPP EVENT] DHCP IPv4 Acquire timeout\n\r");
    }
    break;

    default:
    {
        UART_PRINT("[NETAPP EVENT] Unexpected event [0x%x] \n\r",
                   pNetAppEvent->Id);
    }
    break;
    }
}

//*****************************************************************************
//
//! This function handles HTTP server events
//!
//! \param[in]  pServerEvent    - Contains the relevant event information
//! \param[in]  pServerResponse - Should be filled by the user with the
//!                               relevant response information
//!
//! \return None
//!
//****************************************************************************
void SimpleLinkHttpServerEventHandler(SlNetAppHttpServerEvent_t *pHttpEvent,
    SlNetAppHttpServerResponse_t *
    pHttpResponse)
{
    /* Unused in this application */
    UART_PRINT("[HTTP SERVER EVENT] Unexpected HTTP server event \n\r");
}

//*****************************************************************************
//
//! This function handles General Events
//!
//! \param[in]  pDevEvent - Pointer to General Event Info
//!
//! \return None
//!
//*****************************************************************************
void SimpleLinkGeneralEventHandler(SlDeviceEvent_t *pDevEvent)
{
    uint8_t msg = 4;
    int32_t msgqRetVal;

    /*
        Most of the general errors are not FATAL are are to be handled
        appropriately by the application.
     */
    if(NULL == pDevEvent)
    {
        return;
    }
    switch(pDevEvent->Id)
    {
    case SL_DEVICE_EVENT_RESET_REQUEST:
    {
        UART_PRINT("[GENERAL EVENT] Reset Request Event\r\n");
    }
    break;

    default:
    {
        UART_PRINT("[GENERAL EVENT] - ID=[%d] Sender=[%d]\n\n",
                   pDevEvent->Data.Error.Code,
                   pDevEvent->Data.Error.Source);

        msgqRetVal = mq_send(controlMQueue, (char *)&msg, 1, 0);
        if(msgqRetVal < 0)
        {
           UART_PRINT("[Control task] could not send element to msg queue\n\r");
           while(1)
           {
                ;
           }
        }
    }
    break;
    }
}

//*****************************************************************************
//
//! This function handles socket events indication
//!
//! \param[in]  pSock - Pointer to Socket Event Info
//!
//! \return None
//!
//*****************************************************************************
void SimpleLinkSockEventHandler(SlSockEvent_t *pSock)
{
    if(SL_SOCKET_ASYNC_EVENT == pSock->Event)
    {
        UART_PRINT("[SOCK ERROR] an event received on socket %d\r\n",
                   pSock->SocketAsyncEvent.SockAsyncData.Sd);
        switch(pSock->SocketAsyncEvent.SockAsyncData.Type)
        {
        case SL_SSL_NOTIFICATION_CONNECTED_SECURED:
            UART_PRINT("[SOCK ERROR] SSL handshake done");
            break;
        case SL_SSL_NOTIFICATION_HANDSHAKE_FAILED:
            UART_PRINT("[SOCK ERROR] SSL handshake failed with error %d\r\n",
                       pSock->SocketAsyncEvent.SockAsyncData.Val);
            break;
        case SL_SSL_ACCEPT:
            UART_PRINT(
                "[SOCK ERROR] Recoverable error occurred "
                "during the handshake %d\r\n",
                pSock->SocketAsyncEvent.SockAsyncData.Val);
            break;
        case SL_OTHER_SIDE_CLOSE_SSL_DATA_NOT_ENCRYPTED:
            UART_PRINT("[SOCK ERROR] Other peer terminated the SSL layer.\r\n");
            break;
        case SL_SSL_NOTIFICATION_WRONG_ROOT_CA:
            UART_PRINT("[SOCK ERROR] Used wrong CA to verify the peer.\r\n");

            break;
        default:
            break;
        }
    }

    /* This application doesn't work w/ socket - Events are not expected */
    switch(pSock->Event)
    {
    case SL_SOCKET_TX_FAILED_EVENT:
        switch(pSock->SocketAsyncEvent.SockTxFailData.Status)
        {
        case SL_ERROR_BSD_ECLOSE:
            UART_PRINT("[SOCK ERROR] - close socket (%d) operation "
                       "failed to transmit all queued packets\n\r",
                       pSock->SocketAsyncEvent.SockTxFailData.Sd);
            break;
        default:
            UART_PRINT("[SOCK ERROR] - TX FAILED  :  socket %d , "
                       "reason (%d) \n\n",
                       pSock->SocketAsyncEvent.SockTxFailData.Sd,
                       pSock->SocketAsyncEvent.SockTxFailData.Status);
            break;
        }
        break;

    default:
        UART_PRINT("[SOCK EVENT] - Unexpected Event [%x0x]\n\n",pSock->Event);
        break;
    }
}

void SimpleLinkNetAppRequestMemFreeEventHandler(uint8_t *buffer)
{
    /* Unused in this application */
}

//****************************************************************************
//
//! \brief Push Button Handler1(GPIOSW2).
//!          Press push button2 whenever user wants to
//!          switch to AP mode. Write message into message queue indicating
//!          switching to AP mode.
//!
//! \param[in] none
//!
//! return none
//
//****************************************************************************
void pushButtonInterruptHandler2(uint_least8_t index)
{
    int32_t msgqRetVal;
    struct timespec ts;

    /* Disable the SW2 interrupt */
    GPIO_disableInt(CONFIG_GPIO_BUTTON_0); // SW2

    /* see ControlMessageType. msg=2 applies to ControlMessageType_Switch2 */
    uint8_t msg = 2;

    /* timeout is 0 to send the message immediatelly */
    ts.tv_sec = 0;
    ts.tv_nsec = 0;

    msgqRetVal = mq_timedsend(controlMQueue, (char *)&msg, 1, 0, &ts);
    if(msgqRetVal < 0)
    {
        UART_PRINT("[Control task] could not send element to msg queue\n\r");
        while(1)
        {
            ;
        }
    }
}

/*****************************************************************************
                 Local Functions
*****************************************************************************/
//*****************************************************************************
//
//! Application Boarders display on UART
//!
//! \param  ch - Character to be displayed , n - number of time to display
//!
//! \return none
//!
//*****************************************************************************
void printBorder(char ch,
                 int n)
{
    int i = 0;

    for(i = 0; i < n; i++)
    {
        putch(ch);
    }
}

//*****************************************************************************
//
//! Application startup display on UART
//!
//! \param  none
//!
//! \return none
//!
//*****************************************************************************
int32_t DisplayBanner(char * AppName,
                      char * AppVer)
{
    int32_t ret = 0;
    uint8_t macAddress[SL_MAC_ADDR_LEN];
    uint16_t macAddressLen = SL_MAC_ADDR_LEN;
    uint16_t ConfigSize = 0;
    uint8_t ConfigOpt = SL_DEVICE_GENERAL_VERSION;
    SlDeviceVersion_t ver = {0};
    char lineBreak[] = "\n\r";
    ConfigSize = sizeof(SlDeviceVersion_t);

    /* Print device version info. */
    ret =
        sl_DeviceGet(SL_DEVICE_GENERAL, &ConfigOpt, &ConfigSize,
                     (uint8_t*)(&ver));
    ASSERT_ON_ERROR(ret);

    /* Print device Mac address */
    ret = sl_NetCfgGet(SL_NETCFG_MAC_ADDRESS_GET, 0, &macAddressLen,
                       &macAddress[0]);
    ASSERT_ON_ERROR(ret);

    UART_PRINT(lineBreak);
    UART_PRINT("\t");
    printBorder('=', 44);
    UART_PRINT(lineBreak);
    UART_PRINT("\t   %s Example Ver: %s",AppName, AppVer);
    UART_PRINT(lineBreak);
    UART_PRINT("\t");
    printBorder('=', 44);
    UART_PRINT(lineBreak);
    UART_PRINT(lineBreak);
    UART_PRINT("\t CHIP: 0x%x",ver.ChipId);
    UART_PRINT(lineBreak);
    UART_PRINT("\t MAC:  %d.%d.%d.%d",ver.FwVersion[0],ver.FwVersion[1],
               ver.FwVersion[2],
               ver.FwVersion[3]);
    UART_PRINT(lineBreak);
    UART_PRINT("\t PHY:  %d.%d.%d.%d",ver.PhyVersion[0],ver.PhyVersion[1],
               ver.PhyVersion[2],
               ver.PhyVersion[3]);
    UART_PRINT(lineBreak);
    UART_PRINT("\t NWP:  %d.%d.%d.%d",ver.NwpVersion[0],ver.NwpVersion[1],
               ver.NwpVersion[2],
               ver.NwpVersion[3]);
    UART_PRINT(lineBreak);
    UART_PRINT("\t ROM:  %d",ver.RomVersion);
    UART_PRINT(lineBreak);
    UART_PRINT("\t HOST: %s", SL_DRIVER_VERSION);
    UART_PRINT(lineBreak);
    UART_PRINT("\t MAC address: %02x:%02x:%02x:%02x:%02x:%02x", macAddress[0],
               macAddress[1], macAddress[2], macAddress[3], macAddress[4],
               macAddress[5]);
    UART_PRINT(lineBreak);
    UART_PRINT(lineBreak);
    UART_PRINT("\t");
    printBorder('=', 44);
    UART_PRINT(lineBreak);
    UART_PRINT(lineBreak);

    return(ret);
}

//*****************************************************************************
//
//! This  function clears and enables a GPIO pin interrupt flag
//!
//! \param    index - GPIO index
//!
//! \return None
//!
//*****************************************************************************
static void GPIO_clearAndEnable(uint8_t index)
{
    GPIO_clearInt(index);
    GPIO_enableInt(index);
}

//*****************************************************************************
//
//! This function initializes the application variables
//!
//! \param    None
//!
//! \return None
//!
//*****************************************************************************
static void InitializeAppVariables(void)
{
    OutOfBox_ControlBlock.gatewayIP = 0;
    OutOfBox_ControlBlock.status = 0;

    memset(OutOfBox_ControlBlock.connectionSSID, 0,
           sizeof(OutOfBox_ControlBlock.connectionSSID));
    memset(OutOfBox_ControlBlock.connectionBSSID, 0,
           sizeof(OutOfBox_ControlBlock.connectionBSSID));
}

/*****************************************************************************
                 Main Functions
*****************************************************************************/

//******************************************************************************
//
//! \brief control task. Create switches handlers and waits for
//!        invokations on those switches.
//!         Additinally, activate watchdog timer to validate the application code
//!
//! \param[in]  None
//!
//! \return None
//!
//******************************************************************************
void * controlTask(void *pvParameters)
{
    ControlMessageType queueMsg;
    int32_t retVal;
    uint32_t ocpRegVal;
    mq_attr attr;
    struct timespec ts;

    /* initializes mailbox for http messages */
    attr.mq_maxmsg = 10;             // queue size
    attr.mq_msgsize = sizeof(ControlMessageType);            // Size of message
    controlMQueue = mq_open("control msg q", O_CREAT, 0, &attr);
    if(((int)controlMQueue) <= 0)
    {
        UART_PRINT("[Control task] could not create msg queue\n\r");
        while(1)
        {
            ;
        }
    }

    /* enable interrupt for the GPIO 22 (email trigger) */
    GPIO_setCallback(CONFIG_GPIO_BUTTON_0, pushButtonInterruptHandler2);
    GPIO_enableInt(CONFIG_GPIO_BUTTON_0);

    while(1)
    {
        queueMsg = ControlMessageType_ControlMessagesMax;

        clock_gettime(CLOCK_REALTIME, &ts);
        ts.tv_sec += 2;

        retVal =
            mq_timedreceive(controlMQueue, (char *)&queueMsg,
                            sizeof(ControlMessageType),
                            NULL,
                            &ts);

        switch(queueMsg)
        {
        case ControlMessageType_ControlMessagesMax:
            break;
        case ControlMessageType_Switch2:
            UART_PRINT("[Control task] switching to AP mode\n\r");
            /* SW2 is used to revert to AP mode and stop provisioning 
            (if running) so device can be connected and controlled adhoc */
            retVal = provisioningStop();
            // intermmediate phase, need to push AP switch again
            if(retVal == SL_RET_CODE_DEV_NOT_STARTED)                           
            {
                UART_PRINT(
                    "[Control task] device is not started yet, please press SW2 "
                    "button again\n\r");
                /* Clear and enable again the SW2 interrupt */
                GPIO_clearAndEnable(CONFIG_GPIO_BUTTON_0);
                break;
            }
            // should not happen
            if((retVal == SL_RET_CODE_DEV_LOCKED) || (retVal == SL_API_ABORTED))                        
            {
                UART_PRINT(
                    "[Control task] device cannot start in AP mode, please "
                    "reset the board\n\r");
                /* Clear and enable again the SW2 interrupt */
                GPIO_clearAndEnable(CONFIG_GPIO_BUTTON_0);
                break;
            }

            /* set AP mode regardless of the current mode */
            retVal = sl_WlanSetMode(ROLE_AP);

            /* Check if switching to AP command is successful */
            if(retVal == 0)
            {
                UART_PRINT(
                    "[Control task] device started in AP role, rebooting "
                    "device...\n\r");

                /* indicate AP role on OCP register */
                ocpRegVal = MAP_PRCMOCRRegisterRead(OCP_REGISTER_INDEX);
                ocpRegVal |= (1 << OCP_REGISTER_OFFSET);
                MAP_PRCMOCRRegisterWrite(OCP_REGISTER_INDEX, ocpRegVal);
                /* Clear and enable again the SW2 interrupt */
                GPIO_clearAndEnable(CONFIG_GPIO_BUTTON_0);
                mcuReboot();
            }
            else
            {
                UART_PRINT("[Control task] device not started in AP role\n\r");
            }

            /* Clear and enable again the SW2 interrupt */
            GPIO_clearAndEnable(CONFIG_GPIO_BUTTON_0);
            break;
        case ControlMessageType_ResetRequired:
            UART_PRINT("[Control task] platform reboot is required\n\r");
            mcuReboot();

            break;

        default:
            break;
        }
    }
}

//*****************************************************************************
//
//! \brief This function reboot the M4 host processor
//!
//! \param[in]  none
//!
//! \return none
//!
//****************************************************************************
void mcuReboot(void)
{
    /* stop network processor activities before reseting the MCU */
    sl_Stop(SL_STOP_TIMEOUT);

    UART_PRINT("[Common] CC32xx MCU reset request\r\n");

    /* Reset the MCU in order to test the bundle */
    PRCMHibernateCycleTrigger();
}
void *mqtt_data(void *arg0){

     while(1){
         UART_PRINT("mqtt\n");
//         LOG_INFO("MQTT_EVENT_CONNACK\r\n");
         sleep(5);
     }
 }



void *aws_data(void *arg0){

    while(wifi_flag != 1){
        UART_PRINT("WiFi Connecting\n");
        sleep(3);
    }
        sleep(10);

    int32_t ret;
//    UART_Handle uartHandle;
    MQTTClient_Handle mqttClientHandle;

//    uartHandle = InitTerm();
//    UART_control(uartHandle, UART_CMD_RXDISABLE, NULL);

    ret = ti_net_SlNet_initConfig();
    if(0 != ret)
    {
        UART_PRINT("Failed to initialize SlNetSock\n\r");
    }

    ret = WifiInit();
    if(ret < 0){
        while(1);
    }

        UART_PRINT("mqtt Connecting\n");
    ret = MQTT_IF_Init(mqttInitParams);
    if(ret < 0){
     while(1);
    }

        UART_PRINT("mqtt Connected\n");
    mqttClientHandle = MQTT_IF_Connect(mqttClientParams, mqttConnParams, MQTT_EventCallback);
    if(mqttClientHandle < 0){
        UART_PRINT("mqtt not Connected\n");
     while(1);
    }


    while(1){
     UART_PRINT("aws\n");
     MQTT_IF_Publish(mqttClientHandle,
                      "MQTTDemo",
                      "hello from TI\r\n",
                      strlen("hello from TI\r\n"),
                      MQTT_QOS_0);
     sleep(5);
    }
 }

void * mainThread(void *arg)
{
    int32_t RetVal;
    pthread_attr_t pAttrs;
    pthread_attr_t pAttrs_spawn;
    pthread_attr_t mq_pAttrs;

    struct sched_param priParam;
    struct timespec ts = {0};




    GPIO_init();
    SPI_init();
//    I2C_init();

    /* init Terminal, and print App name */
    InitTerm();

    /* initialize the realtime clock */
    clock_settime(CLOCK_REALTIME, &ts);

    InitializeAppVariables();

    /* Switch off all LEDs on boards */
    GPIO_write(CONFIG_GPIO_LED_0, CONFIG_GPIO_LED_OFF);

    /* initializes signals for all tasks */
    sem_init(&Provisioning_ControlBlock.connectionAsyncEvent, 0, 0);
    sem_init(&Provisioning_ControlBlock.provisioningDoneSignal, 0, 0);
    sem_init(&Provisioning_ControlBlock.provisioningConnDoneToOtaServerSignal,
             0,
             0);
    sem_init(&LinkLocal_ControlBlock.otaReportServerStartSignal, 0, 0);
    sem_init(&LinkLocal_ControlBlock.otaReportServerStopSignal, 0, 0);

    /* create the sl_Task */
    pthread_attr_init(&pAttrs_spawn);
    priParam.sched_priority = SPAWN_TASK_PRIORITY;
    RetVal = pthread_attr_setschedparam(&pAttrs_spawn, &priParam);
    RetVal |= pthread_attr_setstacksize(&pAttrs_spawn, TASK_STACK_SIZE);

    RetVal = pthread_create(&gSpawnThread, &pAttrs_spawn, sl_Task, NULL);

    if(RetVal)
    {
        /* Handle Error */
        UART_PRINT("Unable to create sl_Task thread \n");
        while(1)
        {
            ;
        }
    }
    RetVal = sl_Start(0, 0, 0);
    if(RetVal >= 0)
    {
        DisplayBanner(APPLICATION_NAME, APPLICATION_VERSION);
        RetVal = sl_Stop(SL_STOP_TIMEOUT);
        if(RetVal < 0)
        {
            /* Handle Error */
            UART_PRINT("\n sl_Stop failed\n");
            while(1)
            {
                ;
            }
        }
    }
    else if((RetVal < 0) && (RetVal != SL_ERROR_RESTORE_IMAGE_COMPLETE))
    {
        /* Handle Error */
        UART_PRINT("\n sl_Start failed\n");
        UART_PRINT("\n %s Example Ver. %s\n",APPLICATION_NAME,
                   APPLICATION_VERSION);
        while(1)
        {
            ;
        }
    }

    pthread_attr_init(&pAttrs);
    priParam.sched_priority = 1;
    RetVal = pthread_attr_setschedparam(&pAttrs, &priParam);
    RetVal |= pthread_attr_setstacksize(&pAttrs, TASK_STACK_SIZE);

    if(RetVal)
    {
        /* Handle Error */
        UART_PRINT("Unable to configure provisioningTask thread parameters \n");
        while(1)
        {
            ;
        }
    }

    RetVal = pthread_create(&gProvisioningThread, &pAttrs, provisioningTask,
                            NULL);

    if(RetVal)
    {
        /* Handle Error */
        UART_PRINT("Unable to create provisioningTask thread \n");
        while(1)
        {
            ;
        }
    }
/*
    pthread_attr_init(&mq_pAttrs);
    priParam.sched_priority = 1;
    RetVal = pthread_attr_setschedparam(&mq_pAttrs, &priParam);
    RetVal |= pthread_attr_setstacksize(&mq_pAttrs, TASK_STACK_SIZE);
//    uart thread to read data from STM32
    pthread_attr_init(&mq_pAttrs);
    pthread_create(&mq_thread, &mq_pAttrs, mqtt_data, NULL);
*/

    pthread_attr_t aws_pAttrs;
//    struct sched_param priParam;
    priParam.sched_priority = 1;
    pthread_attr_init(&aws_pAttrs);
    pthread_attr_setschedparam(&aws_pAttrs, &priParam);
    pthread_attr_setstacksize(&aws_pAttrs, 4096);
    pthread_create(&aws_thread, &aws_pAttrs, aws_data, NULL);

//    pthread_attr_t aws_pAttrs;
//    pthread_attr_init(&aws_pAttrs);
//    pthread_create(&aws_thread, &aws_pAttrs, aws_data, NULL);



    pthread_attr_init(&pAttrs);
    priParam.sched_priority = 1;
    RetVal = pthread_attr_setschedparam(&pAttrs, &priParam);
    RetVal |= pthread_attr_setstacksize(&pAttrs, LINKLOCAL_STACK_SIZE);

    if(RetVal)
    {
        /* Handle Error */
        UART_PRINT("Unable to configure linkLocalTask thread parameters \n");
        while(1)
        {
            ;
        }
    }

    RetVal = pthread_create(&gLinklocalThread, &pAttrs, linkLocalTask, NULL);

    if(RetVal)
    {
        /* Handle Error */
        UART_PRINT("Unable to create linkLocalTask thread \n");
        while(1)
        {
            ;
        }
    }
#if 0

    pthread_attr_init(&pAttrs);
    priParam.sched_priority = 1;
    RetVal = pthread_attr_setschedparam(&pAttrs, &priParam);
    RetVal |= pthread_attr_setstacksize(&pAttrs, CONTROL_STACK_SIZE);

    if(RetVal)
    {
        /* Handle Error */
        UART_PRINT("Unable to configure controlTask thread parameters \n");
        while(1)
        {
            ;
        }
    }

    RetVal = pthread_create(&gControlThread, &pAttrs, controlTask, NULL);

    if(RetVal)
    {
        /* Handle Error */
        UART_PRINT("Unable to create controlTask thread \n");
        while(1)
        {
            ;
        }
    }

    pthread_attr_init(&pAttrs);
    priParam.sched_priority = 5;
    RetVal = pthread_attr_setschedparam(&pAttrs, &priParam);
    RetVal |= pthread_attr_setstacksize(&pAttrs, TASK_STACK_SIZE);

    if(RetVal)
    {
        /* Handle Error */
        UART_PRINT("Unable to configure otaTask thread parameters \n");
        while(1)
        {
            ;
        }
    }

    RetVal = pthread_create(&gOtaThread, &pAttrs, otaTask, NULL);

    if(RetVal)
    {
        /* Handle Error */
        UART_PRINT("Unable to create otaTask thread \n");
        while(1)
        {
            ;
        }
    }
#endif
    return(0);
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    是否遇到特定错误? 代码在 MQTT 函数内或其他地方是否显示失败?

    了解错误发生位置和原因的详细信息会有所帮助。

    此外、检查 RTOS 状态以确保不存在堆栈/堆问题也会很好。

    通常、可以将 MQTT 代码插入另一个项目、例如 OOB 项目、因此我将检查上述调试步骤、以查看下一步可以研究的位置。

    此致、

    Michael

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    感谢您的回答。

    我按照以下链接中给出的步骤将 MQTT 添加 到其他项目中。

    dev.ti.com/.../node

    如步骤中所述,他们使用单独函数 WifiInit()与 Wi-Fi 连接,但 OOB 已连接到 will,因此我跳过了该步骤,还手动分配了客户端 ID。 因此、我对这个 wifi 初始化函数有疑问。 仅当器件连接了 WIFI 并为其分配了 IP 后、我才尝试连接到 MQTT。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    您链接的 SimpleLink Academy 模块是将 MQTT 功能添加到其他演示时使用的正确指南。

    WifiInit()执行多项 Wi-Fi 启动任务,例如连接到 AP,但它也执行诸如初始化 Network_IF 层等任务。 MQTT 库需要该层。 您需要修改代码、以便将 Network_IF init 与现有 OOB 代码一起包含在内。

    此外、您使用 OOB 演示+ MQTT 的原因是否特别?

    或许更好的起点是智能锁参考设计。 如需更多信息、请参阅此处的 E2E 帖子:

    https://e2e.ti.com/support/wireless-connectivity/wifi/f/wi-fi-forum/771739/cc3220-implementing-mqtt-in-customized-project

    此致、

    Michael

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我的代码在初始化  Network_IF 层后工作。 感谢您的支持。