This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC3120MOD:CC3120 MOD

Guru**** 2778335 points

Other Parts Discussed in Thread: CC3120

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/992695/cc3120mod-cc3120-mod

器件型号:CC3120MOD
主题中讨论的其他器件:CC3120

大家好、

适用于  CC3120 MOD  

如何查找 ETSI/CE (欧洲)的测试认证报告:

  • EN300328 V2.1.1 (2.4GHz Wi-Fi)
  • EN62311:2008 (MPE)
  • EN301489-1 v2.1.1 (EMC 通用)
  • EN301489-17 v3.1.1 (EMC Wi-Fi)