This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC3220SF-LAUNCHXL:UART2_READ 和 UART2_READTimeout 都无法接收 UART2_STATUS_ECANCELED

Guru**** 2620755 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/1199006/cc3220sf-launchxl-neither-uart2_read-nor-uart2_readtimeout-could-receive-uart2_status_ecancelled

器件型号:CC3220SF-LAUNCHXL

大家好、

环境:simplelink_cc32xx_sdk_6_10_00_05

CCS 版本:12.2.0.00009  

在 UART2 的阻塞模式下、名为 UART2_readCancel 的线程、但 B 线程 UART2_Read 和 UART2_readTimeout 都无法接收 UART2_STATUS_ECANCELED。  UART2_readTimeout 可能会接收 UART2_STATUS_ETIMEOUT。

void  uart2_init (void)
   UART2_Params  uartParams
   //确保在调用 UART_Params_init 之前调用了 UART_init。
   UART2_Params_init (uartParams)
   uartParams.readMode =  UART2_Mode_Blocking  // 回调模式。
   uartParams.writeMode =  UART2_Mode_Blocking //写入模式使用回调模式。
   uartParams.readCallback =  NULL       // 回调函数。
   uartParams.writeCallback =  NULL       //回调函数。
   uartParams.readReturnMode =  UART2_ReadReturnMode_Partial
   uartParams.baudrate =  2000000         //波特率。
   uartParams.dataLength =  UART2_DataLen_8  //数据长度为8位
   uartParams.stopbits =  UART2_stopbits_1   // 1个停止位。
   uartParams.parityType =  UART2_Param_none // 奇偶校验位。
   APP_CB.paramUartHandle = 
   //直到这里、我 用 UART 作为调试端口来执行初始化。
   APP_CB.paramUartHandle =  UART2_open (CONFIG_UART2_Param、&uartParams);
此致、
凯瑟琳
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    文档中的定义为:

    取消 UART2_READ() 函数调用的函数。

    此函      数在 UART2_Mode_callback 中取消异步 UART2_read()操作,或在 UART2_Mode_Blocking 中取消阻止 UART2_read()调用。 在 UART2_Mode_callback 中 ,UART2_readCancel() 使用到目前为止收到的字节数调用已注册的读取回调函数。 应用程序负责检查回调函数中的 count 参数、并处理仅接收字节子集的情况。 回调函数将传递 UART2_STATUS_ECANCELED 的状态

     UART2_Mode_Blocking 中 、UART2_Read() 将返回 UART2_STATUS_ECANCELED、bytesRead 参数将设置为迄今为止接收的字节数。

    该 API 对 UART2_Mode_NonBlocking 没有影响

    参数
    [在] 手柄    由 UART2_open ()返回的 UART2_handle

    因此、对于阻塞模式、您应该得到事件、但我没有自己对其进行测试。

    只是为了理解,您在一个任务上以阻塞模式调用 UART2_read(),而在另一个任务上,您取消了读操作,但读操作仍然被阻塞?

    Shlomi

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 、Shlomi、

    /*
     * Copyright (c) 2017-2019, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    /*
     *  ======== mailbox.c ========
     */
    
    /* XDC module Headers */
    #include <xdc/std.h>
    #include <xdc/runtime/System.h>
    
    /* BIOS module Headers */
    #include <ti/sysbios/BIOS.h>
    #include <ti/sysbios/knl/Task.h>
    #include <ti/sysbios/knl/Mailbox.h>
    #include <ti/sysbios/knl/Clock.h>
    #include <ti/drivers/Board.h>
    #include <ti/drivers/Uart2.h>
    #include "ti_drivers_config.h"
    #define NUMMSGS         5
    #define TASKSTACKSIZE   512
    
    /*
     * This type is accessed by the application. When changing the data members of
     * this structure, considerations should be made for padding and data alignment.
     */
    typedef struct MsgObj {
        Int     id;
        Char    val;
    } MsgObj;
    
    /*
     * Mailbox messages are stored in a queue that requires a header in front of
     * each message. Mailbox_MbxElem is defined such that the header and its size
     * are factored into the total data size requirement for a mailbox instance.
     * Because Mailbox_MbxElem contains Int data types, padding may be added to
     * this struct depending on the data members defined in MsgObj.
     */
    typedef struct MailboxMsgObj {
        Mailbox_MbxElem  elem;      /* Mailbox header        */
        MsgObj           obj;       /* Application's mailbox */
    } MailboxMsgObj;
    
    /* This buffer is not directly accessed by the application */
    MailboxMsgObj mailboxBuffer[NUMMSGS];
    
    Mailbox_Struct mbxStruct;
    Mailbox_Handle mbxHandle;
    
    Task_Struct task0Struct, task1Struct;
    Char task0Stack[TASKSTACKSIZE], task1Stack[TASKSTACKSIZE];
    
    Void readerTask(UArg arg0, UArg arg1);
    Void writerTask(UArg arg0, UArg arg1);
    UART2_Handle UartHandle;
    void uart2_init(void)
    {
        UART2_Params uartParams;
        // 确保调用UART_Params_init之前有调UART_init
        UART2_Params_init(&uartParams);
        uartParams.readMode = UART2_Mode_BLOCKING;  // 回调模式
        uartParams.writeMode = UART2_Mode_BLOCKING; // 写模式使用回调模式
        uartParams.readCallback = NULL;             // 回调函数
        uartParams.writeCallback = NULL;            // 回调函数
        uartParams.readReturnMode = UART2_ReadReturnMode_FULL;
        uartParams.baudRate = 2000000;             // 波特率
        uartParams.dataLength = UART2_DataLen_8;   // 数据长度为8位
        uartParams.stopBits = UART2_StopBits_1;    // 1位停止位
        uartParams.parityType = UART2_Parity_NONE; // 奇偶校验位
        // 到时候这里使用为UART调试口的初始化
        UartHandle = UART2_open(CONFIG_UART2_0, &uartParams);
    
        /* remove uart receive from LPDS dependency */
        // UART2_control(app_CB.paramUartHandle, UART_CMD_RXDISABLE, NULL);
    }
    /*
     *  ======== main ========
     */
    int main()
    {
        Task_Params taskParams;
        Mailbox_Params mbxParams;
    
        /* Call Driver init functions */
        Board_init();
        uart2_init();
        /* Construct read and writer tasks */
        Task_Params_init(&taskParams);
        taskParams.stackSize = TASKSTACKSIZE;
        taskParams.stack = &task0Stack;
        Task_construct(&task0Struct, (Task_FuncPtr)writerTask, &taskParams, NULL);
        taskParams.stack = &task1Stack;
        Task_construct(&task1Struct, (Task_FuncPtr)readerTask, &taskParams, NULL);
    
        /* Construct a Mailbox instance */
        Mailbox_Params_init(&mbxParams);
        mbxParams.buf = (Ptr)mailboxBuffer;
        mbxParams.bufSize = sizeof(mailboxBuffer);
        Mailbox_construct(&mbxStruct, sizeof(MsgObj), NUMMSGS, &mbxParams, NULL);
        mbxHandle = Mailbox_handle(&mbxStruct);
    
        BIOS_start();
    
        return(0);
    }
    
    
    /*
     *  ======== readerTask ========
     */
    Void readerTask(UArg arg0, UArg arg1)
    {
        size_t bytesRead = 0;
        char   input[16];
        while (1) {
            System_printf("UART2_read Enter\n");
            System_flush();
            int status = UART2_read(UartHandle, &input, 16, &bytesRead);
            System_printf("UART2_read return:%d,bytesRead:%d\n",status,bytesRead);
            System_flush();
        }
        System_printf("All messages received. Exiting...\n");
    
        BIOS_exit(0);
    }
    
    /*
     *  ======== writerTask ========
     */
    Void writerTask(UArg arg0, UArg arg1)
    {
    
        while (1) {
            System_printf("UART2_readCancel Enter\n");
            System_flush();
            UART2_readCancel(UartHandle);
            System_printf("UART2_readCancel return\n");
            System_flush();
            Task_sleep((10000 / Clock_tickPeriod)*100);
           }
    
    }

    上面的代码位于邮箱项目中。 我修改了 mailbox.c 文件 进行测试、结果如下。 UART2_READ 未取消。

    测试 结果:

    UART2_readCancel 输入
    UART2_readCancel 返回
    UART2_Read Enter
    UART2_readCancel 输入
    UART2_readCancel 返回
    UART2_readCancel 输入
    UART2_readCancel 返回

    除非 uartParams.readReturnMode = UART2_ReadReturnMode_Partial、 否则 UART2_Read 返回 UART2_STATUS_SUCCESS、而不是 UART2_STATUS_ECANCELED。

    测试 结果:

    UART2_readCancel 输入
    UART2_readCancel 返回
    UART2_Read Enter
    UART2_readCancel 输入
    UART2_readCancel 返回
    UART2_READ 返回:0、字节读取:0
    UART2_Read Enter
    UART2_readCancel 输入
    UART2_readCancel 返回
    UART2_READ 返回:0、字节读取:0

    最棒的

    凯瑟琳

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    是的、你是对的。

    我深入探讨了 UART2驱动程序的实现、ECANCELED 错误似乎仅在回调模式下传播。

    在阻塞模式下、readSem 将被布置、读取将随着接收到的字节计数而中断、直至达到该点(在本例中为0)。

    void __attribute__((weak) UART2_readCancel (UART2_Handle handle)

    UART2_Object *对象= handle->object;
    uintptr_t 密钥;

    if ((object->state.readMode!= UART2_Mode_Blocking)&&
    (object->state.readMode!= UART2_Mode_callback)){
    返回;

    KEY = Hwip_disable();

    if (object->readInUse=false){
    Hwip_restore (key);
    返回;

    object->readInUse = false;
    object->ReadCount = 0;

    if (object->state.rxCanceled == false){
    object->state.rxCanceled = true;
    SemaphoreP_POST (&object->readSem);

    if (object->state.readMode = UART2_Mode_callback){
    object->readCallback (handle、object->readBuf、object->bytesRead、
    object->userArg, UART2_STATUS_ECANCELED);

    Hwip_restore (key);

    Shlomi