This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHXL-CC3235SF: HTTP_POST 连接正在崩溃,同时创建另外两个 pthread ,而不是 http_post pthread (MainThread)。

Guru**** 2611705 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/1223701/launchxl-cc3235sf-http_post-connection-is-crashing-while-creating-two-other-pthread-other-than-http_post-pthread-mainthread

器件型号:LAUNCHXL-CC3235SF

您好、TI!

我无法在我的应用程序项目中创建多个线程。 我将使用 mqtt_client 示例连接 MQTT 服务器。 Project 首先连接 http 服务器、然后接收 MQTT 连接参数、并通过使用它们连接 MQTT 服务器。 两个任务都从同一个任务(MainThread)执行。 功能非常有用。 除此之外,我还有两个任务。 即:

1) bssOperatorThread

2) rect_charg_control_thread

在创建这些线程时,我的 http_client_executor 函数正在受到干扰,这意味着无法连接到服务器和抛出错误。 但是如果不创建上面提到的线程1和2、那么它运行良好。

它们之间似乎可能存在内存问题、否则它们之间没有关系、任务1和2是独立的。 在使用堆栈大小和任务优先级的时候,它也在处理一个任务,但从不同时处理这两个任务。  

这里是我的  http_client_executor ,请检查什么是错的。

//TODO http_client_executor
extern uint8_t http_client_executor(void *pvParameters)
{
    uint8_t IsConnectedWithHttp=0;
    uint8_t tempReturn=0;

    // =============================== Sending a HTTP POST request starts===============================//
    bool moreDataFlag = false;


    int16_t ret = 0;
    int16_t len = 0;

    LOG_INFO("\r\nSending a HTTP POST request to '%s'\r\n", HOSTNAME);

    HTTPClient_Handle httpClientHandle;
    int16_t statusCode;
    httpClientHandle = HTTPClient_create(&statusCode, 0);
    if (statusCode < 0)
    {
        LOG_ERROR("httpTask: creation of http client handle failed", statusCode);
    }

    ret = HTTPClient_setHeader(httpClientHandle,
    HTTPClient_HFIELD_REQ_AUTHORIZATION,
                               USER_AGENT, strlen(USER_AGENT) + 1,
                               HTTPClient_HFIELD_PERSISTENT);
    if (ret < 0)
    {
        LOG_ERROR("httpTask: setting request header failed", ret);
    }

    /*     ===================  suggested header settings===================    */

    // Content Type-> application/json
    ret = HTTPClient_setHeader(httpClientHandle,
    HTTPClient_HFIELD_REQ_CONTENT_TYPE,
                               "application/json", strlen("application/json"),
                               HTTPClient_HFIELD_PERSISTENT);

    if (ret < 0)
    {
        LOG_ERROR("httpTask: setting request header failed", ret);
    }

    // setting charset=utf-8
    ret = HTTPClient_setHeader(httpClientHandle,
    HTTPClient_HFIELD_REQ_ACCEPT_CHARSET,
                               "charset=utf-8", strlen("HTTPClient_setHeader"),
                               HTTPClient_HFIELD_PERSISTENT);

    if (ret < 0)
    {
        LOG_ERROR("httpTask: setting request header failed", ret);
    }

    // x-api-key
    ret = HTTPClient_setHeaderByName(httpClientHandle,
    HTTPClient_HFIELD_REQ_CONTENT_TYPE,
                                     "x-api-key", API_KEY, strlen(API_KEY),
                                     HTTPClient_HFIELD_PERSISTENT);

    if (ret < 0)
    {
        LOG_ERROR("httpTask: setting request header failed", ret);
    }

    //x-app-name
    ret = HTTPClient_setHeaderByName(httpClientHandle,
    HTTPClient_HFIELD_REQ_CONTENT_TYPE,
                                     "x-app-name", APP_NAME, strlen(APP_NAME),
                                     HTTPClient_HFIELD_PERSISTENT);

    if (ret < 0)
    {
        LOG_ERROR("httpTask: setting request header failed", ret);
    }

    // x-svc
    ret = HTTPClient_setHeaderByName(httpClientHandle,
    HTTPClient_HFIELD_REQ_CONTENT_TYPE,
                                     "x-svc", SVC, strlen(SVC),
                                     HTTPClient_HFIELD_PERSISTENT);

    if (ret < 0)
    {
        LOG_ERROR("httpTask: setting request header failed", ret);
    }

    //---------------------------------------------------------//

    ret = HTTPClient_connect(httpClientHandle, HOSTNAME, 0, 0);
    if (ret < 0)
    {
        LOG_ERROR("httpTask: connect failed : %d", ret);
    }

    //===============   First encryption  ================== //

    uint8_t out[SHA256_HASH_SIZE];
    char out_str_app_key[SHA256_HASH_SIZE * 2 + 1];
    unsigned i;

    // Call hmac-sha256 function
    hmac_sha256(BASE_KEY, strlen(BASE_KEY), APP_NAME, strlen(APP_NAME), &out,
                sizeof(out));

    // Convert `out` to string
    memset(&out_str_app_key, 0, sizeof(out_str_app_key));

    for (i = 0; i < sizeof(out); i++)
    {
        snprintf(&out_str_app_key[i * 2], 3, "%02x", out[i]);
    }

    //LOG_INFO("App_Key: %s\r\n", out_str_app_key);

    //===============   Second encryption  ================== //

    // Call hmac-sha256 function
    memset(&out, 0, sizeof(out));
    hmac_sha256(out_str_app_key, strlen(out_str_app_key), DEVICE_ID,
                strlen(DEVICE_ID), &out, sizeof(out));

    char out_str_device_token[SHA256_HASH_SIZE * 2 + 1];

    // Convert `out` to string
    memset(&out_str_device_token, 0, sizeof(out_str_device_token));

    for (i = 0; i < sizeof(out); i++)
    {
        snprintf(&out_str_device_token[i * 2], 3, "%02x", out[i]);
    }

//    LOG_INFO("Device_Token: %s\r\n", out_str_device_token);

//---------------------------------------------------------//
    char REQ_BODY[150];

    memset(REQ_BODY, '\0', sizeof(REQ_BODY));

    sprintf(REQ_BODY,
            "{\"deviceToken\":\"%s\",\"deviceId\":\"%s\",\"mqttTls\":\"false\"}",
            out_str_device_token, DEVICE_ID);

//    LOG_INFO("REQ_BODY: %s\r\n", REQ_BODY);

    ret = HTTPClient_sendRequest(httpClientHandle, HTTP_METHOD_POST,
    REQUEST_URI,
                                 REQ_BODY, strlen(REQ_BODY), 0);
    if (ret < 0)
    {
        LOG_ERROR("httpTask: send failed", ret);
    }

    if (ret != HTTP_SC_OK)
    {
        LOG_ERROR("httpTask: cannot get status", ret);
        tempReturn=0;
        return tempReturn;
    }
    else
    {
        LOG_INFO("HTTP Response Status Code: %d\r\n", ret);
    }


    memset(data, '\0', sizeof(data));
    memset(Playload_Container, '\0', sizeof(Playload_Container));

    LOG_INFO("strlen of data : %d\r\n", strlen(data));

//    char *Playload_Container;
//    Playload_Container = (char*) malloc(sizeof(data));



    len = 0;
    do
    {
        ret = HTTPClient_readResponseBody(httpClientHandle, data, sizeof(data),
                                          &moreDataFlag);
        if (ret < 0)
        {
            LOG_ERROR("httpTask: response body processing failed", ret);
        }
//        UART_PRINT("%.*s \r\n", ret, data);
        sprintf(&Playload_Container[strlen(Playload_Container)], "%.*s\r\n",
                ret, data);
        len += ret;
    }
    while (moreDataFlag);


    ret = HTTPClient_disconnect(httpClientHandle);
    if (ret < 0)
    {
        LOG_ERROR("httpTask: disconnect failed", ret);
    }

    HTTPClient_destroy(httpClientHandle);


    LOG_INFO("PlayLoad : %s\r\n", Playload_Container);
    LOG_INFO("Received %d bytes of payload\r\n", len);

    //  =============  JSON parsing starts ===============//
    json_init(Http_Resp_PL_Topic);

    //--> Token Value
    char val_buff[100];
    memset(val_buff, '\0', sizeof(val_buff));
    IsConnectedWithHttp+=json_parser(Playload_Container, "\"token\"",
                &val_buff[0]);
    memcpy((http_para_for_mqtt_conn.token), val_buff,
           sizeof(http_para_for_mqtt_conn.token)); // copies token value from http, which going to be used as pw for mqtt connection.
    LOG_INFO("token : %.*s**********!\r\n", 2,(http_para_for_mqtt_conn.token));

    //--> Topics->fwd
    memset(val_buff, '\0', sizeof(val_buff));
    IsConnectedWithHttp+=json_parser(Playload_Container, "\"topic\".\"fwd\"",
                &val_buff[0]);
    memcpy((http_para_for_mqtt_conn.events_topic), val_buff,
           sizeof(http_para_for_mqtt_conn.events_topic)); // copies token value from http, which going to be used as pw for mqtt connection.
    LOG_INFO("fwd topic : %s\r\n", (http_para_for_mqtt_conn.events_topic));

    //--> Topics->rev
    memset(val_buff, '\0', sizeof(val_buff));
    IsConnectedWithHttp+=json_parser(Playload_Container, "\"topic\".\"rev\"",
                &val_buff[0]);
    memcpy((http_para_for_mqtt_conn.cmd_topic), val_buff,
           sizeof(http_para_for_mqtt_conn.cmd_topic)); // copies token value from http, which going to be used as pw for mqtt connection.
    LOG_INFO("rev topic : %s\r\n", (http_para_for_mqtt_conn.cmd_topic));

    //--> Topics->alert
    memset(val_buff, '\0', sizeof(val_buff));
    IsConnectedWithHttp+=json_parser(Playload_Container, "\"topic\".\"alert\"",
                &val_buff[0]);
    memcpy((http_para_for_mqtt_conn.alerts_topic), val_buff,
           sizeof(http_para_for_mqtt_conn.alerts_topic)); // copies token value from http, which going to be used as pw for mqtt connection.
    LOG_INFO("alert topic : %s\r\n", (http_para_for_mqtt_conn.alerts_topic));

    //--> mqttUrl
    memset(val_buff, '\0', sizeof(val_buff));
    IsConnectedWithHttp+=json_parser(Playload_Container, "\"mqttUrl\"",
                &val_buff[0]);
    memcpy((http_para_for_mqtt_conn.mqttUrl), val_buff,
           sizeof(http_para_for_mqtt_conn.mqttUrl)); // copies token value from http, which going to be used as pw for mqtt connection.
    LOG_INFO("mqttUrl : %.*s.**.**.**\r\n",2, (http_para_for_mqtt_conn.mqttUrl));
//    LOG_INFO("mqttUrl : %s\r\n",(http_para_for_mqtt_conn.mqttUrl));

    //--> mqttPort
    memset(val_buff, '\0', sizeof(val_buff));
    IsConnectedWithHttp+=json_parser(Playload_Container, "\"mqttPort\"",
                &val_buff[0]);
    (http_para_for_mqtt_conn.mqttPort)=atoi(val_buff); // copies token value from http, which going to be used as pw for mqtt connection.
    LOG_INFO("mqttPort : %d\r\n", (http_para_for_mqtt_conn.mqttPort));

    //--> tlsCaCrt
    memset(val_buff, '\0', sizeof(val_buff));
    IsConnectedWithHttp+=json_parser(Playload_Container, "\"tlsCaCrt\"",
                &val_buff[0]);
    LOG_INFO("tlsCaCrt : %s\r\n", val_buff);

    //--> mqttTls
    memset(val_buff, '\0', sizeof(val_buff));
    IsConnectedWithHttp+=json_parser(Playload_Container, "\"mqttTls\"",
                &val_buff[0]);

    if (strcmp(val_buff, "false") == 0)
    {
        (http_para_for_mqtt_conn.mqttTls) = false;
    }
    else
    {
        (http_para_for_mqtt_conn.mqttTls) = true;
    }
    LOG_INFO("mqttTls : %d\r\n", (http_para_for_mqtt_conn.mqttTls));

    json_dinit();

    //  =============  JSON parsing ends ===============//

//    free(Playload_Container);


    if(IsConnectedWithHttp==8)
    {
        tempReturn=1;
    }
    else
    {
        tempReturn=0;
    }

    return tempReturn;
    // =============================== Sending a HTTP POST request ends===============================//
}

我将创建的两个线程都仅在 Main 函数中。 请查看:

int main(void)
{
    /* Call board init functions */
    Board_init();

    /*UART for Serial Monitor Printing*/
    uartHandle = InitTerm();
    UART_control(uartHandle, UART_CMD_RXENABLE, NULL);

    pthread_t thread;
    pthread_attr_t pAttrs;
    struct sched_param priParam;
    int retc;
    int detachState;

    //======================= Main thread starts =================//

    /* Set priority and stack size attributes */
    pthread_attr_init(&pAttrs);
    priParam.sched_priority = 3;

    detachState = PTHREAD_CREATE_DETACHED;
    retc = pthread_attr_setdetachstate(&pAttrs, detachState);
    if (retc != 0)
    {
        /* pthread_attr_setdetachstate() failed */
        while (1)
        {
            ;
        }
    }

    pthread_attr_setschedparam(&pAttrs, &priParam);

    retc |= pthread_attr_setstacksize(&pAttrs, THREADSTACKSIZE);
    if (retc != 0)
    {
        /* pthread_attr_setstacksize() failed */
        while (1)
        {
            ;
        }
    }

    retc = pthread_create(&thread, &pAttrs, mainThread, NULL);
    if (retc != 0)
    {
        /* pthread_create() failed */
        while (1)
        {
            ;
        }
    }

    //======================= Main thread ends =================//

    //======================= Creating BSS Operations thread starts =================//
    pthread_attr_t pAttrs_1;
    struct sched_param priParam_1;
    pthread_t thread_1;
    retc = 0;

    /* Set priority and stack size attributes */
    pthread_attr_init(&pAttrs_1);
    priParam_1.sched_priority = 1;

    retc = pthread_attr_setdetachstate(&pAttrs_1, PTHREAD_CREATE_DETACHED);
    if (retc != 0)
    {
        /* pthread_attr_setdetachstate() failed */
        while (1)
        {
            ;
        }
    }

    retc = pthread_attr_setschedparam(&pAttrs_1, &priParam_1);

    //        retc |= pthread_attr_setstacksize(&pAttrs_1, 2048);
    retc |= pthread_attr_setstacksize(&pAttrs_1, (1024 * 5));
    if (retc != 0)
    {
        /* pthread_attr_setstacksize() failed */
        while (1)
        {
            ;
        }
    }

    retc = pthread_create(&thread_1, &pAttrs_1, bssOperatorThread, NULL);
    if (retc != 0)
    {
        /* pthread_create() failed */
        while (1)
        {
            ;
        }
    }
    //======================= Creating BSS Operations thread ends =================//

    //   *************** creating a new rect_charg_control_Thread **************//
    pthread_attr_t pAttrs_2;
    struct sched_param priParam_2;
    pthread_t thread_2;
    int retc = 0;

    /* Set priority and stack size attributes */
    pthread_attr_init(&pAttrs_2);
    priParam_2.sched_priority = 1;

    retc = pthread_attr_setdetachstate(&pAttrs_2, PTHREAD_CREATE_DETACHED);
    if (retc != 0)
    {
        /* pthread_attr_setdetachstate() failed */
        while (1)
        {
            ;
        }
    }

    pthread_attr_setschedparam(&pAttrs_2, &priParam_2);

    retc |= pthread_attr_setstacksize(&pAttrs_2, (1024 * 5));
    if (retc != 0)
    {
        /* pthread_attr_setstacksize() failed */
        while (1)
        {
            ;
        }
    }

    retc = pthread_create(&thread_2, &pAttrs_2, rect_charg_control_Thread,
    NULL);
    if (retc != 0)
    {
        /* pthread_create() failed */
        while (1)
        {
            ;
        }
    }
    //=======================  rect_charg_control_Thread ends =================//

    /* Start the FreeRTOS scheduler */
    vTaskStartScheduler();

    return (0);
}

请帮助我们摆脱这个问题。

提前感谢、

肉食

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    等待你的回复,回复 PLZ.

    谢谢。

    肉食

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    大家好、Sarju、

    您能否验证线程是否按预期运行? 如果这是存储器问题、您也可以使用存储器浏览器在调试器中进行检查。 您是否确定他们的优先级是您打算达到的水平? 您是否正在发布定制主题帖?