This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHCC3235MOD:。 NET 连接到 tcpechotls 问题

Guru**** 2605675 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/1277337/launchcc3235mod-net-connect-to-tcpechotls-question

器件型号:LAUNCHCC3235MOD

在使用 python 脚本运行(请参阅 https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/1276970/launchcc3235mod-getting-tcpechotls-to-work-with-python-script-from-windows/)之后、我试图使 tcpechotls 与 Windows .Net framework 4.8.1配合使用、并在" Console "中继续获取"RemoteCertificateNameMismatch "。 WriteLine ("证书错误:{0}"、sslPolicyErrors);"。 我修改了 tcpechotls 中的一些内容、使其在工作站模式下以主机名运行并更改了端口、但这些移动对 python 脚本"python tcpSendReceiveTLS.py 192.168.1.99 58800 1 certs/cacert.pem -s100"(C:\ti_simplelink_cc32xx_sdk_7_10_00_13\tools\cc32xx_tools")起作用。 原始但更改了 Microsoft 示例中的连接代码,位于 SslStream Class (System.Net.Security)| Microsoft Learn 

 

using System;
using System.Collections;
using System.Net.Security;
using System.Net.Sockets;
using System.Security.Authentication;
using System.Security.Cryptography.X509Certificates;
using System.Text;
using System.Threading.Tasks;

namespace tlsMSG
{
    public class SslTcpClient
    {
        private static Hashtable certificateErrors = new Hashtable();

        // The following method is invoked by the RemoteCertificateValidationDelegate.
        public static bool ValidateServerCertificate(
              object sender,
              X509Certificate certificate,
              X509Chain chain,
              SslPolicyErrors sslPolicyErrors)
        {
            if (sslPolicyErrors == SslPolicyErrors.None)
                return true;

            Console.WriteLine("Certificate error: {0}", sslPolicyErrors);

            // Do not allow this client to communicate with unauthenticated servers.
            return false;
        }
        public static void RunClient(string machineName, string serverName)
        {
            // Create a TCP/IP client socket.
            // machineName is the host running the server application.
            TcpClient client = new TcpClient(machineName, 58800);
            Console.WriteLine("Client connected.");
            // Create an SSL stream that will close the client's stream.
            SslStream sslStream = new SslStream(
                client.GetStream(),
                false,
                new RemoteCertificateValidationCallback(ValidateServerCertificate),
                null
                );
            // The server name must match the name on the server certificate.
            try
            {
                sslStream.AuthenticateAsClient(serverName);
            }
            catch (AuthenticationException e)
            {
                Console.WriteLine("Exception: {0}", e.Message);
                if (e.InnerException != null)
                {
                    Console.WriteLine("Inner exception: {0}", e.InnerException.Message);
                }
                Console.WriteLine("Authentication failed - closing the connection.");
                client.Close();
                return;
            }
            // Encode a test message into a byte array.
            // Signal the end of the message using the "<EOF>".
            byte[] messsage = Encoding.UTF8.GetBytes("Hello from the client.<EOF>");
            // Send hello message to the server.
            sslStream.Write(messsage);
            sslStream.Flush();
            // Read message from the server.
            string serverMessage = ReadMessage(sslStream);
            Console.WriteLine("Server says: {0}", serverMessage);
            // Close the client connection.
            client.Close();
            Console.WriteLine("Client closed.");
        }
        static string ReadMessage(SslStream sslStream)
        {
            // Read the  message sent by the server.
            // The end of the message is signaled using the
            // "<EOF>" marker.
            byte[] buffer = new byte[2048];
            StringBuilder messageData = new StringBuilder();
            int bytes = -1;
            do
            {
                bytes = sslStream.Read(buffer, 0, buffer.Length);

                // Use Decoder class to convert from bytes to UTF8
                // in case a character spans two buffers.
                Decoder decoder = Encoding.UTF8.GetDecoder();
                char[] chars = new char[decoder.GetCharCount(buffer, 0, bytes)];
                decoder.GetChars(buffer, 0, bytes, chars, 0);
                messageData.Append(chars);
                // Check for EOF.
                if (messageData.ToString().IndexOf("<EOF>") != -1)
                {
                    break;
                }
            } while (bytes != 0);

            return messageData.ToString();
        }
        private static void DisplayUsage()
        {
            Console.WriteLine("To start the client specify:");
            Console.WriteLine("clientSync machineName [serverName]");
            Environment.Exit(1);
        }
        public static int Main(string[] args)
        {
            string serverCertificateName = null;
            string machineName = "trog3235"; // null;
            //if (args == null || args.Length < 1)
            //{
            //    DisplayUsage();
            //}
            // User can specify the machine name and server name.
            // Server name must match the name on the server's certificate.
            //machineName = args[0];
            if (args.Length < 2)
            {
                //serverCertificateName = machineName;
                serverCertificateName = "D:\\c\\vs2022\\CC3235\\tlsMSG\\certs\\caCert.pem";// machineName;
            }
            else
            {
                serverCertificateName = args[1];
            }
            SslTcpClient.RunClient(machineName, serverCertificateName);
            return 0;
        }

    }
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    配置本地 CA 并将其合并到 tcpechotls 服务器证书中看起来很混乱。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    实际上、通过在 W10本地计算机上安装 dummy_root 证书并在  

    //...
    serverCertificateName = "dummy_server";
    //...