This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHXL-CC3235SF:开箱即用项目构建错误

Guru**** 2815505 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/1442710/launchxl-cc3235sf-out-of-box-project-build-errors

器件型号:LAUNCHXL-CC3235SF

工具与软件:

你(们)好  

我们试图构建 开箱即用项目示例、但无法成功构建。 我们只需将开箱即用项目导入到 CCS (使用 tirtos7和 ticlang)、  

关于错误、请参阅以下屏幕截图。

您对我们有什么建议吗?

第页 S CCS:v12.8.1 &  SDK: simplelink_cc32xx_sdk_7_10_00_13

谢谢。

BR

Trevor

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    详细构建日志如下所示:

    **** Build Finished ****
    
    **** Build of configuration MCU+Image for project out_of_box_CC3235SF_LAUNCHXL_tirtos7_ticlang ****
    
    "C:\\ti\\ccs1281\\ccs\\utils\\bin\\gmake" -k -j 12 all -O 
     
    Building file: "../image.syscfg"
    Invoking: SysConfig
    "C:/ti/sysconfig_1.13.0/sysconfig_cli.bat" --script "C:/Users/97111701/workspace_v12/out_of_box_CC3235SF_LAUNCHXL_tirtos7_ticlang/image.syscfg" -o "syscfg" -s "C:/ti/simplelink_cc32xx_sdk_7_10_00_13/.metadata/product.json" --compiler ticlang
    Running script...
    Validating...
    Generating Code (image.syscfg)...
    Writing C:\Users\97111701\workspace_v12\out_of_box_CC3235SF_LAUNCHXL_tirtos7_ticlang\MCU+Image\syscfg\RegDomainSum5.csv...
    Writing C:\Users\97111701\workspace_v12\out_of_box_CC3235SF_LAUNCHXL_tirtos7_ticlang\MCU+Image\syscfg\RegDomainSum24.csv...
    Writing C:\Users\97111701\workspace_v12\out_of_box_CC3235SF_LAUNCHXL_tirtos7_ticlang\MCU+Image\syscfg\ti_drivers_net_wifi_config.json...
    Finished building: "../image.syscfg"
     
    Building file: "../out_of_box.syscfg"
    Invoking: SysConfig
    "C:/ti/sysconfig_1.13.0/sysconfig_cli.bat" --script "C:/Users/97111701/workspace_v12/out_of_box_CC3235SF_LAUNCHXL_tirtos7_ticlang/out_of_box.syscfg" -o "syscfg" -s "C:/ti/simplelink_cc32xx_sdk_7_10_00_13/.metadata/product.json" --compiler ticlang
    Running script...
    subdir_rules.mk:28: recipe for target 'build-870619151' failed
    Error: Exception occurred calling addInstance()
        at Proxy.<anonymous> (C:\ti\sysconfig_1.13.0\dist\webpack:\src\pinmux\services\scripting\scriptingGuard.ts:34:10)
        at scriptFunc (C:\Users\97111701\workspace_v12\out_of_box_CC3235SF_LAUNCHXL_tirtos7_ticlang\out_of_box.syscfg:60:28)
        at cb (C:\ti\sysconfig_1.13.0\dist\webpack:\src\pinmux\services\scripting\runScript.ts:94:27)
        at Object.withDeprecatedAccess (C:\ti\sysconfig_1.13.0\dist\webpack:\src\pinmux\services\deprecatedAccessGuard.ts:14:10)
        at Object.runAsUserScript (C:\ti\sysconfig_1.13.0\dist\webpack:\src\pinmux\services\scripting\scriptingGuard.ts:49:3)
        at iteratee (C:\ti\sysconfig_1.13.0\dist\webpack:\src\pinmux\services\scripting\runScript.ts:94:5)
        at baseEach (C:\ti\sysconfig_1.13.0\dist\webpack:\node_modules\lodash\lodash.js:530:11)
        at Function.each (C:\ti\sysconfig_1.13.0\dist\webpack:\node_modules\lodash\lodash.js:9409:52)
        at iteratee (C:\ti\sysconfig_1.13.0\dist\webpack:\src\pinmux\services\scripting\runScript.ts:92:6)
        at at (C:\ti\sysconfig_1.13.0\dist\webpack:\node_modules\lodash\lodash.js:530:11)
    Caused by: Error: Configurable "mode" of "/ti/drivers/SPI": Validation failed: [
      {
        "keyword": "type",
        "dataPath": "/options/0/name",
        "schemaPath": "#/definitions/EnumerationOption<number>/properties/name/type",
        "params": {
          "type": "number"
        },
        "message": "should be number"
      },
      {
        "keyword": "additionalProperties",
        "dataPath": "/options/1",
        "schemaPath": "#/definitions/EnumerationOption<string>/additionalProperties",
        "params": {
          "additionalProperty": "legacyNames"
        },
        "message": "should NOT have additional properties"
      },
      {
        "keyword": "anyOf",
        "dataPath": "",
        "schemaPath": "#/anyOf",
        "params": {},
        "message": "should match some schema in anyOf"
      }
    ]
        at validateConfigurable (C:\ti\sysconfig_1.13.0\dist\webpack:\src\pinmux\services\objectManagers\configurable.ts:1281:10)
        at Object.createMetaContentConfigurableMgr (C:\ti\sysconfig_1.13.0\dist\webpack:\src\pinmux\services\objectManagers\configurable.ts:1307:3)
        at S.createMetaContentConfigurableMgr (C:\ti\sysconfig_1.13.0\dist\webpack:\src\pinmux\services\objectManagers\moduleInstance.ts:763:10)
        at iteratee (C:\ti\sysconfig_1.13.0\dist\webpack:\src\pinmux\services\objectManagers\moduleInstance.ts:757:57)
        at baseMap (C:\ti\sysconfig_1.13.0\dist\webpack:\node_modules\lodash\lodash.js:653:23)
        at Function.map (C:\ti\sysconfig_1.13.0\dist\webpack:\node_modules\lodash\lodash.js:9621:51)
        at S.addMetaContentConfigurableMgrs (C:\ti\sysconfig_1.13.0\dist\webpack:\src\pinmux\services\objectManagers\moduleInstance.ts:757:30)
        at S.initMetaConfigurables (C:\ti\sysconfig_1.13.0\dist\webpack:\src\pinmux\services\objectManagers\moduleInstance.ts:801:8)
        at Function.createInstanceImpl (C:\ti\sysconfig_1.13.0\dist\webpack:\src\pinmux\services\objectManagers\moduleInstance.ts:126:11)
        at Function.createInstance (C:\ti\sysconfig_1.13.0\dist\webpack:\src\pinmux\services\objectManagers\moduleInstance.ts:999:28)
    gmake: *** [build-870619151] Error 1
    gmake: Target 'all' not remade because of errors.
    
    **** Build Finished ****

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    该错误是由旧版 syscfg 造成的。 我可以看到您使用的是 v1.13.0。 您是否可以更换 v1.15.0或更高版本并重新测试?

    我可以使用 v1.15。

    此致、

    Shlomi