This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2340R5:处理信号 ZB_BDB_SIGNAL_TROGING 中的状态-1

Guru**** 2923960 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group/zigbee-and-thread/f/zigbee-thread-forum/1513778/cc2340r5-handling-status--1-in-signal-zb_bdb_signal_steering

器件型号:CC2340R5

工具/软件:

CC2340运行 ZBOSS 终端器件示例、并调用了 bdb_start_top_level_commissioning (ZB_BDB_network_steering)来启动网络转向。 当终端设备找不到协调器时、应用程序 在~20秒后收到信号 ZB_BDB_SIGNAL_TROWING 中的状态代码-1。

ZBOSS 用户指南仅列出了2个状态代码:RET_OK 和 RET_INTERRUPT、但未说明状态代码-1在该信号中的含义。

问题是:

1.  收到此状态代码-1后、是否可以再次调用 bdb_start_top_level_commissioning (ZB_BDB_NETWORK_STOINGING)?

2.是否有地方为 bdb_start_top_level_commissioning (ZB_BDB_NETWORK_STOINGING)设置此超时(距离观察时间~20秒)?

此致、

Shuyang